Arduino
  • Products
  • More
Arduino
Arduino Forum Piano Stairs (Musical Stairs) Part 1 - Planning and feasibility
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 10 replies
  • Answers 1 answer
  • Subscribers 412 subscribers
  • Views 1895 views
  • Users 0 members are here
Related

Piano Stairs (Musical Stairs) Part 1 - Planning and feasibility

Former Member
Former Member over 12 years ago

I would like to turn my basement stairs into "piano stairs". This is a request for input more than a show and tell.
 
Background:
You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Project stairs:

http://img.photobucket.com/albums/v112/prn_star/piano%20stairs/IMG_1752.jpg

Stairs from underneath.

http://img.photobucket.com/albums/v112/prn_star/piano%20stairs/IMG_1754.jpg

~Specs:

http://img.photobucket.com/albums/v112/prn_star/piano%20stairs/Untitled.jpg

 

I have purchased nothing yet.

Item starter list:

Raspberry Pi

Ardunio (max) (I would like 12 "keys" or active stairs min)

sensors - tbd

 

The sensing is going to be the hard part (I think):

 

FSR: I started looking into force sensing resisters to be put under the laminate flooring but from googling and reading I'm uncertain that would work well.

 

PIR motion sensors issues/questions:

From looking on youtube most of the PIR sensors either have 2 short a sensing range or too large a range. 10cm to 15cm would probably be idea.

The "reset" time on PIR's factory preset?

If someone tried to key a stair twice quickly it would probably not activate for 2+ seconds?

 

IRDS: Thoughts on using IR distance sensor instead of PIR?

IR has the right range settings from 4 inches (10 cm) to 80cm.

 

IR Beam: Beam sensor would be too difficult to install due to the physical requirements of access to both sides of the stairs.

 

I'm assuming that I can get the sensed activation from the Ardunio to the rPI to play a note or tone?

Would this setup be able to trigger multiple notes at once? Lets say 4 feet(2 people) playing.

 

Thoughts on if this project is worthwhile?

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 12 years ago +1
    Cool idea I remember something similar in a night club mannnnny years ago, and it worked great....except when everyone stood on the stairs. You might want to look at capacitive sensing. You basically stick…
Parents
  • jvdberg@ieee.org
    0 jvdberg@ieee.org over 12 years ago

    The sensing indeed will be the hard part. What worries me the most is the length of the wires from the sensors to the processor. The use of shielded wires is recommended. Some electronic organs already have problems with long wires from the keyboard to the electronics. These wires will pick up RF signals that let the piano play if nobody is using the stairs. These wires can also radiate signals from the processor and cause interference on radio and TV reception. To solve these EMC-problems the best way is to use robust sensors and an interface/isolation board using optocouplers or relays between the sensors and the processor. To let it sound like music it is possible to program the adjacent stairs to play a tune. Then only the rhythm depends on the person using the stairs. You could play different tunes if somebody is going up or down the stairs.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jvdberg@ieee.org
    0 jvdberg@ieee.org over 12 years ago

    The sensing indeed will be the hard part. What worries me the most is the length of the wires from the sensors to the processor. The use of shielded wires is recommended. Some electronic organs already have problems with long wires from the keyboard to the electronics. These wires will pick up RF signals that let the piano play if nobody is using the stairs. These wires can also radiate signals from the processor and cause interference on radio and TV reception. To solve these EMC-problems the best way is to use robust sensors and an interface/isolation board using optocouplers or relays between the sensors and the processor. To let it sound like music it is possible to program the adjacent stairs to play a tune. Then only the rhythm depends on the person using the stairs. You could play different tunes if somebody is going up or down the stairs.