Arduino Forum Arduino I/O Pins
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
  • State Verified Answer
  • Replies 14 replies
  • Answers 2 answers
  • Subscribers 403 subscribers
  • Views 1561 views
  • Users 0 members are here
  • helpme
  • make
  • diy
  • led
  • arduino
Related

Arduino I/O Pins

Former Member
Former Member over 12 years ago

I'm making a button project that need about 10 leds and 12 buttons,

I'm using an arduino uno, but there just arn't enough I/O pins, I'm fairly

new to arduino, so it may be that I just dont know to to properly wire one up and porperly code it to make it work perfectly.

 

The project is this:

 

The idea is to have a project box with about 10 buttons on the project box and little LEDs next to them, wherever the LEDs are placed, there will be pieces of paper indicating what each button represents next to the LEDs . The box would also have 2 buttons on the side of the project box, one would be used to turn on the leds that had their corresponding buttons pushed and the other

would reset the system so it could be used with different combonations.

 

This is my code,

Don't pay attention to the comments!


// this constant won't change:

const int buttonPin = 2;

const int buttonPin2 = 8;

const int buttonPin3 = 3;

const int buttonPin4 = 5;

const int buttonPin5 = 6;

int buttonReset2 = 10;

// the pin that the pushbutton is attached to

int ledPin = 13;

int ledPin2 = 12;

int ledPin3 = 4;

int ledPin4 = 7;

int ledPin5 = 11;

int ledShow2 = 9;

// the pin that the LED is attached to

 

 

// Variables will change:

int buttonPushCounter = 0;

int buttonPushCounter2 = 0;

int buttonPushCounter3 = 0;

int buttonPushCounter4 = 0;

int buttonPushCounter5 = 0;

 

 

// counter for the number of button presses

int ledShow = 0;

int buttonState = 0;

int buttonState2 = 0;

int buttonState3 = 0;

int buttonState4 = 0;

int buttonState5 = 0;

 

 

int buttonReset = 0;

// current state of the button

int lastButtonState = 0;

int lastButtonState2 = 0;

int lastButtonState3 = 0;

int lastButtonState4 = 0;

int lastButtonState5 = 0;

 

 

 

 

void setup() {

  // initialize the button pin as a input:

  pinMode(ledShow, INPUT);

  pinMode(buttonPin, INPUT);

  pinMode(buttonPin2, INPUT);

  pinMode(buttonPin3, INPUT);

  pinMode(buttonPin4, INPUT);

  pinMode(buttonPin5, INPUT);

  // initialize the LED as an output:

  pinMode(ledPin, OUTPUT);

  pinMode(ledPin2, OUTPUT);

  pinMode(ledPin3, OUTPUT);

  pinMode(ledPin4, OUTPUT);

  pinMode(ledPin5, OUTPUT);

  // initialize serial communication:

  Serial.begin(9600);

}

 

 

 

 

void loop() {

  // read the pushbutton input pin:

  buttonReset = digitalRead(buttonReset2);

 

 

  ledShow = digitalRead(ledShow2);

 

  buttonState = digitalRead(buttonPin);

 

  buttonState2 = digitalRead(buttonPin2);

 

  buttonState3 = digitalRead(buttonPin3);

 

  buttonState4 = digitalRead(buttonPin4);

 

  buttonState5 = digitalRead(buttonPin5);

 

 

 

 

 

  // compare the buttonState to its previous state

  if (buttonState != lastButtonState) {

    // if the state has changed, increment the counter

    if (buttonState == 1) {

      // if the current state is HIGH then the button

      // wend from off to on:

      buttonPushCounter++;

    }

    else {

      // if the current state is LOW then the button

      // wend from on to off:

      delay(1);

    }

  }

  // save the current state as the last state,

  //for next time through the loop

  lastButtonState = buttonState;

 

 

 

  // turns on the LED every four button pushes by

  // checking the modulo of the button push counter.

  // the modulo function gives you the remainder of

  // the division of two numbers:

  if (buttonPushCounter % 2 == 0) {

    digitalWrite(ledPin, HIGH);

  } else {

   digitalWrite(ledPin, LOW);

   }

     // compare the buttonState to its previous state

  if (buttonState2 != lastButtonState2) {

    // if the state has changed, increment the counter

    if (buttonState2 == 1) {

      // if the current state is HIGH then the button

      // wend from off to on:

      buttonPushCounter2++;

    }

    else {

      // if the current state is LOW then the button

      // wend from on to off:

      delay(1);

    }

  }

  // save the current state as the last state,

  //for next time through the loop

  lastButtonState2 = buttonState2;

 

 

 

  // turns on the LED every four button pushes by

  // checking the modulo of the button push counter.

  // the modulo function gives you the remainder of

  // the division of two numbers:

  if (buttonPushCounter2 % 2 == 0) {

    digitalWrite(ledPin2, HIGH);

  } else {

   digitalWrite(ledPin2, LOW);

   }

 

  // compare the buttonState to its previous state

  if (buttonState3 != lastButtonState3) {

    // if the state has changed, increment the counter

    if (buttonState3 == 1) {

      // if the current state is HIGH then the button

      // wend from off to on:

      buttonPushCounter3++;

    }

    else {

      // if the current state is LOW then the button

      // wend from on to off:

      delay(1);

    }

  }

  // save the current state as the last state,

  //for next time through the loop

  lastButtonState3 = buttonState3;

 

 

 

  // turns on the LED every four button pushes by

  // checking the modulo of the button push counter.

  // the modulo function gives you the remainder of

  // the division of two numbers:

  if (buttonPushCounter3 % 2 == 0) {

    digitalWrite(ledPin3, HIGH);

  } else {

   digitalWrite(ledPin3, LOW);

   }

 

  // compare the buttonState to its previous state

  if (buttonState4 != lastButtonState4) {

    // if the state has changed, increment the counter

    if (buttonState4 == 1) {

      // if the current state is HIGH then the button

      // wend from off to on:

      buttonPushCounter4++;

    }

    else {

      // if the current state is LOW then the button

      // wend from on to off:

      delay(1);

    }

  }

  // save the current state as the last state,

  //for next time through the loop

  lastButtonState4 = buttonState4;

 

 

 

  // turns on the LED every four button pushes by

  // checking the modulo of the button push counter.

  // the modulo function gives you the remainder of

  // the division of two numbers:

  if (buttonPushCounter4 % 2 == 0) {

    digitalWrite(ledPin4, HIGH);

  } else {

   digitalWrite(ledPin4, LOW);

   }

 

  // compare the buttonState to its previous state

  if (buttonState5 != lastButtonState5) {

 

    if (buttonState5 == 1) {

 

      buttonPushCounter5++;

    }

    else {

 

      delay(1);

    }

  }

  lastButtonState5 = buttonState5;

 

  if (buttonPushCounter5 % 2 == 0) {

    digitalWrite(ledPin5, HIGH);

  } else {

   digitalWrite(ledPin5, LOW);

   }

 

   if (buttonReset == 1 && buttonPushCounter > 0){

     buttonPushCounter--;

   }

   else{

     delay(1);

     if (buttonReset == 1 && buttonPushCounter2 > 0){

     buttonPushCounter--;

   }

   else{

     delay(1);

     if (buttonReset == 1 && buttonPushCounter3 > 0){

     buttonPushCounter--;

   }

   else{

     delay(1);

   }

     if (buttonReset == 1 && buttonPushCounter4 > 0){

     buttonPushCounter--;

   }

   else{

     delay(1);

     if (buttonReset == 1 && buttonPushCounter5 > 0){

     buttonPushCounter--;

   }

   else{

     delay(1);

   }

   if (ledPin == 1 && ledShow == 0){

     ledPin--;

     if(ledPin == 0 && ledShow ==1){

       ledPin++;

     }

     else{

       delay(1);

   }

   }else{

   }

     delay(1);

 

     if (buttonReset == 1 && buttonState == 1){

       buttonState++;

     }

     else{

       delay(1);

     }

     if (buttonReset == 1 && buttonState2 == 1){

       buttonState++;

     }

     else{

       delay(1);

     }

     if (buttonReset == 1 && buttonState3 == 1){

       buttonState++;

     }

     else{

       delay(1);

     }

     if (buttonReset == 1 && buttonState4 == 1){

       buttonState++;

     }

     else{

       delay(1);

     }

     if (buttonReset == 1 && buttonState5 == 1){

       buttonState++;

     }

     else{

       delay(1);

 

 

 

     }

   }

}

   }

   }

 

 

 

Do not pay attention to the comments!

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 12 years ago in reply to Former Member +2
    Michael You could always connect the buttons to the Analogue inputs, across a resistor ladder. You can easily have 6 buttons on one input. There is some discussion here http://forum.arduino.cc/index.php…
  • shabaz
    shabaz over 12 years ago in reply to Former Member +1 verified
    Hi Michael, Ways to do it with no additional parts are more complicated and less straightforward if the number of inputs and outputs exceeds the number of pins; it may be possible using multiplexing (again…
  • ntewinkel
    ntewinkel over 12 years ago +1
    You could also try the Arduino library for a "matrix keyboard" - I haven't tried it myself yet, but it looks like it will make it easier to handle multiple buttons. http://playground.arduino.cc/Main/KeypadTutorial…
Parents
  • shabaz
    0 shabaz over 12 years ago

    Hi Michael,

     

    Too much code to check :-)

    However, if you can get the code for one switch and LED working, then you can scale it up. For lots of I/O, google I2C bus expanders - they are popular, and there will likely be an existing Arduino code library for it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 12 years ago in reply to shabaz

    Though I would like to be able to say I know what your saying, I dont image

    are there anyways to do this where I dont have to add parts to the board, or ways that are more "simple"

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 12 years ago in reply to shabaz

    Though I would like to be able to say I know what your saying, I dont image

    are there anyways to do this where I dont have to add parts to the board, or ways that are more "simple"

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • shabaz
    0 shabaz over 12 years ago in reply to Former Member

    Hi Michael,

     

    Ways to do it with no additional parts are more complicated and less straightforward if the number of inputs and outputs exceeds the number of pins; it may be possible using multiplexing (again, this is a topic you'd need to google/research), but I'm not sure.

     

    I2C is a very common thing, there will be hundreds of hits on the Internet with Arduino, and will be easier.

    Take a look at this; it connects to two pins on the Arduino, and gives you 8 inputs/outputs (configurable).

     

    There is a tutorial here which uses the same I2C port expander IC, with wiring diagrams and code.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 12 years ago in reply to shabaz

    Ok I'll take look at it and I'll also look at I2C again. Thanks so much!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 12 years ago in reply to Former Member

    Michael

    You could always connect the buttons to the Analogue inputs, across a resistor ladder.

    You can easily have 6 buttons on one input.

     

    There is some discussion here

     

    http://forum.arduino.cc/index.php/topic,20125.0.html

    http://tronixstuff.files.wordpress.com/2012/02/circuit1.jpg

     

    Mark

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 12 years ago in reply to mcb1

    Good idea!! :-)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 12 years ago in reply to shabaz

    Cheers

    You do need to be careful, as the buttons end up with a 'priority'.

    ie the one closest to the pin will override the others.

     

    This is only applicable if more than one is pressed at the same time.

     

    I always prefer switching the ground to prevent 'accidents', and its possible to have a binary function as well by having multiple in parallel (but with different values).

     

    Michael

    If you use this method, it pays to have a range for the value rather than an absolute figure to allow for tolerances, voltage etc.

    Terry King has a good sketch to show you what I mean http://arduino-info.wikispaces.com/LCD-Pushbuttons

     

    Mark