Arduino Forum hi,i have a doubt on arduino atmega 2560  project
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
  • State Suggested Answer
  • Replies 7 replies
  • Answers 1 answer
  • Subscribers 402 subscribers
  • Views 571 views
  • Users 0 members are here
  • arduino
Related

hi,i have a doubt on arduino atmega 2560  project

Former Member
Former Member over 11 years ago

am doing web data logger using arduino but while writting the data to the sd card some error occur..sd card "file not opening" according rto the code written by myself the code is below can any one help me out..am usig arduino atmega2560 and ethernet sheild...

#include<SD.h>

#include<SPI.h>

const int chipSelect = 4;

 

 

void setup()

{

// Open serial communications and wait for port to open:

  Serial.begin(9600);

   while (!Serial) {

    ; // wait for serial port to connect. Needed for Leonardo only

  }

 

 

 

 

  Serial.print("Initializing SD card...");

  // make sure that the default chip select pin is set to

  // output, even if you don't use it:

  pinMode(10, OUTPUT);

 

  // see if the card is present and can be initialized:

  if (!SD.begin(chipSelect)) {

    Serial.println("Card failed, or not present");

    // don't do anything more:

    return;

  }

  Serial.println("card initialized.");

}

 

 

void loop()

{

  // make a string for assembling the data to log:

  String dataString = "";

 

 

  // read three sensors and append to the string:

  for (int analogPin = 0; analogPin < 3; analogPin++) {

    int sensor = analogRead(analogPin);

    dataString += String(sensor);

    if (analogPin < 2) {

      dataString += ",";

    }

  }

 

 

  // open the file. note that only one file can be open at a time,

  // so you have to close this one before opening another.

  File dataFile = SD.open("datalog.txt", FILE_WRITE);

 

 

  // if the file is available, write to it:

  if (dataFile) {

    dataFile.println(dataString);

    dataFile.close();

    // print to the serial port too:

    Serial.println(dataString);

  } 

  // if the file isn't open, pop up an error:

  else {

    Serial.println("error opening datalog.txt");

  }

}

  • Sign in to reply
  • Cancel
Parents
  • neilk
    0 neilk over 11 years ago

    Hi Indira

     

    Have a look at the example sketch provided with the Arduino SD card Library called "Cardinfo". I think you will see there that the pin you need to set as Output for the library to work is in fact 53 for the ATMega. If you correct that, things should work.

     

    If not, try running the Cardinfo sketch on its own, to prove that everything is OK with SD Card Interface and the SD Card itself - not all SD cards work!

     

    Best wishes

     

    Neil

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to neilk

    thank u neil ill check this...and will reply to u

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 11 years ago in reply to neilk

    thank u neil ill check this...and will reply to u

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Former Member
    0 Former Member over 11 years ago in reply to Former Member

    hi one more doubt..how can we get thee form key for google spread sheet or form in google docs..actually i need to store my sensor data in excel sheet continuosly through internet can u suggest me any model project work...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago in reply to Former Member

    here us a tutorial http://www.open-electronics.org/how-send-data-from-arduino-to-google-docs-spreadsheet/

     

    tells you all you need to know

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to Robert Peter Oakes

    i tried but i dunno the form key..how to get the form key...

    https://docs.google.com/forms/d/1qAeAlDAN-TC74lKeLSCvucNmNxcPO09PCSVkysuaw_c/edit

    this is the google form...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago in reply to Former Member

    like the link describes, it is in the URL

     

    1qAeAlDAN-TC74lKeLSCvucNmNxcPO09PCSVkysuaw_c

     

    the link you posted to get tot the form works correctly so it must be containing the form key, and this is it i believe

     

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to Robert Peter Oakes

    the same project wat u sent is am doing but int that area(form key ) am getting struck....did u get the output with that project if it is so can u help me...i want to do that project with ur presence..i hope ill rectify the errors..