Arduino Forum Input a signal from a sensor to an Arduino Due
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
  • State Suggested Answer
  • Replies 9 replies
  • Answers 5 answers
  • Subscribers 403 subscribers
  • Views 2310 views
  • Users 0 members are here
  • arduino
  • sensor
Related

Input a signal from a sensor to an Arduino Due

Former Member
Former Member over 11 years ago

I'm working with Arduino Due and I have a sensor that outputs a square signal with voltages in the range of 0-5V.

In the Due specs there is a warning that says:

"Warning: Unlike other Arduino boards, the Arduino Due board runs at 3.3V. The maximum voltage that the I/O pins can tolerate is 3.3V. Providing higher voltages, like 5V to an I/O pin could damage the board."

Is it possible to connect it to the board?

Thanks.

  • Sign in to reply
  • Cancel

Top Replies

  • Former Member
    Former Member over 11 years ago +1 suggested
    Just put voltage divider on sensor output.... it will work great and about talk to sensor 3.3V logic is enough to drive logic1 on 5V sensor...
Parents
  • Former Member
    0 Former Member over 11 years ago

    Just put voltage divider on sensor output.... it will work great

    and about talk to sensor 3.3V logic is enough to drive logic1 on 5V sensor...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to Former Member

    Thanks.

     

    Can I also use a logic level converter?

     

    https://www.sparkfun.com/products/12009

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago in reply to Former Member

    yes you can use one of those, no roblems

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago in reply to Former Member

    yes you can use one of those, no roblems

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • Former Member
    0 Former Member over 11 years ago in reply to Robert Peter Oakes

    So all I need is to connect the sensor's output to the high input on the converter and the low output to the Arduino digital pin? (and obviously the GND connection)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago in reply to Former Member

    I would think so, I have never personally used one but yes that sounds correct

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to Robert Peter Oakes

    OK thanks a lot!