Arduino Forum Temperature-control with arduino / MAX31855 / NXP KTY84
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
  • State Verified Answer
  • Replies 8 replies
  • Answers 2 answers
  • Subscribers 403 subscribers
  • Views 2263 views
  • Users 0 members are here
  • temperature
  • maxim
  • nxp
  • arduino
  • sensor
Related

Temperature-control with arduino / MAX31855 / NXP KTY84

Former Member
Former Member over 11 years ago

Hello Community,

 

I'm a software engineer  so I don't have much experience with HW. My goal is to create a small temperature-control with an arduino and I already found some parts that might work together, but I'm not sure about that and it would be great  if someone more experienced could help me out.

 

Basically I want to measure temperatures up to about 200-250 °C that are created by a e-cigarette-heating element. If the temperature exceeds a certain limit, I want to turn off the heating element. If the temperature drops below a threshold I want to turn the heating element back on.

The control is done by an arduino UNO. Because the heating element needs a lot of power (well not THAT much, but propably more than the arduino can handle), I would use a MOSFET controlled by the arduino to switch it on and off.

 

The measurement could be done using a MAX31855 (Type K) connected via SPI to the arduino. As a thermocoupler I would use a NXP KTY84 which has a tempeture-range from -40°C to +300°C which should be good.

 

So here are the questions:

- Will a MAX31855 work with the NXP KTY84? (I think so, because it has a K in its label. image )

- What kind of MOSFET do you recommend? (I have no idea, but is needs to be activated with the 5V of the Arduino.

 

 

Here are some links to datasheets. They are also attached to this topic:

MAX31855: https://www.adafruit.com/datasheets/MAX31855.pdf

NXP KTY84: http://www.produktinfo.conrad.com/datenblaetter/175000-199999/183458-da-01-en-Temperatursensor_KTY84.pdf

Thanks in advance for your help!

 

Marc

Attachments:
image183458-da-01-en-Temperatursensor_KTY84.pdf
imageMAX31855.pdf
  • Sign in to reply
  • Cancel
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago

    I have recently posted a few YouTube  videos on how to drive MOSFETS and higher power loads, also how to read from none micro-controller voltage levels, you may find it useful

     

    www.youtube.com/user/thebreadboardca

     

    regards

     

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 11 years ago in reply to Robert Peter Oakes

    Hi Peter - Thanks for the time you put into those nice and informative videos.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 11 years ago in reply to Robert Peter Oakes

    Hi Peter - Thanks for the time you put into those nice and informative videos.

    John