Arduino
  • Products
  • More
Arduino
Arduino Forum Arduino YUN sending data to WS via POST
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 6 replies
  • Answers 2 answers
  • Subscribers 411 subscribers
  • Views 1517 views
  • Users 0 members are here
  • yun
  • webservice
  • post
  • server
  • arduino
  • bridge
Related

Arduino YUN sending data to WS via POST

Former Member
Former Member over 11 years ago

Hello Everyoune,

I've my Arduino YUN with a protoshield and some gas sensors (metane, idrogene, temperature, humidity).

I've got to send these values via POST to a web service in PHP. Knowing that:

1) Arduino YUN is connected to a WiFi Router which is connected to the internet (my smartphone working as WiFi Router);

2) The WS works well because when getting post variables from other sources it saves and visualizes data;

3) Arduino YUN is connected to WiFi Router via WiFi and to the PC (which is also connected to the same Router wirelessly) via USB, so I can check serial messages via Serial Monitor on the PC, and also checking on the internet if data are sent and visualized.

 

So, the fact is, even if everybody sends data the same way (see the sketch below) it doesn't work for me. I've also tried to use another Arduino YUN, but nothing. The sketch is:

 

          #include <Bridge.h>

          #include <Console.h>

          #include <FileIO.h>

          #include <HttpClient.h>

          #include <Mailbox.h>

          #include <Process.h>

          #include <YunClient.h>

          #include <YunServer.h>

          #include <dht.h>

          #include <SPI.h>

 

          //IP Address of the sever on which there is the WS: http://www.mywebsite.com/

          IPAddress server(XX,XX,XX,XX);

 

          YunClient client;

          dht DHT;

          #define DHT11_PIN 2

          int temp;

          int hum;

          int metano;

          int idrogeno;

          int led_giallo = 13;

          int led_rosso = 12;

          String parametri ="";           //String of POST parameters

 

          void setup()

          {

                 Bridge.begin();

                 Serial.begin(9600);

 

                 pinMode(led_rosso,OUTPUT);

                 pinMode(led_giallo,OUTPUT);

                 digitalWrite(led_giallo,HIGH);

                 digitalWrite(led_rosso,LOW);

                 delay(2500);

                 digitalWrite(led_giallo,LOW);

          }

 

          void loop()

          {

                 //measures

                 metano = analogRead(0);

                 idrogeno = analogRead(1);

                 hum = (int) DHT.humidity;

                 temp = (int) DHT.temperature;

 

                 if (client.connect(server, 80)) {

                          Serial.println("connected");

                          delay(2500);

                          parametri="temp="+String(temp) + "&hum="+ String(hum)+"&metano="+String(metano)+"&idrogeno="+String(idrogeno);

                          client.println("POST /test/arduino/add.php HTTP/1.1");

                          client.println("Host: XX.XX.XX.XX");

                          client.print("Content-length:");

                          client.println(parametri.length());

                          Serial.println(parametri);

                          client.println("Connection: Close");

                          client.println("Content-Type: application/x-www-form-urlencoded;");

                          client.println();

                          client.println(parametri);  

                 }else{

                        Serial.println("connection failed");

                        digitalWrite(led_rosso,HIGH);

                        delay(1000);

                 }

                 if(client.connected()){

                             client.stop();   //disconnect from server

                 }

                 delay(2000);

    }

 

 

Could anyone help me? Why data does't arrive to the WS?

Thank you all, very much!!!

  • Sign in to reply
  • Cancel

Top Replies

  • Former Member
    Former Member over 11 years ago +1 verified
    I've found the solution. The problem was not about the ip address but how how formulate the request... So I changed from: client.println("POST /test/arduino/add.php HTTP/1.1"); client.println("Host: XX…
  • gadget.iom
    0 gadget.iom over 11 years ago

    Visiting the IP Address you specified resulted in a "Bad Request" error.

    Is your website hosted on a shared hosting plan? If so that IP address is shared across multiple websites and you may not be posting your data to yours.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago

    I've found the solution. The problem was not about the ip address but how how formulate the request...

    So I changed from:

                              client.println("POST /test/arduino/add.php HTTP/1.1");

                              client.println("Host: XX.XX.XX.XX");

    to:

                              client.println("POST /test/arduino/add.php HTTP/1.1");

                              client.println("Host: www.mywebsite.com");

    and it works!!

    Thank you Paul Ellison for your help!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • gadget.iom
    0 gadget.iom over 11 years ago in reply to Former Member

    Great news image

     

    It could be that changing the 'Host:' from the IP to the domain name has allowed Arubas DNS server to redirect your request more effectively.

     

    Glad you got it sorted

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 11 years ago

    If you use an IP address like client.println("Host: XX.XX.XX.XX"), you must know about WiFi routing and forwarding. Without the specifics, I would guess the IP was non routable within the setup. Unless you have the necessary knowledge, it is best to use URL like client.println("Host: www.mywebsite.com") which uses DNS to get where you want to go.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago

    Hi all,

    I am new to working in yun board. I have tried the same program. I gave IPAddress server(192,168,0,54); which is my yun board ip address and to the  client.println("Host: www.mywebsite.com");  I dono what I have to give.  Can anybody please tell me what I have to give here and also please tell me how to see the data on web browser. Is there any files I need to put in memory card or I  dont need anything.

     

    thank you in advance.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ralph23
    0 ralph23 over 9 years ago

    Can this be done by using xampp? I tried changing  xampp apache server to an ip address of 192.168.1.200 and it's what i put in the X's but there's no luck in receiving the data in the server. In the serial monitor though it prints connected.