Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum When is the function delay() a delay?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 41 replies
  • Subscribers 413 subscribers
  • Views 10557 views
  • Users 0 members are here
  • delay
  • arduino_code
Related

When is the function delay() a delay?

colporteur
colporteur over 3 years ago

else if (MainDepartureState == LOW && MainArrivalState == LOW) {
        if (startupMain == HIGH) {
          // pulse turnout for Main train
          digitalWrite(Main_Turnout, HIGH);
          relayDelay();//<-----1
          digitalWrite(Main_Turnout, LOW);
          if (deBug == HIGH) {
            Serial.println("The Main Turnout Activated");
          }
          // Engage Motor for Main
          motors.setSpeedB(minSpeedB);  // Start Motor for Main
          motors.forwardB();
          PowerMain = LOW;
          startupMain = LOW;
          delay(300000);//<----2
          if (deBug == HIGH) {
            Serial.println("Motor Delay Complete");
          }

According to what I have read “The delay() function allows you to pause the execution of your Arduino code for a specified period.”

Why are the delays I am using not working or the values are so extreme? How can I best accomplish a delay?

I tried using the delay() function at point <----1 in my code and it failed miserably. I wanted to activate a relay by turning it on, waiting for relay to engage (delay(2000), then turn it off. The delay(2000) two seconds didn’t work. I wrote a little relay routine that accomplish what I wanted but why did delay(2000) not give me two seconds?

I am using delay() function at <----2 in the code but the value doesn’t reflect the actual delay. I needed to generate some wait time for the motor to engage and trigger a sensor. My desire was a three second delay(3000) but the delay(300000) was a value that actually worked. That would be 300 seconds yes/no?

I'm a code resurrectionist and not an actual programmer. I will try and muddle through discussions 

  • Sign in to reply
  • Cancel

Top Replies

  • colporteur
    colporteur over 3 years ago +6
    Based on GL shared insight, I used a different set of PWM pins so as not to muck with the delay() timer. I also took the BE suggestions and used subtraction in the millis routines. I am happy to report…
  • Gough Lui
    Gough Lui over 3 years ago in reply to colporteur +5
    //user input variables int turnout_delay = 10000; //delay for relay contacts to engage int motor_delay = 900000; //delay for motor to move train unsigned long time_now = 0; int type cannot store outside…
  • Gough Lui
    Gough Lui over 3 years ago in reply to colporteur +3
    I think that it helps if one can see names like "TCCR0B" and know inside that it is short for "Timer Control Counter Register" then that should immediately set-off alarm bells in one's head. Gough Lui…
Parents
  • Gough Lui
    Gough Lui over 3 years ago

    Well, in theory, delay(2000) should delay for 2 seconds. As per https://www.arduino.cc/reference/en/language/functions/time/delay/

    However, there are some potential caveats - for example:

    What board are you using? (ESP8266's for example, don't like to be kept waiting and will crash out by watchdog timer)
    Are you using the right "core" settings in Arduino for the board? (if the clock crystal on the board is not matching the expected clock rate, delays could be wrong.)
    Are you doing something else with the timer peripherals on the microcontroller that could interfere with the Arduino code?

    Try this - what does a simple LED blinky sketch with delay do? Does it wait the expected amount of time? Or alternatively code your delay by checking millis() - does that work or not?

    - Gough

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Gough Lui
    Gough Lui over 3 years ago

    Well, in theory, delay(2000) should delay for 2 seconds. As per https://www.arduino.cc/reference/en/language/functions/time/delay/

    However, there are some potential caveats - for example:

    What board are you using? (ESP8266's for example, don't like to be kept waiting and will crash out by watchdog timer)
    Are you using the right "core" settings in Arduino for the board? (if the clock crystal on the board is not matching the expected clock rate, delays could be wrong.)
    Are you doing something else with the timer peripherals on the microcontroller that could interfere with the Arduino code?

    Try this - what does a simple LED blinky sketch with delay do? Does it wait the expected amount of time? Or alternatively code your delay by checking millis() - does that work or not?

    - Gough

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • colporteur
    colporteur over 3 years ago in reply to Gough Lui

    The board is a Geekcret Arduino Mega 2560 (on chip) knock-off.

    I'm not manipulating any timers.

    The program reads a set of eight IR sensors divided across two tracks. Four sensors on one track four sensors on the second track. The four sensors per track are divided down into pairs. One pair is departure and the other pair is arrival. The exercise is to read a model train motion as it passes over the sensors. A sensor reads 0, when the train is over it. The sequence: stop (0000), departure(0011), in transit(1111), arrival (1100) and stop (0000) as the train moves from right to left over the sensors.

    I tried the exercise of confirming the timing of delay. If saying one-steamboat is a second (old touch football trick) the Blink sketch from examples flashes on & off for the number of seconds set up in delay().

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Gough Lui
    Gough Lui over 3 years ago in reply to colporteur

    Good. This means your board set-up is fine and the problem is most likely in your code ... check data types as I had noted in my other reply.

    - Gough

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Gough Lui
    Gough Lui over 3 years ago in reply to colporteur

    Could you also let us know whether you are using any libraries - you might not be directly manipulating timers, but the libraries you are using may be?

    - Gough