Arduino Forum Arduino UNO R4 coming shortly
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
  • Replies 18 replies
  • Subscribers 399 subscribers
  • Views 4204 views
  • Users 0 members are here
  • uno
  • arduino
Related

Arduino UNO R4 coming shortly

Andrew J
Andrew J over 2 years ago

Saw this today: Arduino UNO r4 on the official site.

Renesas processor, 32-bit, 256MB ram CAN bus and more.  Should really open up new projects and give the Mega a run for its money.  Actually makes you wonder what they might do with that one now.

  • Sign in to reply
  • Cancel

Top Replies

  • scottiebabe
    scottiebabe over 2 years ago +7
    Neat. What's also great to see is they are continuing to invest in the arduino library catalog
  • Gough Lui
    Gough Lui over 2 years ago +3
    Hmm. An interesting development indeed. Still 5V, but the loss of AVR doesn't feel like Uno to me ... But perhaps a good move overall ... I wonder how it stacks up to the SAMD-family that has been running…
  • shabaz
    shabaz over 2 years ago +3
    Looks good! I might actually want to finally use an Uno! However this could be a bit of a pain, unless VCC can be changed to 3.3V, otherwise level shifters will be needed with 3.3V logic. Granted lots…
Parents
  • BigG
    BigG over 2 years ago

    Yes this is a curious addition to the Arduino family. The spec isn't ground breaking but it is very sturdy for Arduino-type applications. I see clock speed is set at 48MHz, with 32kB of SRAM and 256kB of flash. There are two interesting offerings. First, is that the board has a power regulator that can handle with 24V, which they say has an improved thermal design. Cool. And the second is that it provides a CAN bus. Also cool. I suspect this product will suit industrial applications quite well.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • BigG
    BigG over 2 years ago

    Yes this is a curious addition to the Arduino family. The spec isn't ground breaking but it is very sturdy for Arduino-type applications. I see clock speed is set at 48MHz, with 32kB of SRAM and 256kB of flash. There are two interesting offerings. First, is that the board has a power regulator that can handle with 24V, which they say has an improved thermal design. Cool. And the second is that it provides a CAN bus. Also cool. I suspect this product will suit industrial applications quite well.

    • Cancel
    • Vote Up +2 Vote Down