Arduino Forum Arduino UNO R4 coming shortly
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
  • Replies 18 replies
  • Subscribers 399 subscribers
  • Views 4226 views
  • Users 0 members are here
  • uno
  • arduino
Related

Arduino UNO R4 coming shortly

Andrew J
Andrew J over 2 years ago

Saw this today: Arduino UNO r4 on the official site.

Renesas processor, 32-bit, 256MB ram CAN bus and more.  Should really open up new projects and give the Mega a run for its money.  Actually makes you wonder what they might do with that one now.

  • Sign in to reply
  • Cancel

Top Replies

  • scottiebabe
    scottiebabe over 2 years ago +7
    Neat. What's also great to see is they are continuing to invest in the arduino library catalog
  • Gough Lui
    Gough Lui over 2 years ago +3
    Hmm. An interesting development indeed. Still 5V, but the loss of AVR doesn't feel like Uno to me ... But perhaps a good move overall ... I wonder how it stacks up to the SAMD-family that has been running…
  • shabaz
    shabaz over 2 years ago +3
    Looks good! I might actually want to finally use an Uno! However this could be a bit of a pain, unless VCC can be changed to 3.3V, otherwise level shifters will be needed with 3.3V logic. Granted lots…
Parents
  • dougw
    dougw over 2 years ago

    If you want a smaller form factor, the Portenta C33 (ARM Cortex M33) might fit the bill. And if you need more horsepower, the GIGA R1 (Arm Cortex M7 + M4) is a beast. Both would seem to be 3.3V I/O.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dougw
    dougw over 2 years ago

    If you want a smaller form factor, the Portenta C33 (ARM Cortex M33) might fit the bill. And if you need more horsepower, the GIGA R1 (Arm Cortex M7 + M4) is a beast. Both would seem to be 3.3V I/O.