Arduino Forum Arduino controlled automatic chicken coop door opener + extras
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
  • Replies 11 replies
  • Subscribers 405 subscribers
  • Views 2910 views
  • Users 0 members are here
  • ardbeginner
Related

Arduino controlled automatic chicken coop door opener + extras

Former Member
Former Member over 10 years ago

I am just going back to school to become an electrical engineer. While i am currently taking lots of pre reqs i am doing my best to learn on my own. I am new to this site and hope you guys will be helpfull in the future. I thought i would post my current project here for all to see. Maybe you guys will have some ideas and helpful tips.

 

A few nights ago i had a raccoon get in with my chickens. While none were killed, one was hurt. I decided i need to make an automatic door for their coop. They normally have an open door to come and go as they choose when they choose. This was the week link, and at about 2 am i was chasing a raccoon out of the coop with a flashlight. Never again! I'm not in an area where i can use a "simple" pop boom solution. I have an arduino (one of the first off the presses Duemilanove) that i have decided to put to use. I will be using a small harbor freight solar panel, a second hand store drill, an old motorcycle battery, my arduino, an H-bridge, a locking wood chicken coop door and a handful of other parts. I am adding a speaker to play a song so the chickies know its bed time, and a light to help with egg production. It is a relatively simple project but a great learning one for me. I am still learning coding so for simplicity i am using ArduBlocks for the coding. This has aloud me to rapidly prototype my project. I am waiting for a few parts to show up and i will begin the project in earnest. I will post photos and hopefully video as i go. Until then, here is my extremely messy teaser photo.

Attachments:
image
  • Sign in to reply
  • Cancel

Top Replies

  • Former Member
    Former Member over 10 years ago +1
    I am using a light sensor and an old rc car as an analog so i can write the program and have it ready when i have all the parts. The light sensor will be replaced with my solar panel who's primary purpose…
  • mcb1
    mcb1 over 10 years ago in reply to Former Member +1
    Excellent start. You've clearly thought what you need, and more importantly a way to do it. The re-use of available parts also means the design is easier, as you know the hardware will work. Best advice…
  • Former Member
    Former Member over 10 years ago +1
    players.brightcove.net/.../index.html
Parents
  • Former Member
    Former Member over 10 years ago

    Valid point guys but i have taken that into consideration. I am pretty use to working with wood. The body of this guy is 3/4 furniture grade plywood. It would be stable in all put laying in a puddle. Well, enough for me anyways. The runner guides are some quarter sawn walnut that has been around for awhile. Even if that does expand a bit i left enough clearance that it shouldn't interfere with the door operation. Lastly the entire thing is on the inside of the coop under a roof. I left plenty of overhang on the coop when i built it so my chickens will stay dry and warm. I have also worked paste wax into the entire project with a heat gun. It should be just fine. The bottom of the door is also cut at a slight angle to minimize the contact point and help prevent the chickens from filling it with crud.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 10 years ago

    Valid point guys but i have taken that into consideration. I am pretty use to working with wood. The body of this guy is 3/4 furniture grade plywood. It would be stable in all put laying in a puddle. Well, enough for me anyways. The runner guides are some quarter sawn walnut that has been around for awhile. Even if that does expand a bit i left enough clearance that it shouldn't interfere with the door operation. Lastly the entire thing is on the inside of the coop under a roof. I left plenty of overhang on the coop when i built it so my chickens will stay dry and warm. I have also worked paste wax into the entire project with a heat gun. It should be just fine. The bottom of the door is also cut at a slight angle to minimize the contact point and help prevent the chickens from filling it with crud.