Arduino
  • Products & Partners
  • More
Arduino
Documents Arduino Day 2020: NanoRama: We're Giving Away Different Nano Boards for Projects that Use Them!
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 24 Feb 2020 8:35 PM Date Created
  • Last Updated Last Updated: 25 Mar 2020 2:25 AM
  • Views 13789 views
  • Likes 20 likes
  • Comments 139 comments
Related
Recommended

Arduino Day 2020: NanoRama: We're Giving Away Different Nano Boards for Projects that Use Them!

image

Arduino Day 2020: NanoRama Giveaway

Quiz | NanoRama Giveaway | NanoRama Contest  | Fighting Germs Contest | Arduino Tutorials | Arduino Projects | Arduino Homepage image

 

In the comments below:  Let Us Know What Arduino Project You Are Planning on Doing for Arduino Day 2020!

 

We'll be sending out a limited number of Nano boards for project proposals that use them!

 

imageimageimage
Arduino is celebrating its 15th Birthday on March 21st, 2020!  We'll be sending out 25 Nano Boards (5 different Flavors) for project proposals that use them!Project14 will celebrate its 3rd Birthday with a NanoRama Celebration that begins the day before Arduino Day!  Help us celebrate by submitting an Arduino Project as a Birthday Present!Winners Announcement will be on Geek Pride Day on May 25th 2020.  It also happens to be the anniversary of the release of the first Star Wars movie.  A New Hope was released on May 25th, 1977!

 

This year, Arduino Day will be on March 21, 2020.  It will be their 15th birthday and we've decided to celebrate with NanoRama party!  We're kicking things off with Nano Giveaway, where we'll make Arduino Nano's new family of boards available on the community for the first time.  Say happy birthday to Arduino in the comments below, and let us know what Arduino project you plan on doing for Arduino's birthday. If your project idea includes one of the five Arduino Nano boards listed below, we'll send a the board of your choice for projects that use them.  The Nano boards that we are giving away are the Arduino Nano (Classic), Nano Every, Nano 33 IoT, Nano 33 BLE, and Nano BLE Sense.

 

Beginning on the 21st of March,  submit your Arduino Day project in Arduino Projects,  Arduino , your blog, or the NanoRama Birthday Special on  Project14 using the tag NanoRamaCH.  Your project can be a birthday present to celebrate Arduino's 15th birthday,  Project14's 3rd birthday, or both!  The Arduino Nano family is featured throughout Arduino Day and the upcoming NanoRama competition, however, you're also free to submit any Arduino based project, not just a Nano based project, if you'd prefer. The first 20 people to submit an Arduino project for Arduino Day win an Arduino Nano!  We'll also include cool Nano boards along with shopping cart as part of the prizes!  The upcoming NanoRama competition closes on May 14th with a winners announcement on May 25th.

 

Key Dates:

 

EventDate
NanoRama (3rd Anniversary of Project14) Launches:20th March 2020
Arduino Day 2020 (15th Anniversary of Arduino):21nd March 2020
Nano Winners Announced:23rd March 2020
NanoRama Closes:14th May 2020
NanoRama Winners Announced (42nd Anniversary of Star Wars):25th May 2020

 

 

We are giving away 25 Arduino Nano boards (5 of each) for Arduino Projects that Use them! 

 

Here are the Nano boards to choose from:

 

 

image

imageimage
Nano (Classic) - Giving away 5 for Project Proposals that use them!Nano Every - Giving away 5 for Project Proposals that use them!Nano 33 IoT - Giving away 5 for Project Proposals that use them!
Buy NowBuy Now
The Arduino Nano is a small, complete, and breadboard-friendly board based on the ATmega328P (Arduino Nano 3.x). It has more or less the same functionality of the Arduino Duemilanove, but in a different package. It lacks only a DC power jack, and works with a Mini-B USB cable instead of a standard one.

Perfect for everyday projects, this board is Arduino's 5 V Board in the smallest form factor available: 45x18mm!

 

The Arduino Nano Every is an evolution of the traditional Arduino Nano, but featuring a lot more powerful processor, the ATMega4809. This will allow you making larger programs than with the Arduino Uno (it has 50% more program memory), and with a lot more variables (the RAM is 200% bigger).

On-board WiFi and BluetoothRegistered connectivity using a u-blox module, the NINA-W10, a low power chipset operating in the 2.4GHz range. A cheap and easy point of entry for enabling IoT on existing devices (and creating new ones) or for designing pico-network applications. Can be used for applications such as building a sensor network connected to your router, or a BLE device sending data to a cellphone

 

Secure communication is ensured through the MicrochipRegistered ECC608 crypto chip. A 6 axis IMU, makes this board perfect for simple vibration alarm systems, pedometers, relative positioning of robots, etc.

Microcontroller: ATMEGA328

Operating Voltage: 5V

Analog Inputs: 8

Memory: 32 KB FLASH, 2KB  SRAM

Microcontroller: ATMEGA4809

Operating Voltage: 5V

Analog Inputs: 8

Memory: 48 KB FLASH, 6KB SRAM

Connectivity: WiFi, Bluetooth

Microcontroller: ATSAMD21G18

Operating Voltage: 3.3V

Input Voltage: 5V

Memory: 256 KB Flash, 32 KB SRAM

 

imageimage
Nano 33 BLE - Giving away 5 for Project Proposals that use them!Nano 33 BLE Sense - Giving away 5 for Project Proposals that use them!

A Bluetooth 5 board that is perfect for wearables, motion tracking, environment monitoring, and other IoT sensing using its mesh networking support. The Nano 33 BLE (without headers) is Arduino’s 3.3V compatible board in the smallest available form factor: 45x18mm!

 

The Arduino Nano 33 BLE is an evolution of the traditional Arduino Nano, but featuring a lot more powerful processor, the nRF52840 from Nordic Semiconductors, a 32-bit ARMRegistered CortexTm-M4 CPU running at 64 MHz. This will allow you to make larger programs than with the Arduino Uno (it has 1MB of program memory, 32 times bigger), and with a lot more variables (the RAM is 128 times bigger). The main processor includes other amazing features like BluetoothRegistered pairing via NFC and ultra low power consumption modes. The Nano 33 BLE comes with a 9 axis inertial measurement unit (IMU) which means that it includes an accelerometer, a gyroscope, and a magnetometer with 3-axis resolution each. This makes the Nano 33 BLE the perfect choice for more advanced robotics experiments, exercise trackers, digital compasses, etc.

 

If you used Arduino Nano in your projects in the past, the Nano 33 BLE is a pin-equivalent substitute. Your code will still work, but remember, it operates at 3.3V. This means that you need to revise your original design in case it is not 3.3V compatible. Besides that, the main differences to the classic Nano are: a better processor, a micro-USB connector, and a 9 axis IMU.

 

The communications chipset on the Nano 33 BLE can be both a BLE and BluetoothRegistered client and host device. Something pretty unique in the world of microcontroller platforms.

The Nano 33 BLE Sense (without headers) is Arduino’s 3.3V AI enabled board in the smallest available form factor: 45x18mm! The Arduino Nano 33 BLE Sense is a completely new board on a well-known form factor. It comes with a series of embedded sensors:

 

  • 9 axis inertial sensor: what makes this board ideal for wearable devices
  • humidity, and temperature sensor: to get highly accurate measurements of the environmental conditions
  • microphone: to capture and analyse sound in real time
  • gesture, proximity, light color and light intensity sensor : estimate the room’s luminosity, but also whether someone is moving close to the board

 

The Arduino Nano 33 BLE Sense is an evolution of the traditional Arduino Nano, but featuring a lot more powerful processor, the nRF52840 from Nordic Semiconductors, a 32-bit ARMRegistered CortexTm-M4 CPU running at 64 MHz. This will allow you to make larger programs than with the Arduino Uno (it has 1MB of program memory, 32 times bigger), and with a lot more variables (the RAM is 128 times bigger). The main processor includes other amazing features like BluetoothRegistered pairing via NFC and ultra low power consumption modes.

 

Embedded Artificial Intelligence

 

The main feature of this board, besides the impressive selection of sensors, is the possibility of running Edge Computing applications (AI) on it using TinyML. You can create your machine learning models using TensorFlowTm Lite and upload them to your board using the Arduino IDE.

Connectivity: Bluetooth 5.0

Microcontroller: M4 Nordic nRF52840

Operating Voltage: 3.3V

Input Voltage: 5V

Memory: 1 MB Flash, 256 KB SRAM

Embedded 9V Axis IMU

Connectivity: Bluetooth 5.0

Microcontroller: M4 Nordic nRF52840

Operating Voltage: 3.3V

Input Voltage: 5V

Memory: 1 MB Flash, 256 KB SRAM

Embedded 9V Axis IMU

Embedded Environmental Sensors

Microphone

 

Starting March 21st:  

 

We'll Also Be Giving Away 20 Arduino Nano Boards for the first 20 people to submit Arduino Projects for Arduino Day! 

 

You can use whatever board you like but you'll need to tag your project blog NanoRamaCH!

 

 

 

In the comments below:  Let Us Know What Arduino Project You Are Planning on Doing for Arduino Day!

 

We'll be sending out a limited number of Nano boards for project proposals that use them!

  • bluetooth
  • arduino day 2020
  • arduino nano
  • nano every
  • nano iot
  • nano ble
  • nanoramach
  • featured_arduino
  • Arduino Day
  • nano ble sense
  • iot
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • tariq.ahmad
    tariq.ahmad over 6 years ago +11
    Originally, we were going to post winners of the Nano board giveaway the day before Arduino Day. However, due to the lock down in Chicago caused by the Covid-19 virus threat, the team has been working…
  • dubbie
    dubbie over 6 years ago +10
    Nanorama! I like it. I was only just saying a few minutes ago that Arduino Day has somehow passed me by in previous years, so this year I must do something. My idea, which I was thinking about only yesterday…
  • Sean_Miller
    Sean_Miller over 6 years ago +10
    I have a project for work that could use the Arduino Nano 33 IoT. Here is the potential project: The Shield of Compliance At my workplace, Engineers, technicians, supervisors, and interns are all haunted…
  • kmikemoo
    kmikemoo over 5 years ago in reply to eem011

    eem011  There are a few libraries already available to you for CRC.  https://github.com/vinmenn/Crc16      https://github.com/FrankBoesing/FastCRC

    If you're going to send the same data and you just want to verify that it hasn't been corripted... https://www.arduino.cc/en/Tutorial/LibraryExamples/EEPROMCrc

    I think one of the Simon Monk books also details how to do this, but I'm not sure which one (or where my copy is).

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • eem011
    eem011 over 5 years ago

    i need help on how to build a crc with Arduino.

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • pratyush_cetb
    pratyush_cetb over 6 years ago

    I would like build a health monitoring system for elderly people . This would a small air around the waist which would inflate only if a fall is detected. As there are million of cases of old people getting injured due to falling on the floor. All this could be done using accelerometer on arduino ble sense board . The microphone on the board could be used to detect specifc danger sound such or breaking or window or banging of door to detect intruder when they are home alone using machine learning packages such as tensorflow lite or arm-cmiss nn.

    All this along with monitoring vital health signs such temperature and the gesture control could be integrated with the home appliance to make it convient for the old age people.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • quinnzbellz
    quinnzbellz over 6 years ago

    I would like to build a device that turns off my 3d printer when it's done printing

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • soleakun
    soleakun over 6 years ago in reply to dubbie

    i use a used engine oil tank for it. it can take in 100kg food waste

     

    at home i use smaller one featured here Home Is Where the Hack Is Challenge, with Avnet Azure Sphere

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • robogary
    robogary over 6 years ago in reply to tariq.ahmad

    Thank you Tariq for all the extra efforts to keep the E14 community active and vital during all the disruptions.

    You are going way beyond expectations and I think I can speak for the community to say your efforts are appreciated.

     

    Arduino projects are fun to work on and an excuse to procrastinate on my hunney-do projects.

    • Cancel
    • Vote Up +9 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 6 years ago in reply to dixonselvan

    Thank you Dixon!

     

    I am safe, and for this week I finished working from home. I took two holiday days as I have to so dome homework image : Arduino nano study, articles, blogging for the IoT Challenge and other stuff.

     

    Enrico

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 6 years ago in reply to dixonselvan

    Very nice scenario, love it.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dixonselvan
    dixonselvan over 6 years ago in reply to balearicdynamics

    Happy Arduino Day!

     

    That is a nice video balearicdynamics. I can't wait to see what you innovate out of the AI-powered Arduino Nano 33 BLE Sense board.

     

    Stay safe image Hope you are doing good.

     

    Regards,

    Dixon Selvan

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dixonselvan
    dixonselvan over 6 years ago

    Thanks, tariq.ahmad for selecting and sending me an Arduino Nano 33 IoT Board! It was a pleasant surprise.

     

    I should be getting started with the project in some time.

     

    image

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • More
    • Cancel
>