Arduino
  • Products & Partners
  • More
Arduino
Documents Arduino Day 2020: NanoRama: We're Giving Away Different Nano Boards for Projects that Use Them!
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 24 Feb 2020 8:35 PM Date Created
  • Last Updated Last Updated: 25 Mar 2020 2:25 AM
  • Views 13789 views
  • Likes 20 likes
  • Comments 139 comments
Related
Recommended

Arduino Day 2020: NanoRama: We're Giving Away Different Nano Boards for Projects that Use Them!

image

Arduino Day 2020: NanoRama Giveaway

Quiz | NanoRama Giveaway | NanoRama Contest  | Fighting Germs Contest | Arduino Tutorials | Arduino Projects | Arduino Homepage image

 

In the comments below:  Let Us Know What Arduino Project You Are Planning on Doing for Arduino Day 2020!

 

We'll be sending out a limited number of Nano boards for project proposals that use them!

 

imageimageimage
Arduino is celebrating its 15th Birthday on March 21st, 2020!  We'll be sending out 25 Nano Boards (5 different Flavors) for project proposals that use them!Project14 will celebrate its 3rd Birthday with a NanoRama Celebration that begins the day before Arduino Day!  Help us celebrate by submitting an Arduino Project as a Birthday Present!Winners Announcement will be on Geek Pride Day on May 25th 2020.  It also happens to be the anniversary of the release of the first Star Wars movie.  A New Hope was released on May 25th, 1977!

 

This year, Arduino Day will be on March 21, 2020.  It will be their 15th birthday and we've decided to celebrate with NanoRama party!  We're kicking things off with Nano Giveaway, where we'll make Arduino Nano's new family of boards available on the community for the first time.  Say happy birthday to Arduino in the comments below, and let us know what Arduino project you plan on doing for Arduino's birthday. If your project idea includes one of the five Arduino Nano boards listed below, we'll send a the board of your choice for projects that use them.  The Nano boards that we are giving away are the Arduino Nano (Classic), Nano Every, Nano 33 IoT, Nano 33 BLE, and Nano BLE Sense.

 

Beginning on the 21st of March,  submit your Arduino Day project in Arduino Projects,  Arduino , your blog, or the NanoRama Birthday Special on  Project14 using the tag NanoRamaCH.  Your project can be a birthday present to celebrate Arduino's 15th birthday,  Project14's 3rd birthday, or both!  The Arduino Nano family is featured throughout Arduino Day and the upcoming NanoRama competition, however, you're also free to submit any Arduino based project, not just a Nano based project, if you'd prefer. The first 20 people to submit an Arduino project for Arduino Day win an Arduino Nano!  We'll also include cool Nano boards along with shopping cart as part of the prizes!  The upcoming NanoRama competition closes on May 14th with a winners announcement on May 25th.

 

Key Dates:

 

EventDate
NanoRama (3rd Anniversary of Project14) Launches:20th March 2020
Arduino Day 2020 (15th Anniversary of Arduino):21nd March 2020
Nano Winners Announced:23rd March 2020
NanoRama Closes:14th May 2020
NanoRama Winners Announced (42nd Anniversary of Star Wars):25th May 2020

 

 

We are giving away 25 Arduino Nano boards (5 of each) for Arduino Projects that Use them! 

 

Here are the Nano boards to choose from:

 

 

image

imageimage
Nano (Classic) - Giving away 5 for Project Proposals that use them!Nano Every - Giving away 5 for Project Proposals that use them!Nano 33 IoT - Giving away 5 for Project Proposals that use them!
Buy NowBuy Now
The Arduino Nano is a small, complete, and breadboard-friendly board based on the ATmega328P (Arduino Nano 3.x). It has more or less the same functionality of the Arduino Duemilanove, but in a different package. It lacks only a DC power jack, and works with a Mini-B USB cable instead of a standard one.

Perfect for everyday projects, this board is Arduino's 5 V Board in the smallest form factor available: 45x18mm!

 

The Arduino Nano Every is an evolution of the traditional Arduino Nano, but featuring a lot more powerful processor, the ATMega4809. This will allow you making larger programs than with the Arduino Uno (it has 50% more program memory), and with a lot more variables (the RAM is 200% bigger).

On-board WiFi and BluetoothRegistered connectivity using a u-blox module, the NINA-W10, a low power chipset operating in the 2.4GHz range. A cheap and easy point of entry for enabling IoT on existing devices (and creating new ones) or for designing pico-network applications. Can be used for applications such as building a sensor network connected to your router, or a BLE device sending data to a cellphone

 

Secure communication is ensured through the MicrochipRegistered ECC608 crypto chip. A 6 axis IMU, makes this board perfect for simple vibration alarm systems, pedometers, relative positioning of robots, etc.

Microcontroller: ATMEGA328

Operating Voltage: 5V

Analog Inputs: 8

Memory: 32 KB FLASH, 2KB  SRAM

Microcontroller: ATMEGA4809

Operating Voltage: 5V

Analog Inputs: 8

Memory: 48 KB FLASH, 6KB SRAM

Connectivity: WiFi, Bluetooth

Microcontroller: ATSAMD21G18

Operating Voltage: 3.3V

Input Voltage: 5V

Memory: 256 KB Flash, 32 KB SRAM

 

imageimage
Nano 33 BLE - Giving away 5 for Project Proposals that use them!Nano 33 BLE Sense - Giving away 5 for Project Proposals that use them!

A Bluetooth 5 board that is perfect for wearables, motion tracking, environment monitoring, and other IoT sensing using its mesh networking support. The Nano 33 BLE (without headers) is Arduino’s 3.3V compatible board in the smallest available form factor: 45x18mm!

 

The Arduino Nano 33 BLE is an evolution of the traditional Arduino Nano, but featuring a lot more powerful processor, the nRF52840 from Nordic Semiconductors, a 32-bit ARMRegistered CortexTm-M4 CPU running at 64 MHz. This will allow you to make larger programs than with the Arduino Uno (it has 1MB of program memory, 32 times bigger), and with a lot more variables (the RAM is 128 times bigger). The main processor includes other amazing features like BluetoothRegistered pairing via NFC and ultra low power consumption modes. The Nano 33 BLE comes with a 9 axis inertial measurement unit (IMU) which means that it includes an accelerometer, a gyroscope, and a magnetometer with 3-axis resolution each. This makes the Nano 33 BLE the perfect choice for more advanced robotics experiments, exercise trackers, digital compasses, etc.

 

If you used Arduino Nano in your projects in the past, the Nano 33 BLE is a pin-equivalent substitute. Your code will still work, but remember, it operates at 3.3V. This means that you need to revise your original design in case it is not 3.3V compatible. Besides that, the main differences to the classic Nano are: a better processor, a micro-USB connector, and a 9 axis IMU.

 

The communications chipset on the Nano 33 BLE can be both a BLE and BluetoothRegistered client and host device. Something pretty unique in the world of microcontroller platforms.

The Nano 33 BLE Sense (without headers) is Arduino’s 3.3V AI enabled board in the smallest available form factor: 45x18mm! The Arduino Nano 33 BLE Sense is a completely new board on a well-known form factor. It comes with a series of embedded sensors:

 

  • 9 axis inertial sensor: what makes this board ideal for wearable devices
  • humidity, and temperature sensor: to get highly accurate measurements of the environmental conditions
  • microphone: to capture and analyse sound in real time
  • gesture, proximity, light color and light intensity sensor : estimate the room’s luminosity, but also whether someone is moving close to the board

 

The Arduino Nano 33 BLE Sense is an evolution of the traditional Arduino Nano, but featuring a lot more powerful processor, the nRF52840 from Nordic Semiconductors, a 32-bit ARMRegistered CortexTm-M4 CPU running at 64 MHz. This will allow you to make larger programs than with the Arduino Uno (it has 1MB of program memory, 32 times bigger), and with a lot more variables (the RAM is 128 times bigger). The main processor includes other amazing features like BluetoothRegistered pairing via NFC and ultra low power consumption modes.

 

Embedded Artificial Intelligence

 

The main feature of this board, besides the impressive selection of sensors, is the possibility of running Edge Computing applications (AI) on it using TinyML. You can create your machine learning models using TensorFlowTm Lite and upload them to your board using the Arduino IDE.

Connectivity: Bluetooth 5.0

Microcontroller: M4 Nordic nRF52840

Operating Voltage: 3.3V

Input Voltage: 5V

Memory: 1 MB Flash, 256 KB SRAM

Embedded 9V Axis IMU

Connectivity: Bluetooth 5.0

Microcontroller: M4 Nordic nRF52840

Operating Voltage: 3.3V

Input Voltage: 5V

Memory: 1 MB Flash, 256 KB SRAM

Embedded 9V Axis IMU

Embedded Environmental Sensors

Microphone

 

Starting March 21st:  

 

We'll Also Be Giving Away 20 Arduino Nano Boards for the first 20 people to submit Arduino Projects for Arduino Day! 

 

You can use whatever board you like but you'll need to tag your project blog NanoRamaCH!

 

 

 

In the comments below:  Let Us Know What Arduino Project You Are Planning on Doing for Arduino Day!

 

We'll be sending out a limited number of Nano boards for project proposals that use them!

  • bluetooth
  • arduino day 2020
  • arduino nano
  • nano every
  • nano iot
  • nano ble
  • nanoramach
  • featured_arduino
  • Arduino Day
  • nano ble sense
  • iot
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • tariq.ahmad
    tariq.ahmad over 6 years ago +11
    Originally, we were going to post winners of the Nano board giveaway the day before Arduino Day. However, due to the lock down in Chicago caused by the Covid-19 virus threat, the team has been working…
  • dubbie
    dubbie over 6 years ago +10
    Nanorama! I like it. I was only just saying a few minutes ago that Arduino Day has somehow passed me by in previous years, so this year I must do something. My idea, which I was thinking about only yesterday…
  • Sean_Miller
    Sean_Miller over 6 years ago +10
    I have a project for work that could use the Arduino Nano 33 IoT. Here is the potential project: The Shield of Compliance At my workplace, Engineers, technicians, supervisors, and interns are all haunted…
  • jhartmusii
    jhartmusii over 6 years ago

    I would like to investigate using the Arduino Classic to decode Morse Code.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • soleakun
    soleakun over 6 years ago in reply to dubbie

    i updated my original post of an actual prototype that we are working. its capacity is 120kg

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • weiwei2
    weiwei2 over 6 years ago

    After researching around, i am still a bit confused about how to utilize the I2C on the Nano 33 IoT

    i am looking at this information

    https://www.arduino.cc/en/Guide/NANO33IoT , which lead us to this doc describing about adding other serial interface to it, however it only

    mention MKR1000 as an example within.

     

    However, i find my answer in this post. I can assign sercom4 to use i2c.  so i thought of sharing it to others

    https://github.com/ostaquet/Arduino-Nano-33-IoT-Ultimate-Guide

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • boublebonus
    boublebonus over 6 years ago

    I am planning to make a project for a smart house controlled by voice. You could turn on lights, access the internet(something similar to Alexa), turn on your PC etc. To control this system by voice commands I would train some kind of AI to better understand given commands and to improve itself over time. For this project the best board would be Arduino Nano 33 IoT.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dubbie
    dubbie over 6 years ago in reply to cs76

    Alessandro,

     

    I tried something like this using a PIC microprocessor a few years ago, but not in a track car, just my Ford Mondeo. I drove round a square block on my University which also had speed bumps. I could just about see the speed bumps and the corners but I really needed a more sensitive sensor. I look forward to seeing your track car version.

     

    Dubbie

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dubbie
    dubbie over 6 years ago in reply to kc8jrs

    kc8jrs,

     

    Sounds like a good project. I look forward to seeing more about it.

     

    Dubbie

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dubbie
    dubbie over 6 years ago in reply to soleakun

    Lea Kun So,

     

    I like your model of your composter. Very neat. How large is it?

     

    Dubbie

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dubbie
    dubbie over 6 years ago in reply to e14 Contributor

    Jason,

     

    I have not used the JST connectors so far but could be something I think of for the future. I do have some right angled headers (for some reason I cannot remember now) so might try these on a Nano as you have shown, as they do make quite a high item if inserted upright.

     

    Dubbie

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • cs76
    cs76 over 6 years ago

    I'd add a GPS receiver to the Arduino and an sd card to be realize a GPS based acquisition System.

    With this System it'll be possibile to monitor the performance of a vehicle on a specific track day.

     

    Thank you for considering this Project.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • kc8jrs
    kc8jrs over 6 years ago

    I would like to utilize the Nano BLE Sense to create a wearable (hat mounted) nature sensor that can gather data about the users environment, including exercise (accelerometer), light exposure (in lux and spectral ranges by time of day), and natural noise environment, tracking what I experience indoors as compared to outside, and see how it relates to health.

    I would also like to incorporate some LEDs and connect the BLE to a heart sensor that will send feedback on autonomic regulation, so the wearer can see a bar of light that is like the power a player may have in a video game. If your power is low, you need to calm down and self-regulate, so that you can perform better in real world activities.

     

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>