Arduino
  • Products & Partners
  • More
Arduino
Documents Arduino Day 2020: NanoRama: We're Giving Away Different Nano Boards for Projects that Use Them!
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 24 Feb 2020 8:35 PM Date Created
  • Last Updated Last Updated: 25 Mar 2020 2:25 AM
  • Views 13792 views
  • Likes 20 likes
  • Comments 139 comments
Related
Recommended

Arduino Day 2020: NanoRama: We're Giving Away Different Nano Boards for Projects that Use Them!

image

Arduino Day 2020: NanoRama Giveaway

Quiz | NanoRama Giveaway | NanoRama Contest  | Fighting Germs Contest | Arduino Tutorials | Arduino Projects | Arduino Homepage image

 

In the comments below:  Let Us Know What Arduino Project You Are Planning on Doing for Arduino Day 2020!

 

We'll be sending out a limited number of Nano boards for project proposals that use them!

 

imageimageimage
Arduino is celebrating its 15th Birthday on March 21st, 2020!  We'll be sending out 25 Nano Boards (5 different Flavors) for project proposals that use them!Project14 will celebrate its 3rd Birthday with a NanoRama Celebration that begins the day before Arduino Day!  Help us celebrate by submitting an Arduino Project as a Birthday Present!Winners Announcement will be on Geek Pride Day on May 25th 2020.  It also happens to be the anniversary of the release of the first Star Wars movie.  A New Hope was released on May 25th, 1977!

 

This year, Arduino Day will be on March 21, 2020.  It will be their 15th birthday and we've decided to celebrate with NanoRama party!  We're kicking things off with Nano Giveaway, where we'll make Arduino Nano's new family of boards available on the community for the first time.  Say happy birthday to Arduino in the comments below, and let us know what Arduino project you plan on doing for Arduino's birthday. If your project idea includes one of the five Arduino Nano boards listed below, we'll send a the board of your choice for projects that use them.  The Nano boards that we are giving away are the Arduino Nano (Classic), Nano Every, Nano 33 IoT, Nano 33 BLE, and Nano BLE Sense.

 

Beginning on the 21st of March,  submit your Arduino Day project in Arduino Projects,  Arduino , your blog, or the NanoRama Birthday Special on  Project14 using the tag NanoRamaCH.  Your project can be a birthday present to celebrate Arduino's 15th birthday,  Project14's 3rd birthday, or both!  The Arduino Nano family is featured throughout Arduino Day and the upcoming NanoRama competition, however, you're also free to submit any Arduino based project, not just a Nano based project, if you'd prefer. The first 20 people to submit an Arduino project for Arduino Day win an Arduino Nano!  We'll also include cool Nano boards along with shopping cart as part of the prizes!  The upcoming NanoRama competition closes on May 14th with a winners announcement on May 25th.

 

Key Dates:

 

EventDate
NanoRama (3rd Anniversary of Project14) Launches:20th March 2020
Arduino Day 2020 (15th Anniversary of Arduino):21nd March 2020
Nano Winners Announced:23rd March 2020
NanoRama Closes:14th May 2020
NanoRama Winners Announced (42nd Anniversary of Star Wars):25th May 2020

 

 

We are giving away 25 Arduino Nano boards (5 of each) for Arduino Projects that Use them! 

 

Here are the Nano boards to choose from:

 

 

image

imageimage
Nano (Classic) - Giving away 5 for Project Proposals that use them!Nano Every - Giving away 5 for Project Proposals that use them!Nano 33 IoT - Giving away 5 for Project Proposals that use them!
Buy NowBuy Now
The Arduino Nano is a small, complete, and breadboard-friendly board based on the ATmega328P (Arduino Nano 3.x). It has more or less the same functionality of the Arduino Duemilanove, but in a different package. It lacks only a DC power jack, and works with a Mini-B USB cable instead of a standard one.

Perfect for everyday projects, this board is Arduino's 5 V Board in the smallest form factor available: 45x18mm!

 

The Arduino Nano Every is an evolution of the traditional Arduino Nano, but featuring a lot more powerful processor, the ATMega4809. This will allow you making larger programs than with the Arduino Uno (it has 50% more program memory), and with a lot more variables (the RAM is 200% bigger).

On-board WiFi and BluetoothRegistered connectivity using a u-blox module, the NINA-W10, a low power chipset operating in the 2.4GHz range. A cheap and easy point of entry for enabling IoT on existing devices (and creating new ones) or for designing pico-network applications. Can be used for applications such as building a sensor network connected to your router, or a BLE device sending data to a cellphone

 

Secure communication is ensured through the MicrochipRegistered ECC608 crypto chip. A 6 axis IMU, makes this board perfect for simple vibration alarm systems, pedometers, relative positioning of robots, etc.

Microcontroller: ATMEGA328

Operating Voltage: 5V

Analog Inputs: 8

Memory: 32 KB FLASH, 2KB  SRAM

Microcontroller: ATMEGA4809

Operating Voltage: 5V

Analog Inputs: 8

Memory: 48 KB FLASH, 6KB SRAM

Connectivity: WiFi, Bluetooth

Microcontroller: ATSAMD21G18

Operating Voltage: 3.3V

Input Voltage: 5V

Memory: 256 KB Flash, 32 KB SRAM

 

imageimage
Nano 33 BLE - Giving away 5 for Project Proposals that use them!Nano 33 BLE Sense - Giving away 5 for Project Proposals that use them!

A Bluetooth 5 board that is perfect for wearables, motion tracking, environment monitoring, and other IoT sensing using its mesh networking support. The Nano 33 BLE (without headers) is Arduino’s 3.3V compatible board in the smallest available form factor: 45x18mm!

 

The Arduino Nano 33 BLE is an evolution of the traditional Arduino Nano, but featuring a lot more powerful processor, the nRF52840 from Nordic Semiconductors, a 32-bit ARMRegistered CortexTm-M4 CPU running at 64 MHz. This will allow you to make larger programs than with the Arduino Uno (it has 1MB of program memory, 32 times bigger), and with a lot more variables (the RAM is 128 times bigger). The main processor includes other amazing features like BluetoothRegistered pairing via NFC and ultra low power consumption modes. The Nano 33 BLE comes with a 9 axis inertial measurement unit (IMU) which means that it includes an accelerometer, a gyroscope, and a magnetometer with 3-axis resolution each. This makes the Nano 33 BLE the perfect choice for more advanced robotics experiments, exercise trackers, digital compasses, etc.

 

If you used Arduino Nano in your projects in the past, the Nano 33 BLE is a pin-equivalent substitute. Your code will still work, but remember, it operates at 3.3V. This means that you need to revise your original design in case it is not 3.3V compatible. Besides that, the main differences to the classic Nano are: a better processor, a micro-USB connector, and a 9 axis IMU.

 

The communications chipset on the Nano 33 BLE can be both a BLE and BluetoothRegistered client and host device. Something pretty unique in the world of microcontroller platforms.

The Nano 33 BLE Sense (without headers) is Arduino’s 3.3V AI enabled board in the smallest available form factor: 45x18mm! The Arduino Nano 33 BLE Sense is a completely new board on a well-known form factor. It comes with a series of embedded sensors:

 

  • 9 axis inertial sensor: what makes this board ideal for wearable devices
  • humidity, and temperature sensor: to get highly accurate measurements of the environmental conditions
  • microphone: to capture and analyse sound in real time
  • gesture, proximity, light color and light intensity sensor : estimate the room’s luminosity, but also whether someone is moving close to the board

 

The Arduino Nano 33 BLE Sense is an evolution of the traditional Arduino Nano, but featuring a lot more powerful processor, the nRF52840 from Nordic Semiconductors, a 32-bit ARMRegistered CortexTm-M4 CPU running at 64 MHz. This will allow you to make larger programs than with the Arduino Uno (it has 1MB of program memory, 32 times bigger), and with a lot more variables (the RAM is 128 times bigger). The main processor includes other amazing features like BluetoothRegistered pairing via NFC and ultra low power consumption modes.

 

Embedded Artificial Intelligence

 

The main feature of this board, besides the impressive selection of sensors, is the possibility of running Edge Computing applications (AI) on it using TinyML. You can create your machine learning models using TensorFlowTm Lite and upload them to your board using the Arduino IDE.

Connectivity: Bluetooth 5.0

Microcontroller: M4 Nordic nRF52840

Operating Voltage: 3.3V

Input Voltage: 5V

Memory: 1 MB Flash, 256 KB SRAM

Embedded 9V Axis IMU

Connectivity: Bluetooth 5.0

Microcontroller: M4 Nordic nRF52840

Operating Voltage: 3.3V

Input Voltage: 5V

Memory: 1 MB Flash, 256 KB SRAM

Embedded 9V Axis IMU

Embedded Environmental Sensors

Microphone

 

Starting March 21st:  

 

We'll Also Be Giving Away 20 Arduino Nano Boards for the first 20 people to submit Arduino Projects for Arduino Day! 

 

You can use whatever board you like but you'll need to tag your project blog NanoRamaCH!

 

 

 

In the comments below:  Let Us Know What Arduino Project You Are Planning on Doing for Arduino Day!

 

We'll be sending out a limited number of Nano boards for project proposals that use them!

  • bluetooth
  • arduino day 2020
  • arduino nano
  • nano every
  • nano iot
  • nano ble
  • nanoramach
  • featured_arduino
  • Arduino Day
  • nano ble sense
  • iot
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • tariq.ahmad
    tariq.ahmad over 6 years ago +11
    Originally, we were going to post winners of the Nano board giveaway the day before Arduino Day. However, due to the lock down in Chicago caused by the Covid-19 virus threat, the team has been working…
  • dubbie
    dubbie over 6 years ago +10
    Nanorama! I like it. I was only just saying a few minutes ago that Arduino Day has somehow passed me by in previous years, so this year I must do something. My idea, which I was thinking about only yesterday…
  • Sean_Miller
    Sean_Miller over 6 years ago +10
    I have a project for work that could use the Arduino Nano 33 IoT. Here is the potential project: The Shield of Compliance At my workplace, Engineers, technicians, supervisors, and interns are all haunted…
  • dubbie
    dubbie over 6 years ago in reply to redcharly

    Carlo,

     

    It's different. I think I might prefer birdsong and wind rustling in the trees though. More relaxing.

     

    Dubbie

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • hyperspeeed
    hyperspeeed over 6 years ago

    I want to create a simple IoT network. That's why I chose the Arduino Nano 33 IoT. The data will be exchanged via WiFi, that's why I need a WiFi compatible board and the Nano IoT supports it next to Bluetooth, which I also have some plans for.

    This is will be done for research and we (some colleagues and me) will write a paper about that. We are working at the Chair of Computer Engineering at a German university.

    This would really help us out and maybe help the world with some more knowledge image

     

    Nico

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ljakes
    ljakes over 6 years ago in reply to clem57

    The system includes a wind speed, wind direction and rain collector which needs to be in a relative high open area where it can receive unobstructed wind and rain.  Those parts work fine where I have it mounted.  There is also a solar cell that faces the sun to the south.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 6 years ago in reply to ljakes

    Um! Why not place the current system in the shade?

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ljakes
    ljakes over 6 years ago

    Happy birthday Arduino

     

    I run a weather station using an AcuRite 5 in 1 System.  I report readings to Weather Underground. and Citizen Weather Observer Program. I use the Weewx software running on a Raspberry Pi.  However the AcuRite system has a design problem in that when the direct sunlight is shining on the white plastic housing it artificially raises the temperature and decreases the humidity readings.  AcuRite includes an aspirating fan running off a solar panel to compensate for the errors but this hardly works.  The AcuRite System also does not include a light intensity sensor. The temperature readings can still be 5 to 8 degrees high.  I would like to use the Nano 33 BLE Sense board placed in the shade to take temperature, humidity,  and light intensity readings.  I will integrate these readings into the Weewx and substitute them for the innacurate AcuRite readings and publish the more accurate results.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • redcharly
    redcharly over 6 years ago

    For some time I have been interested in audio with Arduino and I have been trying to create an ambient music generator. Look for example in this bad (very very bad) video how the audio reproduced changes according to the value of the sensors, I can switch from the relaxing sound produced by the frogs (:)) to that of an evening enlivened by crickets, only by acting on one of the three sensors installed, the brightness one. Just obscure the photoresistor to simulate a night environment and the sound produced changes.

    Obviously with 3 different sensors installed I can manage up to 8 different sounds.

    Would these brand new and beautiful Arduino Nano make me get at least the same performance? I'd be curious to try.

     

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jomoenginer
    jomoenginer over 6 years ago in reply to jomoenginer

    Not that my idea would be chosen, but I have already purchased an Arduino 33 BLE Sense board and I have a Nano Classic that was sent to me previously, so I will not need a board for this.  

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • pvalyk
    pvalyk over 6 years ago

    I would upgrade my Balcony plant watering system, currently made with an arduino uno.

     

    With that occasion, I would add a micro server on the board, integrate it with my home automation system and also I would like to test the AI capabilities of the Sense board.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • bernhardmayer
    bernhardmayer over 6 years ago

    Good morning.

     

    I would like to update my HighPowerMotorFeatherWing ( HighPowerMotorFeatherWing - a motor driver board for the JECCbot mini and other robots  ) to suit the Arduino Nano and then use an Arduino Nano 33 IoT to show how to control a robot using Bluetooth and WiFi.

     

    Bernhard

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • chamal82
    chamal82 over 6 years ago

    Using Arduino Nano 33 BLE Sense, I am going to build a portable language translator.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>