Arduino
  • Products & Partners
  • More
Arduino
Documents Arduino Day 2020: NanoRama: We're Giving Away Different Nano Boards for Projects that Use Them!
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 24 Feb 2020 8:35 PM Date Created
  • Last Updated Last Updated: 25 Mar 2020 2:25 AM
  • Views 13794 views
  • Likes 20 likes
  • Comments 139 comments
Related
Recommended

Arduino Day 2020: NanoRama: We're Giving Away Different Nano Boards for Projects that Use Them!

image

Arduino Day 2020: NanoRama Giveaway

Quiz | NanoRama Giveaway | NanoRama Contest  | Fighting Germs Contest | Arduino Tutorials | Arduino Projects | Arduino Homepage image

 

In the comments below:  Let Us Know What Arduino Project You Are Planning on Doing for Arduino Day 2020!

 

We'll be sending out a limited number of Nano boards for project proposals that use them!

 

imageimageimage
Arduino is celebrating its 15th Birthday on March 21st, 2020!  We'll be sending out 25 Nano Boards (5 different Flavors) for project proposals that use them!Project14 will celebrate its 3rd Birthday with a NanoRama Celebration that begins the day before Arduino Day!  Help us celebrate by submitting an Arduino Project as a Birthday Present!Winners Announcement will be on Geek Pride Day on May 25th 2020.  It also happens to be the anniversary of the release of the first Star Wars movie.  A New Hope was released on May 25th, 1977!

 

This year, Arduino Day will be on March 21, 2020.  It will be their 15th birthday and we've decided to celebrate with NanoRama party!  We're kicking things off with Nano Giveaway, where we'll make Arduino Nano's new family of boards available on the community for the first time.  Say happy birthday to Arduino in the comments below, and let us know what Arduino project you plan on doing for Arduino's birthday. If your project idea includes one of the five Arduino Nano boards listed below, we'll send a the board of your choice for projects that use them.  The Nano boards that we are giving away are the Arduino Nano (Classic), Nano Every, Nano 33 IoT, Nano 33 BLE, and Nano BLE Sense.

 

Beginning on the 21st of March,  submit your Arduino Day project in Arduino Projects,  Arduino , your blog, or the NanoRama Birthday Special on  Project14 using the tag NanoRamaCH.  Your project can be a birthday present to celebrate Arduino's 15th birthday,  Project14's 3rd birthday, or both!  The Arduino Nano family is featured throughout Arduino Day and the upcoming NanoRama competition, however, you're also free to submit any Arduino based project, not just a Nano based project, if you'd prefer. The first 20 people to submit an Arduino project for Arduino Day win an Arduino Nano!  We'll also include cool Nano boards along with shopping cart as part of the prizes!  The upcoming NanoRama competition closes on May 14th with a winners announcement on May 25th.

 

Key Dates:

 

EventDate
NanoRama (3rd Anniversary of Project14) Launches:20th March 2020
Arduino Day 2020 (15th Anniversary of Arduino):21nd March 2020
Nano Winners Announced:23rd March 2020
NanoRama Closes:14th May 2020
NanoRama Winners Announced (42nd Anniversary of Star Wars):25th May 2020

 

 

We are giving away 25 Arduino Nano boards (5 of each) for Arduino Projects that Use them! 

 

Here are the Nano boards to choose from:

 

 

image

imageimage
Nano (Classic) - Giving away 5 for Project Proposals that use them!Nano Every - Giving away 5 for Project Proposals that use them!Nano 33 IoT - Giving away 5 for Project Proposals that use them!
Buy NowBuy Now
The Arduino Nano is a small, complete, and breadboard-friendly board based on the ATmega328P (Arduino Nano 3.x). It has more or less the same functionality of the Arduino Duemilanove, but in a different package. It lacks only a DC power jack, and works with a Mini-B USB cable instead of a standard one.

Perfect for everyday projects, this board is Arduino's 5 V Board in the smallest form factor available: 45x18mm!

 

The Arduino Nano Every is an evolution of the traditional Arduino Nano, but featuring a lot more powerful processor, the ATMega4809. This will allow you making larger programs than with the Arduino Uno (it has 50% more program memory), and with a lot more variables (the RAM is 200% bigger).

On-board WiFi and BluetoothRegistered connectivity using a u-blox module, the NINA-W10, a low power chipset operating in the 2.4GHz range. A cheap and easy point of entry for enabling IoT on existing devices (and creating new ones) or for designing pico-network applications. Can be used for applications such as building a sensor network connected to your router, or a BLE device sending data to a cellphone

 

Secure communication is ensured through the MicrochipRegistered ECC608 crypto chip. A 6 axis IMU, makes this board perfect for simple vibration alarm systems, pedometers, relative positioning of robots, etc.

Microcontroller: ATMEGA328

Operating Voltage: 5V

Analog Inputs: 8

Memory: 32 KB FLASH, 2KB  SRAM

Microcontroller: ATMEGA4809

Operating Voltage: 5V

Analog Inputs: 8

Memory: 48 KB FLASH, 6KB SRAM

Connectivity: WiFi, Bluetooth

Microcontroller: ATSAMD21G18

Operating Voltage: 3.3V

Input Voltage: 5V

Memory: 256 KB Flash, 32 KB SRAM

 

imageimage
Nano 33 BLE - Giving away 5 for Project Proposals that use them!Nano 33 BLE Sense - Giving away 5 for Project Proposals that use them!

A Bluetooth 5 board that is perfect for wearables, motion tracking, environment monitoring, and other IoT sensing using its mesh networking support. The Nano 33 BLE (without headers) is Arduino’s 3.3V compatible board in the smallest available form factor: 45x18mm!

 

The Arduino Nano 33 BLE is an evolution of the traditional Arduino Nano, but featuring a lot more powerful processor, the nRF52840 from Nordic Semiconductors, a 32-bit ARMRegistered CortexTm-M4 CPU running at 64 MHz. This will allow you to make larger programs than with the Arduino Uno (it has 1MB of program memory, 32 times bigger), and with a lot more variables (the RAM is 128 times bigger). The main processor includes other amazing features like BluetoothRegistered pairing via NFC and ultra low power consumption modes. The Nano 33 BLE comes with a 9 axis inertial measurement unit (IMU) which means that it includes an accelerometer, a gyroscope, and a magnetometer with 3-axis resolution each. This makes the Nano 33 BLE the perfect choice for more advanced robotics experiments, exercise trackers, digital compasses, etc.

 

If you used Arduino Nano in your projects in the past, the Nano 33 BLE is a pin-equivalent substitute. Your code will still work, but remember, it operates at 3.3V. This means that you need to revise your original design in case it is not 3.3V compatible. Besides that, the main differences to the classic Nano are: a better processor, a micro-USB connector, and a 9 axis IMU.

 

The communications chipset on the Nano 33 BLE can be both a BLE and BluetoothRegistered client and host device. Something pretty unique in the world of microcontroller platforms.

The Nano 33 BLE Sense (without headers) is Arduino’s 3.3V AI enabled board in the smallest available form factor: 45x18mm! The Arduino Nano 33 BLE Sense is a completely new board on a well-known form factor. It comes with a series of embedded sensors:

 

  • 9 axis inertial sensor: what makes this board ideal for wearable devices
  • humidity, and temperature sensor: to get highly accurate measurements of the environmental conditions
  • microphone: to capture and analyse sound in real time
  • gesture, proximity, light color and light intensity sensor : estimate the room’s luminosity, but also whether someone is moving close to the board

 

The Arduino Nano 33 BLE Sense is an evolution of the traditional Arduino Nano, but featuring a lot more powerful processor, the nRF52840 from Nordic Semiconductors, a 32-bit ARMRegistered CortexTm-M4 CPU running at 64 MHz. This will allow you to make larger programs than with the Arduino Uno (it has 1MB of program memory, 32 times bigger), and with a lot more variables (the RAM is 128 times bigger). The main processor includes other amazing features like BluetoothRegistered pairing via NFC and ultra low power consumption modes.

 

Embedded Artificial Intelligence

 

The main feature of this board, besides the impressive selection of sensors, is the possibility of running Edge Computing applications (AI) on it using TinyML. You can create your machine learning models using TensorFlowTm Lite and upload them to your board using the Arduino IDE.

Connectivity: Bluetooth 5.0

Microcontroller: M4 Nordic nRF52840

Operating Voltage: 3.3V

Input Voltage: 5V

Memory: 1 MB Flash, 256 KB SRAM

Embedded 9V Axis IMU

Connectivity: Bluetooth 5.0

Microcontroller: M4 Nordic nRF52840

Operating Voltage: 3.3V

Input Voltage: 5V

Memory: 1 MB Flash, 256 KB SRAM

Embedded 9V Axis IMU

Embedded Environmental Sensors

Microphone

 

Starting March 21st:  

 

We'll Also Be Giving Away 20 Arduino Nano Boards for the first 20 people to submit Arduino Projects for Arduino Day! 

 

You can use whatever board you like but you'll need to tag your project blog NanoRamaCH!

 

 

 

In the comments below:  Let Us Know What Arduino Project You Are Planning on Doing for Arduino Day!

 

We'll be sending out a limited number of Nano boards for project proposals that use them!

  • bluetooth
  • arduino day 2020
  • arduino nano
  • nano every
  • nano iot
  • nano ble
  • nanoramach
  • featured_arduino
  • Arduino Day
  • nano ble sense
  • iot
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • tariq.ahmad
    tariq.ahmad over 6 years ago +11
    Originally, we were going to post winners of the Nano board giveaway the day before Arduino Day. However, due to the lock down in Chicago caused by the Covid-19 virus threat, the team has been working…
  • dubbie
    dubbie over 6 years ago +10
    Nanorama! I like it. I was only just saying a few minutes ago that Arduino Day has somehow passed me by in previous years, so this year I must do something. My idea, which I was thinking about only yesterday…
  • Sean_Miller
    Sean_Miller over 6 years ago +10
    I have a project for work that could use the Arduino Nano 33 IoT. Here is the potential project: The Shield of Compliance At my workplace, Engineers, technicians, supervisors, and interns are all haunted…
  • dubbie
    dubbie over 6 years ago in reply to luislabmo

    Luis,

     

    You could always try going for 16 segment displays (if they still exist). That could be fun to see as you get much better text representation.

     

    Dubbie

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • robogary
    robogary over 6 years ago in reply to e14 Contributor

    Hi Jason Lee ( and also Dubbie)

     

    My first project or two, I soldered in the Arduino Nanos into my breadboard prototypes and found doing that was a big disadvantage.

    In the whirlwind of new project or idea, I couldnt borrow a Nano from another project that was soldered in.

    I also couldn't remove the Nano from the project for quick troubleshooting or replacement.

     

    I have 2 solutions for Arduino Nano sockets:

    1) The cheapest is to order the same .1 X .1 header pin connectors the Arduino Uno uses. They come is lengths of 40 pins. I cut them to length, and put on the Nano pins when soldering to keep alignment. After soldering, the Nano can be socketed this way for less than 10 cents US each.  

    For example:  https://www.ebay.com/itm/20-PCS-Female-40pin-2-54mm-Header-Socket-Row-Strip-PCB-Connector-For-Arduino/264241393452?hash=…

    This is an Arduino Nano Project I socketed this way. This is a light organ. It inputs audio into a graphic equalizer IC , the Arduino Nano scans the thru the multiplexed different frequency bands of audio content

    decoded,turns on an output based on the volume of each band exceeding an internal threshold. Each output is a 10 amp MOSFET, altho there are 7 output bands and MOSFETS, the circuit board is wired for about 20amps steady state amps. This little board drives multiple banks of 12V LED strings, a real light show. This solution is good for projects that arent mobile.

    image

     

    2) I really like using these terminal board with Arduino Nano socket for robots, costuming & props, projects that get exhibited alot.

    For example:

    https://www.ebay.com/itm/Nano-Terminal-Adapter-for-the-Arduino-Nano-AVR-ATMEGA328P-AU-Module-Board-DIY/263082889276?hash…

    These are not as inexpensive as the header pins solution, but are still inexpensive, alot sturdier than header pins, easily reused for multiple projects. 

    image

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • redcharly
    redcharly over 6 years ago in reply to redcharly

    Hi, yesterday I made the project I was talking about, but I did it using an Arduino Mega, I would like to have one of these splendid Arduino Nano to try to make something smaller. We hope to be among the chosen ones !! it's great to hear the sounds (waves, birds, wind, etc.) change based on the environmental conditions in my room.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • luislabmo
    luislabmo over 6 years ago

    I'd like to build a simple project for the Arduino that I'd love to share with the community (schematics and source code). I want to use an Arduino Nano Every (other types may work too) to drive 7-segment LED displays. The source code will accommodate any kind of display CC (Common Cathode) or CA (Common Anode) with any amount digits without requiring any change to the code. I'm planning to demo 4-digit displays (CC and CA) and single-digit displays daisychained together.

     

    Luis

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • kbenora
    kbenora over 6 years ago in reply to dubbie

    Yes exactly! And might as well put a speaker in there to play a different tone for each drawer that's opened while we're at it.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dubbie
    dubbie over 6 years ago in reply to e14 Contributor

    Jason,

     

    That's a very interesting hand. Are those servo motors buried in the hand somewhere? It would be good to know more about the hand construction as it seems to work very well.

     

    I too am just about to start soldering a Nano directly to a PCB (well, after I've made the PCB anyway) and as you say, the cheap clones are cheap so I probably will not use sockets. It will be interesting to see your Nano based project.

     

    Dubbie

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 6 years ago

    Happy birthday Arduino!

     

    I've designed a PCB to use the new Arduino Nanos to use in my robotics project, ARX Hand Project. But due to budget constraints, I can't quite commit to soldering one to directly to the PCB! >_<

     

    So far, I've been using the cheap Nanos from China, so it would be amazing if I could get a Nano 33 BLE to solder onto my PCB to use with my project. I would be very keen to learn to use bluetooth to communicate with my robotic hand and control it wirelessly. I could also try to learn implementing machine learning to help improve the reliability and awareness of my robotic hand which would really cool!

     

    Here's a link to a video of my project:

    https://youtu.be/k1Z3GM1UHRM

     

    Unfortunately I don't quite have the time to write up a project page yet due to some issues with health and studies, but it would be of great value to receive the new Arduino Nanos!

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dubbie
    dubbie over 6 years ago in reply to kbenora

    Kelden,

     

    Sounds like a fun project. Wave your hand in front of the draws and they could all be opening and closing. A bit like conducting an orchestra.

     

    Dubbie

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • kbenora
    kbenora over 6 years ago

    Happy birthday Arduino and Project14!

     

    I plan to make a simple but fun project for organizing arduino parts and components that would be controlled by a Nano Every board. Here’s the gist: I would like my small drawers of resistors and switches and such to automatically open and light up when my hand gets close enough. I will embed proximity sensors, servo actuators, and LED’s into 3D printed drawers with labels. An initial prototype of this would only include a handful of automated drawers and later designs will have more features such as detection of parts running out and if the matrix of drawers is very large, a part search function to help point out where the desired components can be found. Many options for going about adding the latter functions so it will be fun finding out which method works best. Hope it turns out and thanks for hosting this Nano celebration!


    -Kelden

     

    #NanoRamaCH

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • weiwei2
    weiwei2 over 6 years ago in reply to weiwei2

    i have a doctorate lecturer friend carrying out research in MOx sensing, according to him, MOX used heater to optimize sensing detection thus they need to operate at high temperature and not suitable for application like oil and gas. Although the ZMOD4450 does have heater inside the chip and is not for O&G, IDT also has other gas sensor that among other detect flamable gas, so it is and interesting topic to me (remind me of the MEMS quiz i take lately that goes into some technology details)

    image

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>