Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MiniZed Hardware Design Macros missing from xparameters.h when using AXI Timer
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 1 reply
  • Subscribers 331 subscribers
  • Views 2625 views
  • Users 0 members are here
  • axi timer
  • minized
Related

Macros missing from xparameters.h when using AXI Timer

LTxAlves
LTxAlves over 3 years ago

Hi!

I needed to use to PWM from the AXI Timer IP. I designed a simple block diagram, exported the hardware to work on it on SDK. Looking at the example given for the PWM using the Timer IP, SDK pointed out some errors with the code. I fixed some by modifying the BSP settings and changing them back. However, I noticed some MACRO definitions were missing in the xparameters.h file, which in turn SDK points out as errors and I have no idea if I can just copy those from another xparameters.h file or what to change in my code/bock design so those definitions appear on my current file.

The block design:

The code:

/******************************************************************************
*
* Copyright (C) 2018 Xilinx, Inc.  All rights reserved.
*
* Permission is hereby granted, free of charge, to any person obtaining a copy
* of this software and associated documentation files (the "Software"), to deal
* in the Software without restriction, including without limitation the rights
* to use, copy, modify, merge, publish, distribute, sublicense, and/or sell
* copies of the Software, and to permit persons to whom the Software is
* furnished to do so, subject to the following conditions:
*
* The above copyright notice and this permission notice shall be included in
* all copies or substantial portions of the Software.
*
* THE SOFTWARE IS PROVIDED "AS IS", WITHOUT WARRANTY OF ANY KIND, EXPRESS OR
* IMPLIED, INCLUDING BUT NOT LIMITED TO THE WARRANTIES OF MERCHANTABILITY,
* FITNESS FOR A PARTICULAR PURPOSE AND NONINFRINGEMENT. IN NO EVENT SHALL
* XILINX  BE LIABLE FOR ANY CLAIM, DAMAGES OR OTHER LIABILITY,
* WHETHER IN AN ACTION OF CONTRACT, TORT OR OTHERWISE, ARISING FROM, OUT OF
* OR IN CONNECTION WITH THE SOFTWARE OR THE USE OR OTHER DEALINGS IN THE
* SOFTWARE.
*
* Except as contained in this notice, the name of the Xilinx shall not be used
* in advertising or otherwise to promote the sale, use or other dealings in
* this Software without prior written authorization from Xilinx.
*
******************************************************************************/
/*****************************************************************************/
/**
* @file  xtmrctr_pwm_example.c
*
* This file contains a design example using the timer counter driver
* and hardware device using interrupt mode. The example demonstrates
* the use of PWM feature of axi timers. PWM is configured to operate at specific
* duty cycle and after every N cycles the duty cycle is incremented until a
* specific duty cycle is achieved. No software validation of duty cycle is
* undergone in the example.
*
* This example assumes that the interrupt controller is also present as a part
* of the system.
*
*
*
*
* <pre>
* MODIFICATION HISTORY:
*
* Ver   Who  Date	 Changes
* ----- ---- -------- -----------------------------------------------
* 1.00b cjp  03/28/18 First release
*</pre>
******************************************************************************/

/***************************** Include Files *********************************/
#include "xtmrctr.h"
#include "xparameters.h"
#include "xil_exception.h"

#ifdef XPAR_INTC_0_DEVICE_ID
#include "xintc.h"
#include <stdio.h>
#else
#include "xscugic.h"
#include "xil_printf.h"
#endif

/************************** Constant Definitions *****************************/
/*
 * The following constants map to the XPAR parameters created in the
 * xparameters.h file. They are only defined here such that a user can easily
 * change all the needed parameters in one place.
 */
#define TMRCTR_DEVICE_ID        XPAR_TMRCTR_0_DEVICE_ID

#ifdef __MICROBLAZE__
#define TMRCTR_INTERRUPT_ID     XPAR_INTC_0_TMRCTR_0_VEC_ID
#else
#define TMRCTR_INTERRUPT_ID     XPAR_FABRIC_TMRCTR_0_VEC_ID
#endif

#ifdef XPAR_INTC_0_DEVICE_ID
#define INTC_DEVICE_ID          XPAR_INTC_0_DEVICE_ID
#define INTC                    XIntc
#define INTC_HANDLER            XIntc_InterruptHandler
#else
#define INTC_DEVICE_ID          XPAR_SCUGIC_SINGLE_DEVICE_ID
#define INTC                    XScuGic
#define INTC_HANDLER            XScuGic_InterruptHandler
#endif /* XPAR_INTC_0_DEVICE_ID */

#define PWM_PERIOD              500000000    /* PWM period in (500 ms) */
#define TMRCTR_0                0            /* Timer 0 ID */
#define TMRCTR_1                1            /* Timer 1 ID */
#define CYCLE_PER_DUTYCYCLE     10           /* Clock cycles per duty cycle */
#define MAX_DUTYCYCLE           100          /* Max duty cycle */
#define DUTYCYCLE_DIVISOR       4            /* Duty cycle Divisor */
#define WAIT_COUNT              PWM_PERIOD   /* Interrupt wait counter */

/**************************** Type Definitions *******************************/

/***************** Macros (Inline Functions) Definitions *********************/

/************************** Function Prototypes ******************************/
int TmrCtrPwmExample(INTC *IntcInstancePtr, XTmrCtr *InstancePtr, u16 DeviceId,
								u16 IntrId);
static void TimerCounterHandler(void *CallBackRef, u8 TmrCtrNumber);
static int TmrCtrSetupIntrSystem(INTC *IntcInstancePtr, XTmrCtr *InstancePtr,
						u16 DeviceId, u16 IntrId);
static void TmrCtrDisableIntr(INTC *IntcInstancePtr, u16 IntrId);

/************************** Variable Definitions *****************************/
INTC InterruptController;  /* The instance of the Interrupt Controller */
XTmrCtr TimerCounterInst;  /* The instance of the Timer Counter */

/*
 * The following variables are shared between non-interrupt processing and
 * interrupt processing such that they must be global.
 */
static int   PeriodTimerHit = FALSE;
static int   HighTimerHit = FALSE;

/*****************************************************************************/
/**
* This function is the main function of the Tmrctr PWM example.
*
* @param	None.
*
* @return	XST_SUCCESS to indicate success, else XST_FAILURE to indicate a
*		Failure.
*
* @note		None.
*
******************************************************************************/
int main(void)
{
	int Status;

	/* Run the Timer Counter PWM example */
	Status = TmrCtrPwmExample(&InterruptController, &TimerCounterInst,
				  TMRCTR_DEVICE_ID, TMRCTR_INTERRUPT_ID);
	if (Status != XST_SUCCESS) {
		xil_printf("Tmrctr PWM Example Failed\r\n");
		return XST_FAILURE;
	}

	xil_printf("Successfully ran Tmrctr PWM Example\r\n");
	return XST_SUCCESS;
}

/*****************************************************************************/
/**
* This function demonstrates the use of tmrctr PWM APIs.
*
* @param	IntcInstancePtr is a pointer to the Interrupt Controller
*		driver Instance
* @param	TmrCtrInstancePtr is a pointer to the XTmrCtr driver Instance
* @param	DeviceId is the XPAR_<TmrCtr_instance>_DEVICE_ID value from
*		xparameters.h
* @param	IntrId is XPAR_<INTC_instance>_<TmrCtr_instance>_INTERRUPT_INTR
*		value from xparameters.h
*
* @return	XST_SUCCESS if the Test is successful, otherwise XST_FAILURE
*
* @note		none.
*
*****************************************************************************/
int TmrCtrPwmExample(INTC *IntcInstancePtr, XTmrCtr *TmrCtrInstancePtr,
						u16 DeviceId, u16 IntrId)
{
	u8  DutyCycle;
	u8  NoOfCycles;
	u8  Div;
	u32 Period;
	u32 HighTime;
	u64 WaitCount;
	int Status;

	/*
	 * Initialize the timer counter so that it's ready to use,
	 * specify the device ID that is generated in xparameters.h
	 */
	Status = XTmrCtr_Initialize(TmrCtrInstancePtr, DeviceId);
	if (Status != XST_SUCCESS) {
		return XST_FAILURE;
	}

	/*
	 * Perform a self-test to ensure that the hardware was built
	 * correctly. Timer0 is used for self test
	 */
	Status = XTmrCtr_SelfTest(TmrCtrInstancePtr, TMRCTR_0);
	if (Status != XST_SUCCESS) {
		return XST_FAILURE;
	}

	/*
	 * Connect the timer counter to the interrupt subsystem such that
	 * interrupts can occur
	 */
	Status = TmrCtrSetupIntrSystem(IntcInstancePtr, TmrCtrInstancePtr,
							DeviceId, IntrId);
	if (Status != XST_SUCCESS) {
		return XST_FAILURE;
	}

	/*
	 * Setup the handler for the timer counter that will be called from the
	 * interrupt context when the timer expires
	 */
	XTmrCtr_SetHandler(TmrCtrInstancePtr, TimerCounterHandler,
							TmrCtrInstancePtr);

	/* Enable the interrupt of the timer counter */
	XTmrCtr_SetOptions(TmrCtrInstancePtr, TMRCTR_0, XTC_INT_MODE_OPTION);
	XTmrCtr_SetOptions(TmrCtrInstancePtr, TMRCTR_1, XTC_INT_MODE_OPTION);

	/*
	 * We start with the fixed divisor and after every CYCLE_PER_DUTYCYCLE
	 * decrement the divisor by 1, as a result Duty cycle increases
	 * proportionally. This is done until duty cycle is reached upto
	 * MAX_DUTYCYCLE
	 */
	Div = DUTYCYCLE_DIVISOR;

	/* Configure PWM */
	do {
		/* Fail check for 0 divisor */
		if (!Div) {
			Status = XST_FAILURE;
			goto err;
		}

		/* Disable PWM for reconfiguration */
		XTmrCtr_PwmDisable(TmrCtrInstancePtr);

		/* Configure PWM */
		Period = PWM_PERIOD;
		HighTime = PWM_PERIOD / Div--;
		DutyCycle = XTmrCtr_PwmConfigure(TmrCtrInstancePtr, Period,
								HighTime);
		if (Status != XST_SUCCESS) {
			Status = XST_FAILURE;
			goto err;
		}

		xil_printf("PWM Configured for Duty Cycle = %d\r\n", DutyCycle);

		/* Enable PWM */
		XTmrCtr_PwmEnable(TmrCtrInstancePtr);

		NoOfCycles = 0;
		WaitCount = WAIT_COUNT;
		while (NoOfCycles < CYCLE_PER_DUTYCYCLE) {
			if (PeriodTimerHit == TRUE && HighTimerHit == TRUE) {
				PeriodTimerHit = FALSE;
				HighTimerHit = FALSE;
				WaitCount = WAIT_COUNT;
				NoOfCycles++;
			}

			/* Interrupt did not occur as expected */
			if (!(--WaitCount)) {
				return XST_FAILURE;
			}
		}
	} while (DutyCycle < MAX_DUTYCYCLE);

	Status = XST_SUCCESS;
err:
	/* Disable PWM */
	XTmrCtr_PwmDisable(TmrCtrInstancePtr);

	/* Disable interrupts */
	TmrCtrDisableIntr(IntcInstancePtr, DeviceId);

	return Status;
}

/*****************************************************************************/
/**
* This function is the handler which performs processing for the timer counter.
* It is called from an interrupt context.
*
* @param	CallBackRef is a pointer to the callback function
* @param	TmrCtrNumber is the number of the timer to which this
*		handler is associated with.
*
* @return	None.
*
* @note		None.
*
******************************************************************************/
static void TimerCounterHandler(void *CallBackRef, u8 TmrCtrNumber)
{
	/* Mark if period timer expired */
	if (TmrCtrNumber == TMRCTR_0) {
		PeriodTimerHit = TRUE;
	}

	/* Mark if high time timer expired */
	if (TmrCtrNumber == TMRCTR_1) {
		HighTimerHit = TRUE;
	}
}

/*****************************************************************************/
/**
* This function setups the interrupt system such that interrupts can occur
* for the timer counter. This function is application specific since the actual
* system may or may not have an interrupt controller.  The timer counter could
* be directly connected to a processor without an interrupt controller.  The
* user should modify this function to fit the application.
*
* @param	IntcInstancePtr is a pointer to the Interrupt Controller
*		driver Instance.
* @param	TmrCtrInstancePtr is a pointer to the XTmrCtr driver Instance.
* @param	DeviceId is the XPAR_<TmrCtr_instance>_DEVICE_ID value from
*		xparameters.h.
* @param	IntrId is XPAR_<INTC_instance>_<TmrCtr_instance>_VEC_ID
*		value from xparameters.h.
*
* @return	XST_SUCCESS if the Test is successful, otherwise XST_FAILURE.
*
* @note		none.
*
******************************************************************************/
static int TmrCtrSetupIntrSystem(INTC *IntcInstancePtr,
			XTmrCtr *TmrCtrInstancePtr, u16 DeviceId, u16 IntrId)
{
	 int Status;

#ifdef XPAR_INTC_0_DEVICE_ID
	/*
	 * Initialize the interrupt controller driver so that
	 * it's ready to use, specify the device ID that is generated in
	 * xparameters.h
	 */
	Status = XIntc_Initialize(IntcInstancePtr, INTC_DEVICE_ID);
	if (Status != XST_SUCCESS) {
		return XST_FAILURE;
	}

	/*
	 * Connect a device driver handler that will be called when an interrupt
	 * for the device occurs, the device driver handler performs the
	 * specific interrupt processing for the device
	 */
	Status = XIntc_Connect(IntcInstancePtr, IntrId,
				(XInterruptHandler)XTmrCtr_InterruptHandler,
				(void *)TmrCtrInstancePtr);
	if (Status != XST_SUCCESS) {
		return XST_FAILURE;
	}

	/*
	 * Start the interrupt controller such that interrupts are enabled for
	 * all devices that cause interrupts, specific real mode so that
	 * the timer counter can cause interrupts through the interrupt
	 * controller
	 */
	Status = XIntc_Start(IntcInstancePtr, XIN_REAL_MODE);
	if (Status != XST_SUCCESS) {
		return XST_FAILURE;
	}

	/* Enable the interrupt for the timer counter */
	XIntc_Enable(IntcInstancePtr, IntrId);
#else
	XScuGic_Config *IntcConfig;

	/*
	 * Initialize the interrupt controller driver so that it is ready to
	 * use
	 */
	IntcConfig = XScuGic_LookupConfig(INTC_DEVICE_ID);
	if (NULL == IntcConfig) {
		return XST_FAILURE;
	}

	Status = XScuGic_CfgInitialize(IntcInstancePtr, IntcConfig,
					IntcConfig->CpuBaseAddress);
	if (Status != XST_SUCCESS) {
		return XST_FAILURE;
	}

	XScuGic_SetPriorityTriggerType(IntcInstancePtr, IntrId,
					0xA0, 0x3);

	/*
	 * Connect the interrupt handler that will be called when an
	 * interrupt occurs for the device.
	 */
	Status = XScuGic_Connect(IntcInstancePtr, IntrId,
				 (Xil_ExceptionHandler)XTmrCtr_InterruptHandler,
				 TmrCtrInstancePtr);
	if (Status != XST_SUCCESS) {
		return Status;
	}

	/* Enable the interrupt for the Timer device */
	XScuGic_Enable(IntcInstancePtr, IntrId);
#endif /* XPAR_INTC_0_DEVICE_ID */

	/* Initialize the exception table */
	Xil_ExceptionInit();

	/* Register the interrupt controller handler with the exception table */
	Xil_ExceptionRegisterHandler(XIL_EXCEPTION_ID_INT,
					(Xil_ExceptionHandler)
					INTC_HANDLER,
					IntcInstancePtr);

	/* Enable non-critical exceptions */
	Xil_ExceptionEnable();

	return XST_SUCCESS;
}

/******************************************************************************/
/**
*
* This function disconnects the interrupts for the Timer.
*
* @param	IntcInstancePtr is a reference to the Interrupt Controller
*		driver Instance.
* @param	IntrId is XPAR_<INTC_instance>_<Timer_instance>_VEC_ID
*		value from xparameters.h.
*
* @return	None.
*
* @note		None.
*
******************************************************************************/
void TmrCtrDisableIntr(INTC *IntcInstancePtr, u16 IntrId)
{
	/* Disconnect the interrupt for the timer counter */
#ifdef XPAR_INTC_0_DEVICE_ID
	XIntc_Disconnect(IntcInstancePtr, IntrId);
#else
	XScuGic_Disconnect(IntcInstancePtr, IntrId);
#endif
}

Some of the Macros which aren't defined: XPAR_INTC_0_DEVICE_ID, XPAR_INTC_0_TMRCTR_0_VEC_ID, XPAR_FABRIC_TMRCTR_0_VEC_ID and causing errors

  • Sign in to reply
  • Cancel

Top Replies

  • LTxAlves
    LTxAlves over 3 years ago +2 verified
    Apparently, due to the interrupt signal not being connected in the block design, SDK didn't generate the Macros for interrupts. Connecting the interrupt signal fixed the issue.