I have managed to boot the base_2022.2 image from sdcard. That's cool.
But in the process of playing with u-boot on the embedded memory, I did a saveenv and it corrupted u-boot.
I could put my own image on there I guess, but I'd like to restore it back to its original glory.
Does avnet have an image I can download for it?
This device is identified by linux like this:
Disk /dev/mmcblk0: 7.09 GiB, 7616856064 bytes, 14876672 sectors
Units: sectors of 1 * 512 = 512 bytes
Sector size (logical/physical): 512 bytes / 512 bytes
I/O size (minimum/optimal): 512 bytes / 512 bytes
Disklabel type: dos
Disk identifier: 0x00000000