Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Embedded Vision Kits / Image Sensor Interface / FMC-IMAGEON /High speed frame rate
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 0 replies
  • Subscribers 357 subscribers
  • Views 331 views
  • Users 0 members are here
Related

Embedded Vision Kits / Image Sensor Interface / FMC-IMAGEON /High speed frame rate

pollutioncontroltech
pollutioncontroltech over 8 years ago

Hi there,

I have been trying to figure out what kind of hardware/software is needed for my project. The project is getting the images with a high speed image sensor with a frame rate of 500-1000fps at a lower resolutions such as 160x120,  480x360 pixels or @VGA (any of resolution is okay). The frames will be read with FPGA SoC board and will be saved to external hard drive via FPGA board.

https://www.xilinx.com/support/documentation/application_notes/xapp794-1080p60-camera.pdf

While I was searching online I came across this project/kit (attached link) from Xilinx/Avnet. It has an Avnet FMC-IMAGEON (FMC daughter board) with VITA-2000 (Phyton-1300 C as option too) camera/image sensor with Xilinx ZC702 board. It would read the images at 60fps with 1080p resolution, and then do the other tasks ( display the images etc.)

I am basically looking for something like this, but I will be needing more fps at lower resolutions. I know that the necessary arrangements in codes/IP’s shall be made. Other than that, I have these questions popped up in my mind:

Q1: Can this example project do 500+fps with lower resolution (160x120pixels)?
Q2: If not, what is the bottleneck and is there a way to fix it?
Q3: If the bottleneck is the image sensor, can it be replaced with any other, do you sell different embedded vision kits that capable of doing my project?
Q4: If the bottleneck is the FMC daughter board, do you have a better one or do you have any suggestions?
Q5: If the bottleneck is interface, what do you suggest?
Q6: Is there any other way to connect the image sensor to an FPGA, if so would lead/help me to find out?

 

I am interested in Embedded Vision Kits like this, and board level cameras/image sensors but couldn’t find any similar kits that has an image sensor that has a frame rate that my project requires (500-1000fps at any resolution). If there is one would you send me a link and furthermore I would have some more technical question to be answered ( so if I am reaching out the wrong person please direct me to right one)

 



Thanks in advance !

Regards,

Sirac KAYA