RIoTboard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • RIoTboard
  • More
  • Cancel
RIoTboard
Blog Linux 4.1 + Ubuntu 14.04 on RIoTboard
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RIoTboard to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 13 Sep 2015 5:15 AM Date Created
  • Views 4261 views
  • Likes 3 likes
  • Comments 14 comments
Related
Recommended

Linux 4.1 + Ubuntu 14.04 on RIoTboard

e14 Contributor
e14 Contributor
13 Sep 2015

Intro

I was inspired by Otto's blog series of getting Debian Linux on the RIoTboard: Linux on the RIoTBoard Part 1: U-Boot. However I need Ubuntu instead.

 

Following are the steps to get a current Linux kernel (4.1) with Ubuntu 14.04 (should work with a more current version one too).

 

Requirements

I used Ubuntu 14.04 x86_64 to implement these instructions (actually it was a Virtual machine on VirtualBox).

 

Install Build dependencies:

sudo apt-get install git build-essential fakeroot kernel-package u-boot-tools lzop zlib1g-dev libncurses5-dev gcc-4.7-arm-linux-gnueabihf
sudo ln -s arm-linux-gnueabihf-gcc-4.7 /usr/bin/arm-linux-gnueabihf-gcc

Please note the specific install of gcc 4.7.  This is because the current version (as of 09/2015) in 14.04 of gcc 4.8 has a bug when building the Linux Kernel.  Feel free to try 4.9 or a fixed 4.8.

The following is needed to chroot to arm based rootfs.

sudo apt-get install qemu-user-static

This is needed to help in the steps to create an sdcard image.

sudo apt-get install qemu-utils kpartx

 

Environment Variables

Here are environment variables used in the scripts that follow.

export ARCH=arm
export CROSS_COMPILE=/usr/bin/arm-linux-gnueabihf-
export RIOT_PATH=~/riotboard
export RIOT_OUTPUT=$RIOT_PATH/output
mkdir -p $RIOT_OUTPUT

 

U-Boot

Here are the steps to build version 2015.07 of U-boot:

cd $RIOT_PATH
wget ftp://ftp.denx.de/pub/u-boot/u-boot-2015.07.tar.bz2
tar xjf u-boot-2015.07.tar.bz2
cd u-boot-2015.07
make riotboard_defconfig
make
cp u-boot.imx $RIOT_OUTPUT/.
cd $RIOT_PATH

If you prefer to use the latest U-Boot or a different version see: SourceCode < U-Boot < DENX

 

Bootscript

The boot.scr is used by U-Boot to give it the boot arguments to pass to the kernel as well as were to find the kernel and DTB.

Please note this script is very basic and needs to know where you will be booting from.  Change the DEVICE= line if you will be booting from eMMC or MicroSD instead.  My eMMC is busted so I have to boot from uSD or SD.

mkdir -p $RIOT_PATH/bootscript
cd $RIOT_PATH/bootscript
# Device 0=SD, 1=MicroSD, 2=eMMC
DEVICE=0
cat <<EOF > bootscript
setenv bootargs console=ttymxc1,115200 nosmp video=mxcfb0:dev=hdmi,1280x720M@60,bpp=32 video=mxcfb1:off fbmem=10M vmalloc=400M rootwait root=/dev/mmcblk0p1
mmc dev $DEVICE
ext4load mmc $DEVICE:1 10800000 /boot/zImage
ext4load mmc $DEVICE:1 16800000 /boot/imx6dl-riotboard.dtb
bootz 10800000 - 16800000
EOF
mkimage -A arm -O linux -T script -C none -a 0 -e 0 -n "boot script" -d bootscript boot.scr
cp boot.scr $RIOT_OUTPUT/.
cd $RIOT_PATH

 

Kernel

I decided to use a specific released version (i.e. v4.1) of the kernel rather than the tip.  Feel free to change the tag to switch to a different version or remove the -b option if you want to build the tip.  I have not fully tested 4.1 but so far seems to work ok on the RIoTboard.

For detail on each step below see Otto's blog.

cd $RIOT_PATH
git clone https://git.kernel.org/pub/scm/linux/kernel/git/torvalds/linux.git -b v4.1
cd linux
make imx_v6_v7_defconfig
# Do this next step if you need to change kernel config.
make menuconfig
# this next step will take a long time.  You can try -j option to parallelize.
make bzImage
mkdir -p $RIOT_OUTPUT/boot
sudo cp arch/arm/boot/zImage $RIOT_OUTPUT/boot/zImage
make dtbs
sudo cp arch/arm/boot/dts/imx6dl-riotboard.dtb $RIOT_OUTPUT/boot/imx6dl-riotboard.dtb
make modules
make modules_install INSTALL_MOD_PATH=$RIOT_OUTPUT
make headers_install INSTALL_HDR_PATH=$RIOT_OUTPUT/usr
cd $RIOT_OUTPUT
tar -czf linux-kernel.tgz boot lib usr
rm -rf boot lib usr

 

Root Filesystem

For the rootfs I decided to start from the official ubuntu release and customize it as opposed to building it completely like Otto showed in his blog for Debian.  You can browse here: Index of /ubuntu-core/releases if you would like to pick a different ubuntu release.  If you do, make sure to use an armhf one and update the customizations below in case they are different for your distro.

Unlike other steps above I am going to break this one down:

Get a starting rootfs

cd $RIOT_PATH
mkdir -p $RIOT_OUTPUT/rootfs
wget http://cdimage.ubuntu.com/ubuntu-core/releases/trusty/release/ubuntu-core-14.04-core-armhf.tar.gz
sudo tar --numeric-owner -xzpf ubuntu-core-14.04-core-armhf.tar.gz -C $RIOT_OUTPUT/rootfs

Customize the rootfs

We will chroot to the arm rootfs to make some of the customizations.

# to enable arm emulation
sudo cp /usr/bin/qemu-arm-static $RIOT_OUTPUT/rootfs/usr/bin/
# to enable dns lookups to work
sudo cp /etc/resolv.conf $RIOT_OUTPUT/rootfs/etc
sudo chroot $RIOT_OUTPUT/rootfs

Do your customizations.  Feel free to adjust the stuff below to your needs.  Please note not all of what I am doing below needs to be done from chroot (e.g the file editing and creations).

# setup a locale
locale-gen en_US en_US.UTF-8
# Install any packages you want that are not in the core rootfs from Ubuntu.com
apt-get -y install openssh-server ntpdate
# Create users. The following adds usr/pw: ubuntu/ubuntu
PASSWD=`openssl passwd -crypt ubuntu`
/usr/sbin/useradd ubuntu -m -s /bin/bash -p $PASSWD
# The stuff below can be done outside of chroot. Just make sure to adjust destination files if you do.
# Enable the user to sudo without the need for pw.
echo -e 'ubuntu\tALL=(ALL)\tNOPASSWD: ALL' >> /etc/sudoers
# Configure your network
cat <<EOF >> /etc/network/interfaces
auto eth0
iface eth0 inet dhcp
EOF
# Set the hostname
echo riotboard > /etc/hostname
# Enable login from the serial console
cat <<EOF > /etc/init/serial-console.conf
# serial-console - getty
#
# This service maintains a getty on console from the point the system is
# started until it is shut down again.

start on stopped rc RUNLEVEL=[2345]

stop on runlevel [!2345]

respawn
exec /sbin/getty -L 115200 ttymxc1 vt100
EOF
#setup fstab to mount the rootfs
echo '/dev/mmcblk0p1  /  auto  errors=remount-ro  0  1' >> /etc/fstab

Clean up apt, exit chroot and remove the chroot setup files

# Clean up apt
apt-get clean
exit
# Clean up files we added to enable chroot and dns
sudo rm $RIOT_OUTPUT/rootfs/usr/bin/qemu-arm-static
sudo rm $RIOT_OUTPUT/rootfs/etc/resolv.conf

 

Bundle up the rootfs:

cd $RIOT_OUTPUT/rootfs
sudo tar -czpf ubuntu-trusty.tgz *
sudo mv ubuntu-trusty.tgz $RIOT_OUTPUT/.

 

Create SD Card Image

Now we create the SD Card image that we will write to an SD card.  You could even write this to the eMMC device (don't forget to change the boot script to load from device 2 if you do this).  If you prefer you can use /dev/sdX instead of sdcard.img below if you want to write direct to the SD card instead of an image first.

cd $RIOT_OUTPUT
# Create a file to hold the disk image
qemu-img create sdcard.img 3600M
# Partition the disk image leaving some room (10mb) for u-boot in front of the first partition.
sfdisk --force -uM sdcard.img << EOF
10,,83
EOF
# create devices from the disk image
sudo kpartx -av sdcard.img
# format the partition. Make sure to use the correct device from the previous command.
mkfs.ext4 -j /dev/mapper/loop0p1
# create a mount point
sudo mkdir -p /mnt/sdcard
# Mount the partition we formatted.
sudo mount -t ext4 /dev/mapper/loop0p1 /mnt/sdcard
# Unpack the root fs and kernel
sudo tar --numeric-owner -C /mnt/sdcard -zxpf ubuntu-trusty.tgz
sudo tar --numeric-owner -C /mnt/sdcard -zxpf linux-kernel.tgz
# Copy the boot script to the top level
sudo cp boot.scr /mnt/sdcard/boot.scr
# Unmount and clean up devices
sudo umount /mnt/sdcard
sudo kpartx -dv sdcard.img
# put u-boot 2 blocks into the disk image.  Don't leave out the notrunc option.
dd if=u-boot.imx of=sdcard.img bs=512 seek=2 conv=notrunc

Now you can use dd or whatever tool you want to write the disk image to an SD card. Eg: sudo dd if=sdcard.img of=/dev/sdd bs=1m

 

Boot your SD Card

Plug the SD Card into the SD card slot.  Set the switches 2,4,5,7 to OFF and the rest to ON to boot from SD.

If you are using a MicroSD, make sure to change the boot script to use device 1 instead of 0 and set the dip switches to 2,4,5,8 OFF and the rest ON.

 

Notes

See Otto's blog post mentioned above for how to use the MfgTool to write the above files to the eMMC flash from Windows as well as more detailed explanations to some of the stuff above..

  • Sign in to reply
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to joesgarage

    Because Oneiric is 11.10 and Trusty is 14.04 which is the Ubuntu version I am using.  You can rename the ubuntu-trusty.tgz file to oneiric.tgz if you like or you can add the following to the ucl2.xml:

     

    <LIST name="i.MX6SOLO-UbuntuTrusty-RIOT-eMMC" desc="Choose eMMC as media">
      <CMD state="BootStrap" type="boot" body="BootStrap" file ="u-boot-mx6solo-RIoTboard.bin" >Loading U-boot</CMD>
      <CMD state="BootStrap" type="load" file="uImage" address="0x10800000"
        loadSection="OTH" setSection="OTH" HasFlashHeader="FALSE" >Loading Kernel.</CMD>
      <CMD state="BootStrap" type="load" file="initramfs.cpio.gz.uboot" address="0x10C00000"
        loadSection="OTH" setSection="OTH" HasFlashHeader="FALSE" >Loading Initramfs.</CMD>
      <CMD state="BootStrap" type="jump" > Jumping to OS image. </CMD>
    
      <CMD state="Updater" type="push" body="$ dd if=/dev/zero of=/dev/mmcblk0 bs=1M count=20">Wipe partition and bootloader</CMD>
    
      <CMD state="Updater" type="push" body="send" file="mksdcard.sh.tar">Sending partition shell</CMD>
      <CMD state="Updater" type="push" body="$ tar xf $FILE "> Partitioning...</CMD>
      <CMD state="Updater" type="push" body="$ sh mksdcard.sh /dev/mmcblk0"> Partitioning...</CMD>
    
      <CMD state="Updater" type="push" body="send" file="files/u-boot.imx">Sending u-boot</CMD>
      <CMD state="Updater" type="push" body="$ dd if=$FILE of=/dev/mmcblk0 bs=512 seek=2">write u-boot.imx</CMD>
      <CMD state="Updater" type="push" body="$ dd if=/dev/zero of=/dev/mmcblk0 bs=512 seek=1536 count=16">clean up u-boot parameter</CMD>
      <CMD state="Updater" type="push" body="frf">flush the memory</CMD>
    
      <CMD state="Updater" type="push" body="$ mkfs.ext4 -j /dev/mmcblk0p1">Formatting rootfs partition</CMD>
      <CMD state="Updater" type="push" body="$ mkdir -p /mnt/mmcblk0p1"/>
      <CMD state="Updater" type="push" body="$ mount -t ext4 /dev/mmcblk0p1 /mnt/mmcblk0p1"/>
    
      <CMD state="Updater" type="push" body="pipe tar --numeric-owner -zxv -C /mnt/mmcblk0p1" file="files/ubuntu-trusty.tgz">Sending and writing rootfs</CMD>
      <CMD state="Updater" type="push" body="frf">Finishing rootfs write</CMD>
    
      <CMD state="Updater" type="push" body="pipe tar --numeric-owner -zxv -C /mnt/mmcblk0p1" file="files/linux-kernel.tgz">Sending and writing Kernel and Modules</CMD>
      <CMD state="Updater" type="push" body="frf">Finishing writing Kernel and Modules</CMD>
    
      <CMD state="Updater" type="push" body="send" file="files/boot.scr">Sending bootscript</CMD>
      <CMD state="Updater" type="push" body="$ cp $FILE /mnt/mmcblk0p1/boot.scr">Copy bootscript into root</CMD>
      <CMD state="Updater" type="push" body="frf">flush the memory</CMD>
    
      <CMD state="Updater" type="push" body="$ umount /mnt/mmcblk0p1">Unmounting rootfs partition</CMD>
    
      <CMD state="Updater" type="push" body="$ echo Update Complete!">Done</CMD>
    </LIST>

     

    Also don't forget to edit the cfg.ini to point to this config by setting: name = i.MX6SOLO-UbuntuTrusty-RIOT-eMMC

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • joesgarage
    joesgarage over 11 years ago

    Hi.

    Why didn't you create the oneiric.tgz  file for the mfg tool ?  Isn't it required ?

    From Ottos post, it appears we need:

    - u-boot.imx

    - boot.scr

    - linux-kernel.tgz

    - oneiric.tgz

     

    //-Joe

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to zainzymplsi

    I don't have a use for them in my project so haven't tested if they are there or not.  I was assuming the mainline kernel would fully support the capabilities of the i.MX6 by now.   If not you could try the latest 4.2 or build your kernel and dtb from: linux-2.6-imx.git - Freescale i.MX Linux Tree or from https://git.kernel.org/cgit/linux/kernel/git/shawnguo/linux.git and see if you have better luck.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • zainzymplsi
    zainzymplsi over 11 years ago

    Hi,

    can you show the steps to add in IPU/VPU/GPU support.

     

    Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<