Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Using Circuit Studio
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Locked Locked
  • Replies 15 replies
  • Subscribers 91 subscribers
  • Views 3077 views
  • Users 0 members are here
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Using Circuit Studio

e14 Contributor
e14 Contributor over 11 years ago

I was to renew my PADS license and was very excited when when I found out that Altium is offering Circuit Studio. PADS has so many bugs and such unpredictable behavior. At any rate I downloaded the Circuit Studio trial and as former D09 user I was able to quickly adapt. But I will say that there is very limited documentation on on Circuit Studio so I did have several questions on how to use some of the features but Marisol from Altium was REALLY GREAT in walking me through using the tool and answering all my questions. I was amazed at how quick she would respond to my emails. The support I received during the trial was truly a first class experience! I am very happy with my decision of having bought Circuit Studio and look forward to the future updates as the tool matures. 

  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor +2
    Hi Jean, This is Lawrence Romine with Altium. I am responsible for the care and feeding of this product. Firstly, thanks very much for your business and your return to the Altium brand! Secondarily, I…
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to shabaz +1
    Hi Clem, Shabaz, Yes, circuit Studio is very similar to AD with some limitations (no FPGA nor simulation). Productivity seems good after the mandatory learning curve, which was longer for me, being a previous…
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor +1
    Hi Javier, To import DXF files into ACS, first create a new blank PCB document in your project. With the blank PCB doc selected, navigate to File -> Import.. and browse to your DXF file's location. If…
  • clem57
    clem57 over 11 years ago

    Do you have any circuits that you can compare under both?

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • shabaz
    shabaz over 11 years ago

    Hi Jean B,

     

    I've use Altium Designer (a long time ago when they first introduced DXP), and from screenshots (I have not tried it yet) Circuit Studio looks very similar although with a different menu system perhaps, which looks good. How did you find it?

    I'm wondering if Circuit Studio is like a bleeding-edge version of Altium Designer, i.e. will get certain innovations first which will then be incorporated and matured/enhanced in Altium Designer.

    This is just a guess though : (  - wondering if you knew about the different products since you say you used Designer in the past too.

    How good is productivity with Circuit Studio for you? Is it fast to create custom components?

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to shabaz

    Hi Clem, Shabaz,

    Yes, circuit Studio is very similar to AD with some limitations (no FPGA nor simulation). Productivity seems good after the mandatory learning curve, which was longer for me, being a previous PADS user. I have started two PCBoards since 2 months using CS and have not gone through major issues. The library management is easy and creating custom components can be done using templates, or from modifying existing parts, or from scratch. I think Altium really wanted to get into the market of small-business users with an affordable solution which "does the job".

    Actually I started a PCB with PADS DxDesigner+PCB suite, got fed up and did not renew the licence, I re-did the same board with CS, managed to import some libraries from PADS and I can tell that CS compares very favorably with PADS.

    I must say that there are still some improvements to be done in CS, but I hope this will be covered in further releases.

    • Cancel
    • Vote Up +1 Vote Down
    • Cancel
  • clem57
    clem57 over 11 years ago in reply to e14 Contributor

    Thanks for comparing the two.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor

    Hi Jean, This is Lawrence Romine with Altium. I am responsible for the care and feeding of this product. Firstly, thanks very much for your business and your return to the Altium brand! Secondarily, I wanted to publicly acknowledge your comments, and everyone's comments on this and other forums for that matter. We are now in Beta Test with v1.1 of CircuitStudio. Of course, this will contain the expected maintenance of the tool that you should expect, but also some great new capabilities that I've listed below. Please also know that we are paying very close attention to our customers feedback, the evaluators feedback, the feedback we are getting from e14 support staff, and social media outlets. These channels are extremely important to us and directly impact the future development of the product. So, please keep it coming. Here is what you can expect in 1.1 scheduled for mid-May:

     

    - Importers Updated - AD10 and older, Protel, PCAD (these are in addition to the Eagle/OrCAD/PADs importers in there now), and yes, that includes AD10 Board files

    - Mixed Mode Simulation

    - .STEP Export

    - DXF Import

    • Cancel
    • Vote Up +2 Vote Down
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor

    Lawrence,

     

    Is the import function from AD10 available now?

     

    Will (and when) Circuit Studio be able to directly export to Designer?

    Or, will Designer be able to import directly from Circuit Studio?

     

    Without Designer import/export capability the product has nothing to offer justifying the huge change from what I am using now.

     

    Thanks,

     

    Jay Zebryk

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor

    Jay,

    CircuitStudio V1.1 which includes the AD10 PCBDOC support was released last night. As well, the update to Altium Designer that includes support for CircuitStudio file formats was released last week. So, as long as you update to the most recent build of both products, you should be able to move bidirectionally. Thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago

    Hi,

    I updated to CircuitStudio V1.1 and I cannot import DXF files. With this version is supposed that it is possible?. If so, how?

    Best regards

    Javier

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago

    What version of pads were you using. Does the Circuit studio router push and shove etc.

     

    Geoff

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor

    Hi Javier,

    To import DXF files into ACS, first create a new blank PCB document in your project. With the blank PCB doc selected, navigate to File -> Import.. and browse to your DXF file's location. If successful, you will see an Import from AutoCAD window with options to set scaling, origin etc. Depending on your original DXF's parameters, set these accordingly & you should be able to view the contents.

     

    If you face errors, there will be a LOG file generated within your project. If the contents of the LOG file says: "Class not registered", then you need to re-install the TeighaX located in <Your install directory>\Program Files (x86)\Altium\CS\System\Installation\TeighaX_Setup_3.9.0.msi . If the LOG file does not show anything but still the import fails, it is a scaling / layers issue.

     

    Also make sure, you have installed the AutoCAD imports under extensions. Hope this helps.

     

    Ashok.

    • Cancel
    • Vote Up +1 Vote Down
    • Cancel
>