Analog Devices
  • Products & Partners
  • Manufacturers
  • Analog Devices
  • More
  • Cancel
Analog Devices
Blog What Would You Build with the Pocket IO™︎ Development Platform?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Analog Devices to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: rscasny
  • Date Created: 20 Apr 2017 4:31 PM Date Created
  • Views 6543 views
  • Likes 12 likes
  • Comments 35 comments
  • maxim_blogs
  • industrial automation
  • industrial_automation
  • maxim blogs
Related
Recommended

What Would You Build with the Pocket IO™︎ Development Platform?

rscasny
rscasny
20 Apr 2017

The Pocket IOTm programmable logic controller (PLC) development platform from Maxim Integrated Products, Inc. addresses the challenges of industrial automation and Industry 4.0 designers who need to keep a manufacturing line running 24 hours a day, 7 days a week, and provides you with the ability to achieve the smallest form factor and highest power efficiency for next-generation PLC designs.image

 

The Pocket IOTm programmable logic controller (PLC) development board is a reference design that integrates:

 

  • 30 IO's consisting of four analog inputs, one analog output, eight digital inputs, eight digital outputs,
  • Two RS485 (Profibus-capable field busses)
  • Three encoder motor-control ports
  • Four IO-LinkRegistered masters.

 

Pocket IO connectivity is through USB or its own Wi-FiRegistered network.

 

Code can be developed to run on the IntelRegistered Edison using the popular and easy to use open-source ArduinoRegistered software IDE.

 

The Pocket IO provides the following key advantages to increase productivity:

 

  • Real-time intelligence: Fast data processing provides the necessary data to make intelligent decisions quickly and effectively to optimize yield.
  • Adaptive manufacturing: Manufacturing flexibility allows for real-time changes and adjustments to avoid potential downtime.
  • Distributed control: Ultra-small footprint of less than 10 cubic inches and smart energy consumption brings PLC down to the manufacturing line, re-distributing intelligent control and providing redundancy.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

So, the question is: What prototype would you build with the Pocket IOTm development board? Please offer your comments below

  • Sign in to reply

Top Comments

  • DAB
    DAB over 9 years ago +4
    Very intriguing. I have been looking for a controller to integrate into an old CNC Kit I never finished. I could use the Digital IO to control the stepper motors and monitor the stops. I no longer need…
  • balearicdynamics
    balearicdynamics over 9 years ago +3
    If I have one of these in my hand I recall my memories... It was the mid of '80s and I was an active member of the Italian Society of Ergonomics. With the collaboration of the University of Turin Dept…
  • dougw
    dougw over 9 years ago +3
    I like the functionality in this product and would consider it if the need arose. It is a bit of struggle to break into the PLC market as the industry seems very conservative and leans towards proven rugged…
  • balearicdynamics
    balearicdynamics over 9 years ago in reply to Jan Cumps

    As far as I know, not the IC, just the modules.

    From Intel PCN115580-00 document:

     

    image

    image

    No IC is mentioned there.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to Workshopshed

    Did Intel stop producing the Edison IC? I thought it was only the Dev boards they stopped?

    Need to double-check ...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 9 years ago in reply to Workshopshed

    Andy I am trying to setup a real-world project based on this PLC, if the supplier agree. I have read too the specifications but I just understood something like it is compatible with the Edison. Maybe your are better reading the specifications so my worry now it is near to be a certain. rscasny , what happens if we start a project involving a small woodworking factory and the Edison goes out of production? This product is not so cheap; what happens if the factory is interested and want to expand the test project on other task areas ? I hope that the supplier is providing a new version based on something different than Edison. Or it is just the CPU that is used and the board that Intel stopped producing does not affect this product?

     

    I hope that someone can give us some clarifications about.

     

    BTW. I have downloaded and read in detail the Intel official document and as far as I know, my impression is that they just stopped producing the bare Edison development boards. Or there is some detail that I missed ...

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Workshopshed
    Workshopshed over 9 years ago

    A PLC is a great way to control a complex Electro-mechanical project. I know Tim Hunkin uses old controllers to control his animatronic games such as i-Zombie

     

    My main concern with this module is that it's based around the Edison. A very functional board but given that Intel have stopped development it does raise the question of product life and support.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • cybermah
    cybermah over 9 years ago

    I would attempt to build a 3d printer.  But unlike regular 3d printers, I would use a robotic arm design.  The Pocket IO looks like it would be an excellent alternative to the regular arduino and stepper motor drivers.

     

    Thanks

     

    Dana

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>