Analog Devices
  • Products & Partners
  • Manufacturers
  • Analog Devices
  • More
  • Cancel
Analog Devices
Forum Why Is Analog Design Harder Than Digital Design?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Analog Devices to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 20 replies
  • Subscribers 53 subscribers
  • Views 13695 views
  • Users 0 members are here
  • why is analog design harder than digital design?
  • precision measurement
  • digital design
  • analog design
  • reliable circuit protection
  • rugged connectivity
  • efficient power
Related

Why Is Analog Design Harder Than Digital Design?

rscasny
rscasny over 6 years ago

Are you an analog design engineer or digital? By most standards, the marketplace is producing more digital design engineers than analog. Ask most engineers and they would tell you why: analog design is harder than digital, and requires more knowledge and more factors to consider such as a deep understanding of efficient power, precision measurement, wireless connectivity, and reliable circuit protection. What  do you think?

 

Let's talk about that a bit more. Is analog design just a matter of knowledge, or is there something more involved? It likely boils down to that fact that analog design involves more than just analog. It's influenced by circuit theory, signal processing, control systems, and device physics, and more. When you consider that circuits and components are more integrated and operated at ultra low power, one needs to consider both pow power, low noise, and stability over the required temperature range.

 

What's analog design require? Efficient power ICs to extend the lifetime and reduce heat dissipation for your design. Precision measurement ICs to feature high accuracy and high performance for across-the-board precision analog applications. Rugged connectivity to offer the industry’s highest level of protection for connectivity in hazardous environments. Reliable protection ICs to protect systems from faults by maintaining and monitoring proper voltage, current, and temperature levels.

 

For sure, analog design has always been more complicated than digital design. While both require the engineer to make design compromises, analog beats digital design in the arena of complexity. All the variables involved just make it nothing but hard.

 

I've told you what I think. How about you?

 

Why do you think analog design is more difficult than digital design? If you have an example, share it with the element14 community?

 

  • Sign in to reply
  • Cancel

Top Replies

  • genebren
    genebren over 6 years ago +6
    Digital is On or Off, where Analog is continuous. Because of this difference, designing Analog circuits becomes much more difficult, as there are so many considerations that need to taken into account…
  • neuromodulator
    neuromodulator over 6 years ago +6
    I think digital is more of an illusion as signals are analog, and that fact will at some point have practical implications even if one tries to ignore that. I also think not that many are into analog because…
  • dougw
    dougw over 6 years ago +6
    Until digital becomes analog (high frequency) it is a bit like a cookbook - just follow the datasheet. With analog, the datasheet is just the start of an adventure.
  • dougw
    dougw over 6 years ago

    I don't think I answered the question earlier.

    I don't think of digital as easier or harder than analog. I started out very keen on digital but ended up spending just as much time on analog and I now like both.

    I apply the same level of rigor to both digital and analog when designing circuitry, so for me they are about the same hard.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 6 years ago in reply to DAB

    True. For example if you wanted to design a multiplication circuit using gates, op-amps and transistors. It is pretty tricky whether you design a digital multiplier or an analog multiplier. I wouldn't say one is easier than the other - it just depends on your experience.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • genebren
    genebren over 6 years ago in reply to DAB

    There are tremendous amounts of overlap of skills between analog and digital design, and a set of building blocks (laws and theorems) that are common knowledge for either disciplines.  That too is true for electronics and other science fields.  One of the best engineers that I ever had the privilege of working  with was actually a PHD physicist.  His physics background was so helpful in understanding the lower level reasons (and theoretical limits) of electronics, especially as it applied to the life sciences application we were working with (pressures, fluidics, light, etc.).

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • dubbie
    dubbie over 6 years ago in reply to dougw

    Douglas,

     

    I thought Chemistry was a sub-set of physics!

     

    Dubbie

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 6 years ago

    I voted

    I am primarily an analog design engineer.

    and then realised that I was the first out of 26 to do so !

    Actually I'm primarily an analogue design engineer but there wasn't an option for that image

     

    I do spend a lot of time doing digital stuff, mainly micros and FPGA but very often the heart of a design will be analogue.

    Often the software side will take longer but the real enabler is analogue - for example in a weighing system I worked on recently most of the design time went into the micro and the Bluetooth interface but the harder part was getting the load cell interface, ADC and power supply (complete with battery management), right, and testing it to prove it's right.

     

    But like many others who have already commented - I wouldn't quite call out one of analogue or digital as harder - it rather depends on how ambitious you are.

     

    MK

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • DAB
    DAB over 6 years ago in reply to genebren

    Hi Gene,

     

    Agreed, there are a lot of overlap, but there are also very keen differences.

    It all depends upon what type of analog circuit you are dealing with and what parameters are involved.

     

    In my experience with advanced aerospace projects, you need very good specialist in both areas to make the project work.

     

    DAB

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • kamtar
    kamtar over 6 years ago

    I would say that it's simple: Digital design is more about working within artificial systems designed by other people. Analog is more about fighting with laws of physics.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 6 years ago in reply to kamtar

    I'd like to think I was getting more friendly with them rather than fighting image

     

    A great deal of analog design involves interacting with things designed by other people, when I get round to it I shall post a blog about my tribulations with voltage references and their data sheets which will illustrate this point.

     

    MK

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • saicheong
    saicheong over 6 years ago

    Nobody will say design a CPU is an easy task or use digital sensors is already easy that use an analog sensors, or say bluetooth is easier that FM analog.

    It depending on what we working for.

     

    People believe digital is easier that the analog because currently the most powerful and flexible human make computer system is digital,

    , we package the logic in software, run in a very complex machine with more that billion components, and make those Abstraction.

     

    In current technology, most of the case we use ADC transfer analog to digital signal, process it and translate back to analog signal by DAC is easier that direct face of analog, it is because the digital signal is well define, mathematisation of data, error prove, our digital computer is powerful and flexible and cheap by mass production that analog, we use digital to hold the complex thing and make outside (analog) simpler.

     

    As Randall say that Power IC is analog design, which is the point of view for Application Engineering ( IC customers), however most Power IC use embedded digital MPU for the heart, as monitor the voltage and current by ADC, implement soft startup, and control MOSFET ON/OFF for precision outputs help to reduce the external components and complex of analog circuits.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • Riffse
    Riffse over 4 years ago

    Analogue design often requires a nuanced optimisation process, the process requires an intuitive level of knowledge, where the process has become as much an art as a clear design process.  Even when the engineer has achieved a high level of ability and knowledge it is still often necessary to build multiple prototypes in order to fully optimise the design.  I design discrete op-amps my latest one is a 'tail current adjustment amplifier' which is a new concept.  I am very aware that although I now have a fully developed circuit, it could be unity gain unstable if it's converted to an IC, and the input transistors are of critical importance to achieve the correct noise performance, so a manufacturer would need to be able to garrantee this.  The design itself has gone through approximately 10 different designs, I have also had to design and build my own test equipment to measure noise and distortion.  So yes there are many difficulties with analogue design, however I think if I was to attempt to design complex digital circuits from the transistor level, this is likely to be just as difficult as you are often pushing the technology to its limits of speed and power consumption.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
<