Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Looking for a matching FFC connector. A Molex rep suggested I try here.
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 309 subscribers
  • Views 1429 views
  • Users 0 members are here
  • connector
  • flat cable
  • ffc
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Looking for a matching FFC connector. A Molex rep suggested I try here.

quickshoe
quickshoe over 3 years ago

I contacted Molex looking for something compatible with the board and cable that I'm working with. Note that the cable in the photo has ears on the ends. The pitch is 1mm. I received a couple samples from Molex, but the cable wouldn't insert. I anyone here familiar with these cables and where else I might look?

See attached photos:

FFC with earsFFC connectors on boardFFC connector on board

  • Sign in to reply
  • Cancel
  • shabaz
    shabaz over 3 years ago

    Hi,

    If it's a one-off, then you could trim the edges. Since 1 mm pitch is quite large, it will be easy to trim with the accuracy required.

    Alternatively, if it's not a 1-off, then you could replace that flat flex with a normal one, so that it fits normal flat flex connectors. Even if the remote end connector is designed for the existing flat flex, it should be able to accommodate the normal flat flex, provided some care is taken when positioning it. Or, a custom flat flex could be used with one end for a normal connector, if it is not a 1-off.

    One other option could be to try a connector with more connections than the flat flex has, so that the excess width of the existing flat flex has space. Might not be ideal but I can't see why it wouldn't work.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • quickshoe
    quickshoe over 3 years ago in reply to shabaz

    I appreciate the suggestions. I'd like to keep the latching feature if possible. If I can't find a compatible solution, then this is the route that I'll take.