Intel
  • Products
  • Manufacturers
  • Intel
  • More
  • Cancel
Intel
Blog Your Thoughts on Intel's New TinyTILE Platform
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Intel to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: spannerspencer
  • Date Created: 17 Aug 2016 10:52 AM Date Created
  • Views 4755 views
  • Likes 5 likes
  • Comments 25 comments
  • intel
  • tinytile
  • devboard
  • intel curie
  • iot
  • pet monitor
Related
Recommended

Your Thoughts on Intel's New TinyTILE Platform

spannerspencer
spannerspencer
17 Aug 2016

I've just been doing the rounds here at element14, and thought you might like a quick insiders' look at the the new SBC on the block; Intel's TinyTILE. It's a very neat little package, and I like to think that you guys have a similar mindset to myself when it comes to a new board -- the form factor is every bit as important as the pricing.

 

Not that I know right now what kind of price tag you can expect to see dangling from the TinyTILE (it's looking like it'll be around the $30 mark, similar to its bigger brother), but the size of it conjures up some very interesting project prospects. Let's take a look at the silicon and solder of it.

 

TinyTILE: A Mini Genuino 101. Kinda.

I suppose that if you wanted to sum up the TinyTILE in the time it takes to chew a Fruit Pastel, that's how you'd pitch it. A miniaturised Genuino/Arduino 101, and that's a pretty mouthwatering flavour, no?

 

"TinyTILE is an Intel Curie module based board," the official blurb tells us, continuing, "measuring approx 35mm x 26mm." Noice! That's deliciously postage stamp sized. And being that it's an adaptation of the Genuino 101, you can program it either using the Arduino IDE or Intel's own ISPC (Intel Software Platform for Curie) software.


The facts are these:imageimage

  • Low-power 32-bit Intel Quark microcontroller

  • 384kB flash memory

  • 80kB SRAM

  • Low-power integrated DSP sensor hub and pattern matching technology

  • Bluetooth Low Energy (BLE)

  • 6-axis sensor with accelerometer and gyroscope

  • Battery charging circuitry (PMIC)

 

Low power consumption, Bluetooth, built-in sensors and the option for battery power gives me the impression that we're looking at a great solution for always-on, remote applications. All very IoT, and possibly even wearable tech given it's core focus on inherent motion sensing.

 

First TinyTILE Impressions

The element14 crew just previewed the TinyTILE for crowds at the Intel Developers Conference in San Francisco, so early reactions to the hardware are imminent.

 

Given it's such a new piece of kit, we're also waiting on some of the finer details (a launch date, for one, currently expected around and deeper imagery but in the meantime I wanted to hear what you guys thought of TinyTILE, and what kind of projects you envisage it being capable of. Please go nuts with your TinyTILE ideas and suggestions in the comments.

 

Oh, and if you're looking for a bit of inspiration, here's a project that invades your dog's privacy with impressive ease while you're at work!

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply

Top Comments

  • michaelkellett
    michaelkellett over 10 years ago in reply to shabaz +2
    Until Intel publish proper data sheets for this and related processors the whole thing remains a huge puffed up PR campaign like "Intel Inside" but with less detail. I've looked a few times and there just…
  • shabaz
    shabaz over 10 years ago in reply to michaelkellett +1
    Hi Michael, My theory is that there is more information they would be willing to share, but that they do not have a mechanism internally for getting it out to individuals because they've never had to do…
  • johnadriaan
    johnadriaan over 10 years ago in reply to michaelkellett +1
    I found these: Intel Quark SE Microcontroller C1000: Overview Intel Quark SE Microcontroller C1000: Datasheet It's a Pentium-level processor, minus the x87 and MMX et al instructions. I am definitely going…
  • clem57
    clem57 over 10 years ago

    I like the new form factor. Is that name a tm by Intel? If so a great name. Seems like Intel is flexing muscle in this area of IoT...

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 10 years ago in reply to mcb1

    Well you could still power it via the Hirose DF40 connector without an add-on board. image

    Ok so it's not the more common coaxial power jack or 0.1" header strip found on similar boards.

    It looks like someone has already thought of this:

    http://49r33r28abcg3uefmh3wkkei.wpengine.netdna-cdn.com/wp-content/uploads/2014/12/Hirose-and-Intel-Edison-product-image…

     

    Not sure that the on-board WiFi comes into it really as it appears to have been designed for IoT and wearable type applications which tends to suggest that additional wired connectivity was anticipated and presumably why they provided the high density 70pin connector to keep the connectivity options open whilst keeping the size down.

     

    SparkFun appear to be making full use of the Edison's Hirose DF40 connectivity in their Edison 'block' range:

    https://www.sparkfun.com/news/1589

     

    Perhaps though the addition of a couple of easier to access pads to solder a power supply onto would have made it more flexible if users were really only interested in the WiFi and Bluetooth connectivity side of it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 10 years ago in reply to beacon_dave

    provide a solution to the connectivity issues for prototyping

    Yes and No.

    They allow connections (at a relatively large cost), but then you always need an add-on board to even just power it up.

     

    then plug into the connector on the production PCB...

    Why design something that has onboard wifi, but needs a addon board simply to power it, and physically connect to it.?

     

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 10 years ago in reply to mcb1

    Don't the Edison breakout boards provide a solution to the connectivity issues for prototyping ? Once prototyped, simply unplug the Edison module and then plug into the connector on the production PCB...

     

    EDI2BB.AL.K INTEL, X86 Edison Breakout Board Kit, Wi-Fi/BT Compatible Module | Farnell element14

     

    EDI2ARDUIN.AL.K INTEL, Intel Edison Kit For Arduino ,Atom , Wi-Fi/BT Compatible Module, Integrated Wi-Fi, 4GB Memory | …

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 10 years ago

    spannerspencer

    I'll bite ...when are they hooking you guys up with one to track your daily movements from the Chicago office? image

     

    This form factor is certainly more useful that the Edison since it has actual connection points.

    Hopefully they can provide some more documentation.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>