Microchip
  • Products
  • Manufacturers
  • Microchip
  • More
  • Cancel
Microchip
Forum Need technical help from Microchip? Ask our Expert!
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Microchip to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 112 replies
  • Subscribers 31 subscribers
  • Views 11203 views
  • Users 0 members are here
  • help
  • microchip
  • expert
  • mike_mcglade
  • questions
Related

Need technical help from Microchip? Ask our Expert!

nlarson
nlarson over 16 years ago

This thread has been closed to new questions.

However, we welcome you to Post Your Question about Embedded in the element14 Community Embedded group. You'll find many fellow members and experts who have just the answer you're looking to find! 

 

Thank You, Your Friends at element14 Community

MikeMcGlade

Mike McGlade

Mike has 16 years of experience with Microchip products including MCU, Memory & Analog.  He also has significant knowledge of lighting, safety & security and vending industries.

 


  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    Hi

     

    Maybe you might want to look at this thread. image

     

    http://forums.hardwarezone.com.sg/showthread.php?p=49091874

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    Hi Mike

     

    I'm having some trouble with a bit of PIC assembly code running on a PIC16F722.  I am trying to use the Timer0 interrupt and the SSP module, in SPI mode.  The SSP module is communicating with an MCP23S17.

    The affected sections of the code are

     

              movlw     0x87                                 ;Put 0x87 in the working register

              movwf     OPTION_REG                   ;Copy the working register to the options register, Port B pull-ups disabled, Timer0 pre-scaler set to 256

     

    and

     

    SPI_Byte_Out:

              bcf          INTCON, GIE                    ;Disable all interrupts while transmitting
              movwf      SSPBUF                         ;Copy the working register to SSPBUF
              bsf          STATUS, RP0                  ;Access memory bank 1
              btfss       SSPSTAT, BF                  ;Check buffer full bit for end of transmission
              goto        $-1                                  ;Go to previous instruction until transmission is complete
              bcf          STATUS, RP0                  ;Access memory bank 0

              bsf          INTCON, GIE                   ;Re-enable all interrupts after transmission

              return

     

    When the first part of the code shown is commented out, or if the GIE bit is cleared, the SSP module functions reliably.  However when this part of the code is included, the SSP module doesn't function properly, with nothing output on the SO pin and the code hanging at the Buffer Full bit test.

    Have your encountered this before, or can you see what I'm doing wrong?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • MicrochipRTCfr
    MicrochipRTCfr over 15 years ago in reply to e14 Contributor

    Hi Mohasin,

     

    Do you use the latest Microchip Application Libraries containing the TCP/IP v5.25 or > ?

    It is essential to use the latest ones with your WiFi module as it contains updated firmware.

    After installing the libraries, you'll find several WiFi projects in the C:\Microchip Solutions v2010-08-04\ directory.

    There are some online webseminars on the TCPIP stack which you may want to listen to in order to understand how to interface your application with the TCP/IP stack.

     

    Another option is to attend the Microchip training dedicated to TCP/IP (webserver) ref COM4201 in one of the Microchip Regional Training Centers

     

    regards

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    hi

    i need to know the difference between  DM240001DM240001DM240002.DM240002.

    Does the DM240002.DM240002. support dspic as PIM or it  just for PIM PIC

     

    if it does not support how i can use dspic with DM240002.DM240002.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • KennyMillar
    KennyMillar over 15 years ago in reply to e14 Contributor

    See my reply to your original post.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to KennyMillar

    thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • samplerman
    samplerman over 15 years ago in reply to e14 Contributor

    Hi according to the Microchip website the  DM240001DM240001 caters for the 100pin PIMs be it PIC24 or dspic etc and the DM240002.DM240002. caters for the lower pin count 44 Pin PIMS as below:

     

    "The Explorer 16 Development Board is a low-cost modular development system for Microchips 16-bit microcontrollers It comes in two versions  DM240001DM240001 ships with the 100-pin PIMs and DM240002.DM240002. ships with the lower pin-count 44-pin PIMs"

     

    I hope this helps

    Carl

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    My notebook gone due to the break in, are there any application for tracking notebook or tv use microchip, lucky, they are not interesting my develop kit.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    Hi Mike:

     

    This code works good in simulation but in the real situation not works,the GP0 and GP1 is 0 V,Can you help me?. The compiler is CCS.

     

    thanks

     

    #include <12f629.h>
    #fuses HS,NOWDT,NOPROTECT,NOPUT                                   
    #use fast_io(a)
    #use delay(clock=20000000)
    void main()
    {
    set_tris_a(0b111100);
    output_a(0x00);
    while(1){
    output_high(PIN_A0);
    output_low(PIN_A1);
    delay_us(200);
    output_low(PIN_A0);
    output_low(PIN_A1);
    delay_us(300);
    output_low(PIN_A0);
    output_high(PIN_A1);
    delay_us(200);
    output_low(PIN_A0);
    output_low(PIN_A1);
    delay_us(300);
    }
    }

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    hi i want to buy the explorer 16 development board ...is it Necessary  to buy pickit2  which is part #DV164121

    im interested to control the whole board with pic18LF4550 (using USB )

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>