PCB Design, Prototyping and Production
  • Products & Partners
  • More
PCB Design, Prototyping and Production
PCB Blogs Experimentation with the UL 94V-0 designation of printed circuit boards
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join PCB Design, Prototyping and Production to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: wolfgangfriedrich
  • Date Created: 1 Oct 2023 3:55 PM Date Created
  • Views 5920 views
  • Likes 7 likes
  • Comments 8 comments
  • pcb
  • fire
  • fiberglass
  • 94V-0
  • very sad
Related
Recommended

Experimentation with the UL 94V-0 designation of printed circuit boards

wolfgangfriedrich
wolfgangfriedrich
1 Oct 2023

Disclaimer: This post is rated VS (very sad); continue reading at your own risk.

Extreme temperature testing is nothing a hobbyist is normally even thinking about. The 94V-0 flammability rating that is printed on most production PCBs basically states that the PCB (and only the PCB) would stop burning within 10 seconds after being subjected to vertical combustion. For more detailed reading about this topic, I recommend IEC 60695-11-10 and 60695-11-20 and ISO 9772 and 9773.

I had the opportunity to test all (ha!) my PCBs for flammability and wanted to share some results.

First up is a panelized small board. The disintegrated weaved fiberglass layers are nicely visible. Copper traces are totally gone, the green hue might be oxidized copper or leftovers from the blue soldermask. Colours behave funny in heat, I found a glass orb that used to be stained blue and now was completely clear. Original pictures of the small panel for comparison.

image image

image image

And here is one of my Pixi analog boards with holes, pads and traces still visible. Yes, this is an Arduino Uno shield, again with the original boards for comparison.

image

image image

Components also seem to be somewhat fire retardant. A unidentified board with visible skeletons of resistors and a TSSOP-20 chip. Not sure if they make good Halloween decorations.

image

Other interesting stuff:
A wire clipper, which btw won me a Rock'n Roll speaker to start my lab again.

image

Enamel coated cups and ceramics survived the best. Tools like pliers and tweezers, even stainless, not so much. And a dishwasher safe ceramic bowl in a not so happy dishwasher.

image image

Exact temperatures are not known as the test setup was rather random. But I have fund Pyrex bowls melted into blobs of glass or fused together in shape. Things like my beloved Metcal GT-120 soldering iron and 858D hot air pencil did not stand a chance and the trusted Tek MSO2024B simply disintegrated during the event.

GT-120 and 585D Disappointed :

image

This all happened to me earlier this year during the Tantallon wildfire in Nova Scotia, which burnt down 150 homes including mine.

Kids, listen. Data back-up is important, but it only works if it is off-site either on somebody else's computer (the cloud) or diligently managed by a swarm of carrier pigeons. Here is an ASUSTOR 1102 NAS drive with 2x 4TB hard-drives. I doubt any data recovery service is going to find any '1's and '0's in the correct order on this one.

image

If you are wondering why I even wrote this post; talking about it is part of the processing of the events and dealing with the aftermath in a (sort of) lighter way helps me moving forward. The old projects needed some sort of closure before I can move on, recreating some of them again or using this as an opportunity for doing something completely different. Thanks for reading.

 - W.
 

  • Sign in to reply

Top Comments

  • javagoza
    javagoza over 3 years ago +1
  • wolfgangfriedrich
    wolfgangfriedrich over 3 years ago in reply to shabaz

    Thanks for the kind words. It is a life changing event. Even though it will be with me forever, the good will prevail. The ugly happened and is gone and I will overcome the bad. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 3 years ago

    Sorry this happened : (

    I hope everything improves with your new home or rebuild, and I hope eventually you'll be so occupied with interesting projects and more enjoyable times that you won't look back on this event often at all.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • javagoza
    javagoza over 3 years ago

    Cry

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<