Hello I'm Matthew James Pitsicalis , and i belive that there should be a easy to use and open source device that can be as small as a tv stick but powerful and that could have a kit that can have a device that can be placed anywhere as a tv antenna and could be transmitting over wifi or cell data and could stream to the stick through wifi or cell data again and could dvr onto a micro sd card and has kodi built in, and is solar powered and that has the mycroft ai and has fm radio built in and has a easy to use ui and remote, and is small as a roku stick, and is affordable, has a hdmi on the other end. Please comment and help start this project because it would be nice to give a gift that you can make that can go on for a long time. AND THE FINAL THING IS I WANT IT TO BE POWERED BY THE RASPBERRY PI!!!
PLEASE HELP MAKE THIS PROJECT A REALITY