Raspberry Pi Projects
  • Products
  • Raspberry Pi
  • Raspberry Pi Projects
  • More
  • Cancel
Raspberry Pi Projects
Blog Hydrogen Fuel Cells!
  • Blog
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi Projects to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 2 Dec 2013 3:40 PM Date Created
  • Views 3760 views
  • Likes 5 likes
  • Comments 15 comments
  • endurance
  • autopilot
  • ardupilot
  • element14
  • hydrogen
  • control
  • UAV
  • matlab
  • raspberrypi
  • rpiexpert
  • rpi
  • fuel-cell
  • raspberry_pi_projects
  • adc
  • simulink
  • piface
Related
Recommended

Hydrogen Fuel Cells!

e14 Contributor
e14 Contributor
2 Dec 2013

Hydrogen fuel cells (in particular PEMFCs) are an exciting technology which has been around for a while now. Unfortunately, they haven't really take off (excuse the pun) due to their high cost, poor lifetime and slow transient performance.

 

1. So why are people still interested?

 

Well, firstly you have the good old "clean & green" argument. In operation, the take in oxygen (from the air) and hydrogen (the fuel), and give out heat, water and electricity. No carbon dioxide, monoxide, sulfides and other nasty things.

Secondly, they're not dependent on fossil fuels to run, and are currently the most promising energy generation technology that is independent of the elements (wind, solar, etc).

Hydrogen has a superb energy density, meaning not much weight gives you a huge endurance.

Fuel cells tend to have no moving parts, unless the have a cooling fan or air supply fan, so they are mechanically very simple.


2. So why aren't we using them?

 

They require platinum as a catalyst so make the chemical reactions work. Platinum is incredibly expensive, and more annoyingly it tends to be washed away over time which reduces the fuel cells lifespan.

They are slow to respond, so cruising along at 10% power, then suddenly demanding a full 100% may take anything from seconds, to minutes, to hours, depending on the type of fuel cell. This proves a big challenge in mechanical transport, such as planes, and cars.

Hydrogen is a pain in the rear, generally. To produce the high quantities we need, we can only do it (cost-effectively) by burning fossil fuels. Of course it can be generated using renewables (wind, solar, etc), but this is far too expensive at the moment for the industry to consider.

Hydrogen also is a pain to store. Because there are so few molecules in such a large amount of space (low density), you have to store it at tremendous pressures to get a usable quantity, which requires huge storage tanks. Not particularly practical in transport applications. There are other methods, but cost and practicality is still a huge issue.

 

3. Where do I fit in?

 

To start I am not a chemical engineer. However, I am a PhD researcher for the Hydrogen Fuel Cells & their Applications Doctoral Training Centre (DTC) in the United Kingdom, so I know a fair amount about it. By trade I am a autonomous control engineer, specialising in unmanned aerial vehicles (UAVs).

Given all the problems outlined above, even the suggestion of putting a fuel cell on a small UAV, which is essentially a modified off the shelf remote controlled hobby plane, seems crazy. But it is do-able, and has been done. The advantages for flight aren't the clean & green approach currently dominating the selling point of fuel cells, but that key word "endurance". To fly for 10 hours, a UAV would have too many batteries to float, let alone fly, but with hydrogen's energy density this may well be possible. That's what I'm going to find out.

 

4. So that's nearly 500 words with no raspberryPi?

 

Haha, hopefully I have set the scene now. Let's talk about the electronics!

The fuel cell is a dumb system. It's just a contained and continuous chemical reaction. But it can be controlled through the hydrogen supply, the load and the temperature. I can overcome the poor transient performance if I know that "soon" I will need full power; I can simply crank the fuel cell up, dump the excess power, then when the time comes, 100% is there to give. Sounds wasteful, but it turns this fuel cell into something useful. To control the logic we need a computer. On a small UAV the raspberryPi is ideal, in terms of size, power (in & out), flexibility and functionality.

Running a Real Time Operating System (RTOS) is a seriously useful tool, which I could not do on my work last year (using Arduino). I can programme in any language, use other peoples software (eg the camera) and share my code with the world (and myself for backup!) on GitHub.

So far I am using several add-ons including the MATLAB/SIMULINK support (to help the academics!), rPi Camera, delta-sigma-pi I2C ADC, piFace SPI Digital IO, TMP102 I2C temperature sensors and have the whole lot connected to an onboard UAV autopilot.

 

At risk of making this essay any longer, I'll wrap up now. I hope this is something that tickles your interest, and keep tuned for some videos, pictures tutorials and demos in the coming weeks. In the meantime, if you are interested in the plane the check out my page on diydrones.

 

Simon

_________________________________

S HOWROYD MEng (Hons) RAFVR(T)

Academic Researcher

Fuel Cells in Unmanned Vehicles

Autonomous Systems Specialist

Aeronautical & Automotive Engineering

Loughborough University

 

image

  • Sign in to reply

Top Comments

  • DAB
    DAB over 12 years ago in reply to rodreig89kishore +1
    Hi Kishore, Hydrogen is actually much safer than current gasoline and easier to use than ethanol. Most of the hysteria stems from the vivid pictures of the Hindenburg, but analysis has shown that it was…
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to rodreig89kishore +1
    Hi Kishore, Liquid hydrogen is a whole world of issues due to it's boil off and therefore safety due to over-pressuring. This is the "risky" nature of hydrogen you talk about. Not to get confused with…
  • DAB
    DAB over 12 years ago in reply to e14 Contributor +1
    Hi Simon, I dabble in a lot of technology areas. We should soon have more efficient processes for energy extraction and conversion. My new book. "I Killed Schrodingers Cat!," will open many new research…
  • rodreig89kishore
    rodreig89kishore over 12 years ago in reply to DAB

    True that DAB. We cannot fight public hysteria.

     

    If I am not wrong it must be the hysteria that mixed with true facts that led me to believe that hydrogen is a much dangerous gas than it is.
    Well you cleared another doubt too. Gelly wont work. image

     

    Well that is another start for me then.
    TY for your input DAB.

     

    I like to learn more.
    Now that my notion has been dispelled about hydrogen  I'd like some more info on it.

     

    Wikipedia and Google search doesn't make the cut. lol image
    I would like to find more solutions for the environment.

     

    Keep feeding me the info. Learning is what I do.

     

    To protect the environment that I love the most. image

     

    Thank You DAB again.

     

    P. KISHORE KUMAR

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • rodreig89kishore
    rodreig89kishore over 12 years ago in reply to e14 Contributor

    TY image Simon for giving more insight on Hydrogen.

     

    All I used was basic stuff to formulate such notion. I am glad and humbled by your opinion.I need more info on it to learn more on it.It is good that you have the knowledge and I don't
    To learn is my ultimate goal.:D
    You mentioned about a paper.Can you mail it to me.
    I would love to study more on this subject.
    I like the environment cleaner, better, and more efficient. image
    Please keep me posted. image

    Thank You.


    P.KISHORE KUMAR

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 12 years ago in reply to e14 Contributor

    Hi Simon,

     

    I dabble in a lot of technology areas.

    We should soon have more efficient processes for energy extraction and conversion.

    My new book. "I Killed Schrodingers Cat!," will open many new research areas into how we can manipulate atoms and charge transmissions to much higher efficiencies.

    So keep watching, we are about to enter a new era.

     

    DAB


    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 12 years ago in reply to johnbeetem

    John there is nothing free!

    Solar and wind energy have a large up front cost and a fair amount of maintenance.

    There is a break even point, but we need to treble the efficiency factors before they can be relied upon for the mass market.

    Hydrogen is ubiquitous and the most GREEN fuel available.  Even without the fuel cell, hydrogen is a very sensible way to go for energy.

    Plus, with a very extensive natural gas pipeline infrastructure in place, it would be very easy to have home fueling stations for those of us already using natural gas.

    A gas station might be 20th century, but it will still be the norm for a good part of the 21st century as well.

     

    DAB


    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • johnbeetem
    johnbeetem over 12 years ago in reply to e14 Contributor

    One way is to use hydrogen to store excess energy produced by your solar panels and/or wind turbine.  Then when you need it, you can convert the hydrogen back to electricity, or transfer it into your car as a range extender.  Having to drive to a gas station (whatever gas) is so 20th Century.  Why use fossil fuels when solar and/or wind energy is delivered to your home for free?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>