Raspberry Pi Projects
  • Products
  • Raspberry Pi
  • Raspberry Pi Projects
  • More
  • Cancel
Raspberry Pi Projects
Blog PIK3A Retro Gaming Table Mk II
  • Blog
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi Projects to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: spannerspencer
  • Date Created: 22 Mar 2016 10:45 AM Date Created
  • Views 18283 views
  • Likes 12 likes
  • Comments 44 comments
  • retro gaming
  • rpibeginner
  • retro
  • pi3
  • pik3a
  • raspberry pi
  • raspberry_pi_projects
Related
Recommended

PIK3A Retro Gaming Table Mk II

spannerspencer
spannerspencer
22 Mar 2016

I'm not a fan of Ikea. In fact, it's a place I usually try to avoid, until I discovered that you can hack it's ultra-cheap tables into retro video game systems! You know the one I mean: PIK3A: The Raspberry Pi 3 IKEA Retro Gaming Table.

 

You guys have been busy making your own versions, which I'm thrilled to be reading about. Keep those photos and top tips coming.

 

But in the meantime, meet PIK3A Mark II.

image

Hackin' the LACK

This is, in many respects, the same build as the PIK3A Mk I. The idea came about when I initially bought the square LACK tables that we mounted a monitor in, and added controls to. I was casually keeping an eye out for a table that'd accommodate two players, with six buttons each. You know. A Street Fighter II machine!image

 

There were definitely options, but the table size makes them prohibitively intrusive for the average living room. So I needed a way to reduce it, while maintaining the full control set.

 

The answer presented itself in the LACK TV stand; a narrow, 90cm by 26cm table that boasts a shelf and a table top deep enough to accept the joysticks and buttons. By dispensing with the monitor and going straight into the TV, the unit is easily accommodated in your average (well, as average as us element14 types ever really are) front room.

 

There isn't much to explain about the build that isn't already covered in the PIK3A Mk I. I cut two access holes in the bottom so I could get to the joystick and buttons for each player, and drilled start and coin buttons into the edge as before.

image

I kept the Raspberry Pi 3 external, mounting it in a case underneath the table top, in the centre. It's still nicely hidden, and there's only a short length of USB cable from the controls into the RPi. The benefits of this are that you don't need any extensions or panel mount connectors for the micro USB input or HDMI output. It also makes it easy to get to the SD card, should you need to.

 

There's no need for any acrylic or polycarbonate sheeting over the top either, given that there's no screen, making this a quick, simple yet highly effective variation on the PIK3A.

 

That said, one nice tweak might be coming up with a way to eliminate the HDMI cable and send the video to the TV wirelessly. Any thoughts on that?

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply

Top Comments

  • bwelsby
    bwelsby over 10 years ago in reply to shabaz +2
    Hm yes 12 inputs may not be enough, how about another hack... as in hack a genuine bluetooth keyboard
  • e14 Contributor
    e14 Contributor over 10 years ago +2
    You can hack a LG an-wl100 to wireless transmit HDMI and you can buy them for around 15 bucks on eBay. Directions for hacking Hacking the LG Wireless Media Kit AN-WL100W . Not a compact solution but it…
  • ipv1
    ipv1 over 10 years ago +1
    Awesome man!
  • spannerspencer
    spannerspencer over 10 years ago in reply to shabaz

    Ah, this is an interesting twist! It hadn't occurred to me that the RPi could go behind the TV, and then just use the table as a Bluetooth controller. That's inspired!

     

    What I'm currently using as an encoder for the controls is a small board that came with the joystick and buttons bundle. It identified itself as two standard gamepads. But that could be swapped for something else that has Bluetooth, I guess?

     

    Any thoughts on what'd be a good device to go with for this?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • bwelsby
    bwelsby over 10 years ago

    Nice one. 

    How about moving the RPi to the TV and adding bluetooth to the arduino so it acts as bluetooth kb & mouse.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 10 years ago

    Hi!

    Another nice design!

    Maybe install another 'Pi behind the TV, and run the RetroPi on that, and then something like this:

    networking - Linux: Share keyboard over network - Super User 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ipv1
    ipv1 over 10 years ago

    Awesome man!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<