Raspberry Pi Projects
  • Products
  • Raspberry Pi
  • Raspberry Pi Projects
  • More
  • Cancel
Raspberry Pi Projects
Blog Raspberry PI 4 Water Cooling
  • Blog
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi Projects to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: feiticeir0
  • Date Created: 9 Sep 2022 9:52 AM Date Created
  • Views 4832 views
  • Likes 13 likes
  • Comments 6 comments
  • Water Cooling
  • Raspberry PI Water Cooled
  • raspberry pi 4 water cooled
  • Raspberry PI 4 Water cooling
  • Raspberry PI Water Cooling
  • raspberry_pi_projects
Related
Recommended

Raspberry PI 4 Water Cooling

feiticeir0
feiticeir0
9 Sep 2022

Hi all ! Hope everyone is well.

Just want to share my latest project - a water cooled Raspberry PI.

Why ? Well, since I was a teenager (I'm from the 80s) that I wanted to have a Water cooled Desktop PC.  I first saw one in 2004 at a Lan Party (- Remember those ? Smiley) of a friend of mine and I was in awe.

At that time I didn't have the resources to make one and let's be honest, there wasn't much offer like it is today and what was available, was way to expensive for me.

But now, times are different and, before I create a desktop version, why not put my Raspberry PI 4 (that's running Home Assistant and Ubiquiti Software for the Network management) with a water cooled setup ?

Here it is:

Water Cooled RPiWater Cooled RPi

Water Cooled RPIWater Cooled RPi

Components

My goal was to have the smaller setup I could do. This is already a bit overkill, but nonetheless, it was fun.

For a minimal water cooled setup - scaled for the RPi - we need:

  • Reservoir for the cooling liquid (I ended up using a small plastic container that I had)
  • Submersible pump (the standard setups for bigger PCs it's common for the pump to come with the reservoir all in one).
  • Water cooling block
  • Radiator
  • Thermal Pad to sit between the water cooling block and the RPi
  • Fan
  • Hose (I'm using 10mm diameter outside and 8mm inside)

Fan Radiator

Setup

I've taken care to choose components that would fit and used 3v or 5v - enough to be powered by the Raspberry PI.

The Pump is 5v and small enough to fit inside the container. Because the pump nozzle is a bit smaller, I had to use a zip tie to firmly secure the hose.

The Fan is 60mm, enough to be paired with the Radiator - that's is also 60mm . This will cool the liquid as it passes through the radiator.

The water cooling block is 40x40mm . I had to file the sides a bit for it to sit between the DSI connectors of the camera and the display. I had care not to file to much or I could have a leak.

All (except the pump) the components connectors and 9mm/10mm for the hose to fit tight.

Before mounting the RPi, I've connected everything and start pumping to see if no leaks were present.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

It's working for 12 hours now and has been all night and I've placed a piece of white paper between the setup and the table to see if it leaked... For now, I'm safe. !

I know it's a bit overkill for just running Home Assistant and Ubiquiti software, but I'll probably move that to another RPi and will have a bit of fun overclocking it just to see how far it will go !

Happy projects.

  • Sign in to reply
  • milosrasic98
    milosrasic98 over 4 years ago

    This is such an amazing setup, thanks for sharing the parts you've used! I'm going to give this a go for sure at one point, hopefully soon!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<