Raspberry Pi Projects
  • Products & Partners
  • Raspberry Pi
  • Raspberry Pi Projects
  • More
  • Cancel
Raspberry Pi Projects
Blog Raspberry Pi BLE and WiFi Internet Radio
  • Blog
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi Projects to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fmilburn
  • Date Created: 17 Jun 2022 4:51 AM Date Created
  • Views 7080 views
  • Likes 18 likes
  • Comments 17 comments
  • ble
  • wifi
  • volumio
  • radio
  • raspberry pi
  • music
  • moode
  • internet radio
  • streaming
Related
Recommended

Raspberry Pi BLE and WiFi Internet Radio

fmilburn
fmilburn
17 Jun 2022

My brother who is a wood working enthusiast asked me about electronics for making a BLE speaker box with the form factor of a mid-century table top radio.  His inspiration, which I really like, is this:

Old School Radio

He had found a BLE receiver / amp with 2" speakers and wanted some thoughts on adding some electronic bling and 3D printed parts help.  I told him sure, but we could do better.  My suggestion was to add internet radio capability and music storage to the BLE and use a Raspberry Pi (i.e. feature creep).  I found an inexpensive 25W amplifier hat on Amazon which purports to have a Texas Instruments (Burr-Brown) TAS5713 chipset with Nichicon capacitors and two days later it was in my possession.

image

An unused Raspberry Pi 3B was pressed into service.  The new hat can take anywhere from 12 to 20V as input and will also power the Pi so an old 20V laptop power brick was attached to the hat.  For now a pair of old, but relatively high quality, bookshelf speakers from the junk box were hooked up.  This is what it looks like:

Test Setup

There are a number of apps and resources on line to do this with a Raspberry Pi. Volumio and Moode were selected for further evaluation.  Both have a modified OS that is downloaded and installed on the Pi and web based interfaces.  Volumio has free and paid versions but BLE is only available with the paid version.  A quick look at the github page shows it hasn't had recent updates.

Moode has frequent updates and what appears to be an active forum. It is also open source and free.  I thought the Volumio User Interface was a bit slicker but otherwise Moode was a better fit for this project. 

This is what the Moode web interface looks like running on my iPad:

Moode Web Interface on iPad

It sounds great to my tone deaf ears that have high end frequency loss mixed with tinnitus.  The web interface is a bit clunky and some modifications to the software require SSH into a headless Pi which isn't that great for an unsophisticated user.  Hopefully it can be set up beforehand so my brother doesn't have to fool with it.

The next step is to add physical features for installation on the cabinet in addition to the web interface as shown in the clouded section of the block diagram below:

image

Namely:

  • On / off switch
  • Manual volume control
  • Source control (e.g. internet radio, BLE, loaded files)
  • Small display

These capabilities aren't included in the application as downloaded but I've been browsing through the Moode forum and it appears all can be done since the OS is Raspbian based and accessible.

We aren't trying to get audiophile performance.  Nonetheless, I would appreciate any suggestions others might have on both hardware and software as I've not attempted something like this before.

  • Sign in to reply
  • BigG
    BigG over 4 years ago

    I was curious about your two choices, so I've been reading through the docs. I see Volumio is Javascript based while Moode is developed using PHP. According to Volumio docs it uses Websockets to receive commands. There is also a GitHub repository for the Volumio backend and the UI. Similarly for Moode, there's also a GitHUb repository. According to Moode GitHub page, the PHP based Moode Audio Player is a derivative of the WebUI audio player client for MPD.

    Interestingly, if you search online you can find quite a few Python MPD options, like this client option: https://pypi.org/project/Mopidy-Simple-Webclient/

    That is for https://mopidy.com/

    Personally, I think Python or Javascript would give you better developer options than PHP on a Raspberry Pi, if you want to use Bluetooth.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • robogary
    robogary over 4 years ago

    For the mechanical dial display, I've seen other projects use a servo to drive the meter needle. The servo would be behind the dial, with an axle extending thru to mount the needle on. The dial backplate and needle can be 3D printed or scavenged from a junker. If the website doesnt have a frequency display, just make one up and have the RPi use that value on the dial anytime that web-station is selected. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<