Raspberry Pi Projects
  • Products
  • Raspberry Pi
  • Raspberry Pi Projects
  • More
  • Cancel
Raspberry Pi Projects
Blog Sleepy Pi Overview
  • Blog
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi Projects to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 14 Dec 2013 4:17 PM Date Created
  • Views 4951 views
  • Likes 4 likes
  • Comments 7 comments
  • raspberry
  • raspi
  • raspberrypi
  • raspberry_pi_projects
Related
Recommended

Sleepy Pi Overview

shabaz
shabaz
14 Dec 2013

Introduction

The Sleepy Pi is a board produced not a million miles from my home town, and it is designed to extend the Raspberry Pi (RPI) capabilities. After having examined it, the conclusion is that the board is fantastic with a rich set of functionality and extremely well-designed, and it will provide tremendous value for projects with the types of requirements listed below.

image

This board should interest people with any of these requirements:

1.    The ability to run the RPI from a battery

2.    The ability to run the RPI intermittently (based on events or time), perhaps over days/months from a remote location

3.    Interface to hardware and run microcontroller code

4.    Use existing Arduino compatible boards

5.    The ability to keep time without a time server on the Internet

It opens up some unique opportunities.  For example you could shut down the RPI, collect data using the far lower power  in-built microcontroller on the Sleepy Pi, and then periodically wake up the RPI and send the data to a server. The RPI could run for days/weeks/months like this at a remote location.

 

Main Features

The main features are:

1.    Provide battery backed up clock (it has a socket for a watch type cell)

2.    Provide efficient, regulated power to the RPI (there is a built-in DC-DC converter and a DC barrel socket) – or use your existing power supply (there is a USB socket for that)

3.    Allow the RPI to be put to a ‘deep sleep’ (power off) and awakened at certain defined times or when a particular event (analog or digital input) occurs

4.    Allows external hardware to receive a switched power supply, so that it can be put to sleep too

You can see the RTC back-up battery socket on the underside (battery not supplied due to postal restrictions - a CR1632 cell is needed for enabling that capability):

image

The diagram here is from the Sleepy Pi website:

image

This photo shows the mapping of where bits of functionality are located on the board:

image

Owing to its design, it has some very attractive additional advantages:

1.    Arduino compatible boards can be plugged in on top, for extending usefulness

2.    There is an on-board Atmel AVR microcontroller – on of the world’s most popular microcontrollers – which allows for some relatively high speed interfacing to hardware without the varying latency that Linux would incur

3.    Decent area for prototyping – saves an additional board

4.    Built-in ADC (in the AVR chip) for connecting to analog sensors (two 10-bit analog channels)

5.    Additional 'peripherals' available inside the AVR chip, such as PWM for controlling analog devices or for light dimming/motor control (requires additional circuitry)

 

Design Overview

There are many bad and good boards out there, this one falls in the extremely good category.

Hardware Design

The design is really nice – the list of good points seems endless: sensibly, it is a rectangular board without strange cut-outs (which save little space and wouldn’t allow the PCB to fit many cases anyway) so it allows for a usable prototyping area which is really nice. There is space for screw terminals and Arduino headers. All connections are well labelled.

Many connectors are supplied, so you can use the board as you wish. The existing RPI 26-pin connector is not totally consumed and lost; there is an inline header so that additional boards could in theory become part of the sandwich.

The board is securely fastened to the RPI using hex spacers (you will need a 2.5mm hex driver for the supplied bolts). As a design suggestion, perhaps some more holes on the Sleepy Pi would be good, so that it can be bolted into a case. Extra holes may be hard to implement because the board is so packed. A good workaround is to use hex spacers with male thread on one end, so it is a very minor point.

It is nice that decent hex bolts are supplied (this controls the amount of space the head consumes around the board) and insulating washers for the paranoid (like me). I’m really struggling to find a bad point about the Sleepy Pi.

I’d suggest one additional hole, so that it can finally fix the RPI weakness of two holes, since a total of three holes will allow it to firmly be fixed to a surface.

As another suggestion, perhaps a couple of very small holes near the battery, so that it can be tied down if desired and not vibrate/drop out (people may use the Sleepy Pi in some extreme conditions), especially since it is on the underside of the board.

As far as I can tell, the board does not foul up any existing connector on the RPI, including the camera connector.

AVR Microcontroller (Arduino)

In normal (expected) use, no additional hardware is needed and you will be able to run Arduino code directly on the Sleepy Pi.

If required, there is a 6-pin Atmel AVR header for an external programmer. This will allow you to run code written without Arduino support too.

Note that as far as I can tell, the board could in theory even be used independently of the RPI. So, if you happen to need an AVR microcontroller and RTC and DC-DC supply to power your electronic circuit, then this board could be useful for that purpose too.

If you don’t wish to go Arduino-mode and wish to program the AVR yourself, then a programmer is available for under £20($30) (Olimex AVR-ISP-MK2) from Farnell/Newark and it will plug in directly to the Sleepy Pi. I’ve not used it, but it is worth a try – since the Atmel version AVR-ISP 2 is a little tricky sometimes to set up with Windows 7.

The AVR is a great introduction to microcontrollers and has so many uses and existing code snippets available all over the Internet.

Circuit Design

Looking at the schematic, it all looks very nice – decent protection on the power inputs, very good power control using MOSFETs (with protection too), unlike some RPI power control designs which use relays, and the design looks an extremely good quality (a few tantalum, and mainly ceramic caps everywhere as expected for this type of design) and decent modern component selection everywhere.

This is the type of design someone would do for themselves and be proud of the result, rather than a design intended for sale at a reduced price point with a compromised quality.

In the spirit of open source, the schematic is available and any code is on Github. This is a really important because many RPI boards are intended for educational use yet the creators hide the design (maybe they should be named and shamed!) because so much can be learned from looking at the design detail.

Prototyping Area

The prototyping area is of the round isolated rings variety, which is amongst the most useful – it can be used for through-hole parts but also for soldering up surface-mount devices sometimes and joined with thin bare wire.

 

Summary

It is no surprise if you’ve read the above - this is an impressive board. It is well designed and packed with features. The cost may seem high (£36.99 including VAT) but it does what you would previously have needed several boards to do, and good parts cost money - the design is of a very high quality.

  • Sign in to reply

Top Comments

  • mcb1
    mcb1 over 12 years ago +1
    Shabaz Nice writeup, and the features are exactly what I had planned for my Remote Web camera , but needed quite a few boards and connections to achieve. Jonathon has done very well, and anyone wanting…
  • e14 Contributor
    e14 Contributor over 12 years ago +1
    Two comments on the battery: CR2032 would have been better. Partly this is due to the postal stupidity in the UK where you now need a 10 quid courier delivery for a 50p battery, but also because it's fairly…
  • Nate1616
    Nate1616 over 12 years ago +1
    Very nice blog Shabaz. I have also had the opportunity to test this board and must say this is a great add-on to the Raspberry Pi. I did have an issue with using a usb GSM module but would say that its…
  • e14 Contributor
    e14 Contributor over 12 years ago

    Two comments on the battery:

    CR2032 would have been better. Partly this is due to the postal stupidity in the UK where you now need a 10 quid courier delivery for a 50p battery, but also because it's fairly easy to get CR2032's as they're much more commonly used that other sizes. I can get them at my local newsagent for example..

     

    Second, did you try to remove the battery from the holder ?  I use that same style of holder for 2032's and it takes a significant amount of force to get the battery out. Some people will find they need an (insulated) tool to lever them out. So I'm doubtful of the need to tie the the battery in.

     

    Two things I'd have liked:

    1. a connection to the rev 2 Pi's reset connection

    2. both reset and power on/off available on headers rather than only switches

     

    the first of these lets the AVR be an external watchdog, the second means you can have full external control.

     

    The switching regulator with a wide input range was something the Pi could have done with from day one, but as the Sleepy Pi actually costs more than the Pi itself, I think it's understandable that the RPF didn't add all of these features.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 12 years ago

    Shabaz

    Nice writeup, and the features are exactly what I had planned for my Remote Web camera, but needed quite a few boards and connections to achieve.

     

    Jonathon has done very well, and anyone wanting one should head here.  http://spellfoundry.com/products/sleepy-pi/

     

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<