RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Here's Why I think You Should Consider Applying for the MAX32650 EV Kit RoadTest
  • Blogs
  • RoadTest Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 12 replies
  • Subscribers 2668 subscribers
  • Views 1884 views
  • Users 0 members are here
  • maxim integrated
Related

Here's Why I think You Should Consider Applying for the MAX32650 EV Kit RoadTest

rscasny
rscasny over 6 years ago

I know I have been getting a lot of fantastic products lately to roadtest. It's kind of pre-Holiday wishlist!

 

But there's one roadtest, I'd like you to take another loook at: Maxim MAX32650-EVKIT

 

The Ev kit is from Maximum Integrated. this kit is for the MAX32650.image

 

The MAX32650 ultra-low power memory scalable microcontroller designed specifically for high performance battery powered applications. It is often used with industrial sensors, IoT, sports watches, fitness monitors, wearable medical patches and portable medical devices.

 

Here's some more information on the MAX32650.

 

The MAX32650 is part of Maxim Integrated's DARMAN Series of low-power microcontrollers. They are smart, with the biggest memories in their class and a massively scalable memory architecture. They run forever, thanks to wearable-grade power technology. They are also tough enough to withstand the most advanced cyberattacks.

 

These ultra low-power microcontrollers are designed to handle the complex applications demanded by today’s advanced battery-powered devices and wireless sensors.They are based on ArmRegistered CortexRegistered-M4 with FPU CPU with 3MB flash and 1MB SRAM. Memory scalability is supported with multiple memory-expansion interfaces, including a HyperBusTm/XccelaTm DDR interface and two SPI execute in place (SPIX) interfaces. A secure digital interface supports external high-speed memory cards, including SD, SDIO, MMC, SDHC, and microSDTm

 

Here's some tech specs:

  • 120MHz Arm Cortex-M4 with FPU
  • SmartDMA Provides Background Memory Transfers with Programmable Data Processing
  • 120MHz High-Speed and 40MHz Low-Power Oscillators
  • 7.3728MHz Low Power Oscillators
  • 32.768kHz and RTC Clock (Requires External Crystal)
  • 8kHz Always-on Ultra-Low Power Oscillator
  • 3MB Internal Flash, 1MB Internal SRAM
  • 104µW/MHz Executing from Cache at 1.1V
  • Five Low Power Modes: Active, Sleep, Background, Deep-Sleep, and Backup
  • 1.8V and 3.3V I/O with No Level Translators

 

Here's some documentation: https://datasheets.maximintegrated.com/en/ds/MAX32650-EVKIT.pdf

 

 

If you do have the time, fill out an application here:  Maxim MAX32650-EVKIT

  • Sign in to reply
  • Cancel

Top Replies

  • Jan Cumps
    Jan Cumps over 6 years ago in reply to genebren +4
    genebren , I was pleasantly pleased when reviewing the MAX32660 for that RoadTest - my first encounter with Maxim. The family has some very nice sleep, deep sleep and coma power modes - and the 1.8 V option…
  • michaelkellett
    michaelkellett over 6 years ago +3
    I think it's the DARWIN family It's an interesting, if slightly odd, beast - the processor is capable of very low power operation but can work with masses of external (and much higher power) memory. It…
  • genebren
    genebren over 6 years ago +3
    I have never been a big fan of the MAXIM parts, as I find their pricing to be on the high side. Also, I like to work with components that are a little more hand soldering friendly. When I think about the…
  • skywalker1211
    skywalker1211 over 6 years ago

    great EV Kit equip with low power, large memory controller.

    i was looking for similar spec mcu few years back for eink price tag. i think this is good fit to the application.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • noorpuri
    noorpuri over 6 years ago

    I have attended an Microchip workshop in the Darmstad Germany  related to MAX32650. It is much best for very low power embedded product development. And also, it has equipped with a very nice embedded software framework.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
<