RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum If you had a Altera Cyclone IV Dev Kit, what would you build?
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 44 replies
  • Subscribers 2762 subscribers
  • Views 4901 views
  • Users 0 members are here
Related

If you had a Altera Cyclone IV Dev Kit, what would you build?

awinning
awinning over 16 years ago

Hi,

 

As mentioned in the RoadTest for the DK-STRT-4CGX15N-0B Dev kit, we would like you to tell us what you would build if you had the opportunity. When the RoadTest closes I will choose a short list and create a poll for you to vote in. Winners of the poll will receive the kits,

 

Good Luck,

Ally

  • Sign in to reply
  • Cancel
  • blakme
    blakme over 16 years ago in reply to e14 Contributor

    Even I would like to vouch for one review like Kenny described.

     

    I guess it would be reasonable to give some time for others to come up with proposals. But personally i dont prefer the rules changing in the midway

     

    Thanks,

    Lakshmi

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago in reply to KennyMillar

    I would vouch for at least one review like Kenny described.

     

    That would provide other users valuable info on how FPGAs can be used and where they can provide advantage.

     

    For that existing projects are required to have a good comparison available.

     

     

     

     

     

    Elias

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • KennyMillar
    KennyMillar over 16 years ago in reply to awinning

    Having read the documentation (again) I think the Cyclone IV Transceiver dev kit is already a complete product - and the software which is bundled with it is suitable for evaluating the main Cyclone chip on board.

     

    I think it'd be better described as an eval kit - although for advanced users with PCI Express experience it is also a dev kit.

     

    Having said all that, I do think it's an interesting kit. It has the FPGA and a CPLD and USB Blaster all on board.

     

    So If I had an Altera Cyclone IV Dev Kit, here is what I'd do with it:

     

    I'd use the kit to learn more about FPGA devices and CPLD devices; I'd look at some of the projects which I've built over the past few years and see how easily any of them could be boiled down to a single FPGA rather than the dozens of components normally used; I'd look at their suitability for replacing glue logic in digital circuits, and even if they have any mixed signal capabilities.

     

    For the E-14 community, I would 'blog' from time to time on the learning process, the toolset and the results. I'd blog about the difference bewteen conventional microcontollers + glue and FPGAs; and I'd blog about the pros and cons of each. Maybe i'd even look at the 'FP' part of FPGA and discuss the theory versus the practicality of using one.

     

    So that's my proposal. :-)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • awinning
    awinning over 16 years ago in reply to blakme

    Hi Lakshmi,

     

    Thanks for the reminder, I am actually wondering how to proceed.

     

    I have had a talk with Altera, and they think it is a really specialized kit as some of the guys on the thread mentioned. So I am thinking I should re-open the test for a week or so with no limitations and draw as normal, rather than hold a vote as I had planned. But then I don't like changing the rules halfway through anything.

     

    What do you think?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • blakme
    blakme over 16 years ago in reply to e14 Contributor

    Hi Alistair,

    Is there any update to the Road Test?....

     

    Thanks,

    Lakshmi

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago
    Hi,

    Working for the first time with an Altera FPGA, the first thing to be done is blinking a led.

    After becoming familiar with it, I would try to develop the following projects:
    1. Network Stress Tester - a high speed packet generator designed to test networking equipments under heavy load (eg. many small packets).
    2. A high performance hardware firewall - designed as a PCI-e ethernet controller with configurable packet filters that take advantage of the FPGA to offload the host PC. This could be used to protect servers or networks against denial of service attacks (for example very many small packets could produce heavy load for a software router, but a FPGA could filter them without much effort).

    I am a student in fourth year at Applied Electronics. I have worked with Xilinx FPGAs before but I never worked with one from Altera.
    Having some networking experience, mostly software, I saw many times a server overwhelmed by heavy network load. That's why I thought about a hardware networking project.
    I don't know many things about low-level networking and PCI-e, receiving some advice from an Altera application engineer would be great.


    Bogdan-Florin Florea
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • firatkocak
    firatkocak over 16 years ago in reply to awinning

    Hi Alistair,

     

    I thought too much and decided not to attend this event. Because my project needs too much time to be spared nd i don't have so much time for the project. So i don't want other members to vote for a project that will probably not come to an end.

     

    But, i still believe that my idea is not totally "Not Applicable". With some necessary external components, it is an achievable project. Just i don't have time for it.

     

    Firat

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • KennyMillar
    KennyMillar over 16 years ago in reply to e14 Contributor

    Phil,

     

    I've read through the getting started guide and the reference guide for that board a few times now, and am racking my brains for a good use for it.

    The best I've came up with so far is programming it to play a networked game of PONG on it's LCD, with two players connected via telnet!

     

    I'm not mocking the device at all - it has Gb ethernet, FPGA and CPLD along with a MAX processor for JTAG debugging - we just need to think a bit laterally and come up with something better than just measuring the BER on it's tranceiver image

     

    I think I'll start by looking at what Blocks are available for it and see if something jumps out at me from there. 

     

    -Kenny

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago in reply to KennyMillar

    That'll teach me to skip ahead!

     

    I didn't realise this was a PCIe dev board. In which case, my Altera DE1 board is probably FAR more suitable as a dev platform for the printer.

     

    Going by the specs for the board, the only things that are coming to mind are "Ethernet controller" and... well... "Ethernet controller." Seems like a bit of a one-trick pony to me.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • KennyMillar
    KennyMillar over 16 years ago in reply to e14 Contributor

    Phil et al,

     

    These sound like great ideas, but I can't see how they'd fit around a Cyclone IV ?

     

    It has very limited i/o in it's standard form and to get enough analog / digital interfaces onto it you'd need to build almost as much hardware again and attach it to the Express connector. (Unless I have missed something in the spec!).

     

    One other thing we should bear in mind with this kit (and please someone correct me if I am wrong) is that as-shipped the transceiver is connected to the Ethernet PHY interface, and requires microsurgery on microscopic SMD components to move the transceiver to the SMA connectors.

     

    There is another transceiver connected to the Express connector - but to interface to that would require some pretty advanced logic - or bung it in a suitably equipped PC and write some low level device drivers for it!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>