RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum If you had a Altera Cyclone IV Dev Kit, what would you build?
  • Blogs
  • RoadTest Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 44 replies
  • Subscribers 2675 subscribers
  • Views 4284 views
  • Users 0 members are here
Related

If you had a Altera Cyclone IV Dev Kit, what would you build?

awinning
awinning over 15 years ago

Hi,

 

As mentioned in the RoadTest for the DK-STRT-4CGX15N-0B Dev kit, we would like you to tell us what you would build if you had the opportunity. When the RoadTest closes I will choose a short list and create a poll for you to vote in. Winners of the poll will receive the kits,

 

Good Luck,

Ally

  • Sign in to reply
  • Cancel
  • awinning
    awinning over 15 years ago in reply to firatkocak

    Hey Firat,

     

    We will be looking into August before we do the poll and possibly late August before it finishes, so one thing you have is time to decide, whether to cointinue, withdraw, or even change plans. So no need to stress at the moment. We have a good bunch of guys on the group, so I think you should be able to get help with decisions, prgramming, almost anything on the project. For extra equipment for the test, I may be able to help somewhat, but think an extra dev kit may be a bit much. I believe the Cyclone IV is the most expensive kit we have ever done.

     

    I'm not sure if this would work but could you build either a TX or an RX and use a generic PC WiFi modem for the other half of the test?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • firatkocak
    firatkocak over 15 years ago in reply to awinning

    Hi Alistair,

     

    Nothing is impossible, it is just a matter of time image

     

    I may think of designing a loopback system which receives source video signal from one channel and sends the received video signal to the any other available channel. So, with this way, i can eleminate the use of secondary Cyclon kit.

     

    I will seriously think about my project and make a final decision. Thank you very much.

     

    Firat

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 15 years ago

    I don't agree with those video/wireless ideas. They are not realistic.

     

    I will go for a high speed SPI/IIC Flash programmer. Most SPI/IIC programmers in the market are based on MCUs running below 24M. They are very slow for the big devices(like Spansion 128Mbit SPI Flash). With the help of FPGA, the clock can go above 100M easily.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • ar_sys
    ar_sys over 15 years ago in reply to Former Member

    Hi Eddie, 
     
    Why you want kill a mosquito with a bazooka ?  image 
    A fast SPI write engine require less than 500 LUT . You can use a 50$ FPGA starter board. 
     
    Also I think that the sector-erase and block-write time  is the major cause of slow programming of SPI memory chip. Change clock from 20Mhz  to 100 Mhz do not obtain a great write-time gain.

     

    -Alessandro

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • WarrenW
    WarrenW over 15 years ago
    I honestly have no idea. Looking at some of the other suggestions, I would like to think I could setup a video link to my TV/Video from the computer? I don't know if this is possible but heck it would be an interesting thing to try for me.
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mokum
    mokum over 15 years ago

    i would like to try out some soft core microcontroller projects that have been developed, a high speed data capture application..

     

    cheers

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • espanholito
    espanholito over 15 years ago

    I'm currently starting my phd on buildings comfort and energy efficiency improvement. In order to accomplish the established goals I will have to implement Artificial Intelligence algorithms at different devices (Microcontrollers, FPGA's, PC's) and test it's performance/cost relation.

     

    So if I win this RoadTest I will use the Kit for building an application with the following topics:

     

    -Remote and Local acquisition of Temperature, Humidity, CO2, et. sensors;

    -Control Building appliances;

    -Heavy artificial intelligence algorithms performance tests;

    -Web-services applications;

     

    Of course, the developing of this project will take some time, but I will post every update on the developing status of the developed applications.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • blakme
    blakme over 15 years ago

    I am an experienced FPGA design engineer and have used Xilinx, Altera & Lattice FPGAs in various projects.

     

    Given a chance, I would like to build an accelerator on the Aletra board to monitor hundreds of stocks Real-Time.
    User should be able to set various conditions on the individual or group of stocks to monitor. The accelerator
    would provide real-time trigger/notification to the host when the conditions are met.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 15 years ago in reply to blakme

    Hi "blakme",

     

    As this is a product that is best suitable to be used with a PC as a card I think your project sounds very interesting.

     

    Where would the data itself come in from?

     

    Have you thought about some prediction algorithms?

     

     

    Elias

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • blakme
    blakme over 15 years ago in reply to Former Member

    Hi Elias,

    I am still working on the details and haven't thought about prediction algorithms yet.

     

    Just to start with, the live market data will be pulled from google/yahoo finance website.

     

    -Lakshmi

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>