RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Exar XRP7714 review
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 11 replies
  • Subscribers 2755 subscribers
  • Views 1923 views
  • Users 0 members are here
  • exar
  • xrp7714
  • review
Related

Exar XRP7714 review

obones
obones over 15 years ago

Hello,

 

I was one of the lucky few selected to receive the evaluation board for the Exar XRP7714ILB-FXRP7714ILB-F quad channel step down controller.

I also attended the online seminar, but because I was kept away from the screen during the second half of it, some of my remarks could actually be answered by the video itself.

I will also refer to the messages posted by Eric Cocquerez and Enrico Migchels in the following thread: http://www.element-14.com/community/thread/4260 so please read it before.

 

First the package: I received a nice box with the same parts as mentionned by others: The evaluation board, a 110-240Vac to 12Vdc converter, a USB cable and a USB drive with datasheets and a version of PowerStudio on it.

The initial unpacking lead to the following discoveries:

 

- The converter does not come with the mains cable. Not a big deal, especially considering it is the same format as what is at the back of a computer. It is also only capable to deliver 1.6A, far from the max 5A indicated on the datasheet. One must keep that in mind when intending to test the board without a proper lab supply at hand.


- There are a few 1 pin headers on the board, most of which were slightly bent because of the packing. It was easy enough to get them back straight, but when delivering to rough parts of the world, they may break and I believe they could be quite useful when evaluating the board.

 

Being naturally curious, I tried to understand what the connectors are for on the board. Most have a clear enough description (GPIO, I2C, LDOOUT, GND) or an obvious use such as the red and black sockets. But there are quite a few others, some even unpopulated which I could not make an idea of what they are.

I tried to look for a datasheet of the evaluation board itself on the enclosed USB drive but could not find it, nor could I find it on the Exar website. That's quite a pity as I believe CON2, HDR1, HDR2, J2, J3, J4, J7 and J8 could make for quite a few interesting developments.

 

Because I use a WinXP x64 computer as my main developement PC, I had to register on the Exar website to be able to get the 64bits drivers. As Eric mentioned, the account has to be validated by someone at Exar before one can access the resources. Unfortunately for me, this did not happen so I had to go back to my other PC using WinXP 32 bits to follow with the test. Note that it seems this is a Windows only solution here, no Linux to be seen anywhere in the docs.

 

I'm not as good in power solutions as Enrico appears to be, but just like him I found the XRP7714ILB-FXRP7714ILB-F to be quite good at what it claims to be doing. Not much ripple, good efficiency and most of all, good reporting of what the rails are doing and what the faults are when they occur. This is indeed very handy when developping a remote product that is hardly accessible. One could think of supply chains, packaging systems, onboard power supplies, or, like me, undertable power supply for train modeling. I did not go as far as setting up the whole system as I already have my power solutions (quite archaic, I admit), but this product has quite unlimited applications.

 

Usage of the Power Studio is quite intuitive even if it can seem quite daunting when new to the field of power management. The first question that came to my mind was "what if I end up with an invalid setup? Could I fry the board?"

As I could not find an answer to this question, I did not go very far in changing the default recommended values but that was enough for an initial assesment of the product.

The only thing that I would have liked to test, and which I did not dare trying, was changing the output voltage while a load is applied to the system. The idea behind this would have been to have a current limited programmable voltage source. I was not sure if it would turn off the output while applying the new voltage recommendation or, even worse, turn the mosfet fully on, thus risking frying the load attached to the board.

I don't believe the webminar answered that question, but if anyone finds out about this, that would be nice.

 

In the end, this product seems quite good for intelligent power solutions and I believe it can be very useful for industrial applications where precision and information are a must.


As this is my first review here, I hope it was useful to some of you. Do not hesitate to post your remarks about it.

 

Regards

Olivier

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to enrico.migchels

    Hi Enrico, glad you were able to replace the FETs and get it working - nice piece of engineering. You are correct regarding the banana jacks and we are removing them in our next generation boards.

     

    Olivier, sorry that piece was missing and glad you were able to get around it easily. Upon power up, the 7714 reads in the values of the currently loaded registers and uses that configuration. Because these boards are delivered un-programmed the outputs are off until a configuration is loaded.

     

    Kenny, it should work on a Mac - it works on my Mac and, in fact, I was doing the webinar from a Mac!

     

    Thanks again everyone, Pete

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • cookieglitch
    cookieglitch over 15 years ago in reply to awinning

    Working perfectly on this mac. Might be safari itself rather than just the mac. Firefox works perfectly.

    Even fight between Mac and windows this time image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • KennyMillar
    KennyMillar over 15 years ago in reply to awinning

    Aye it did :-(

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • awinning
    awinning over 15 years ago in reply to KennyMillar
    Did the crappy old piece of Windows junk do what the shiny Mac couldn't then? image
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • KennyMillar
    KennyMillar over 15 years ago in reply to awinning

    Hi Ally,

     

    Yeah it's turned up etc. Must be a mac/safari thing.

    I'll try on an old windows box I have propping up a table somewhere.... :-P

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • awinning
    awinning over 15 years ago in reply to KennyMillar

    Works fine for me Kenny. There's a volme control bottom right, is that turned up?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • KennyMillar
    KennyMillar over 15 years ago in reply to e14 Contributor
    Maybe it's just me, but there does not seem to be any audio on the webinar recording. :-(
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • obones
    obones over 15 years ago in reply to e14 Contributor

    Hello, the mains cable is the one you plug in your wall outlet and that goes to the 220 to 12 converter. I was actually not complaining that it is missing, I was just wanting to warn others that if they don't have an IEC cable handy they would not be able to use the provided 220 to 12 converter. I understand perfectly that you cannot provide this cable as one of its ends changes depending on where you ship the board, US uses a different plug than France for instance.

     

    You are right that my account was approved, but I did not recall having received an email at that time. I looked in my archive, it is not there, but maybe it got classified as spam and deleted automatically after a month.

    I was able to login and access the schematic for the board, nice one there, I love that you use Altium Designer as I'm quite used to it myself. It would have been even nicer if the schematic PDF was on the USB key directly.

     

    About frying, I was not very worried about frying the chips themselves, but rather frying the circuit that is connected after the board.

    Maybe I did not read correctly but I don't remember seeing a paragraph about how the chip controls the FET when it is being programmed. I see a few possibilities :

     

    1. Shutdown the FET

    2. Turn the FET fully on

    3. Keep the current PWM until programming is done and new PWM is taken into account

     

    I believe number 3 is the way it works but I'm not sure.

     

    Thaks for reply

    Regards

    Olivier

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • enrico.migchels
    enrico.migchels over 15 years ago in reply to e14 Contributor

    Hi Pete,

     

    My package also did not come with a mains cord for the power brick. For me this was no problem as I have tons of cables lying around.

     

    About frying FET's. In my enthusiasm I fried one :-) . Two FET's in 1 package is not standard to my warehouse, so I had to improvise a bit and placed 2 separate FET's in S0-8 package. It works, that counts.

     

    One remark: The 4mm banana sockets look a bit odd to me. It makes the whole assembly too high (also extra shipment costs). I would have choosen different connectors, like 1 screw terminal block. This is also easier for production as it is placed in 1 action, the 4mm connectors all have to mounted separately to the board (glad I'm not the one having to do it).

     

    Anyway, the kit was a nice learning experience. I used a similar programmable device in the past to control a plasma TV power supply. Plasma screens have unique settings per set so these settings have to be transferred from the Plasma screen barcode Label to the power supply. In the end the project was banned. Furthermore in China people adjust power supply settings by adjusting potentiometers, it turns out to be cheaper :-)

     

    Best regards, Enrico Migchels

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    I forgot to mention that we have a new webinar online available for viewing:

     

    Quickly creating an Optimized Power System with Digital (Programmable) Power
    https://exar.webex.com/exar/lsr.php?AT=pb&SP=EC&rID=44653822&rKey=4e75e1d5c29e675a

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
>