RoadTests & Reviews
  • Products & Partners
  • More
RoadTests & Reviews
RoadTest Forum How Would You Roadtest the MaaXBoard?
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 17 replies
  • Answers 9 answers
  • Subscribers 2747 subscribers
  • Views 4098 views
  • Users 0 members are here
  • maaxboard
Related

How Would You Roadtest the MaaXBoard?

rscasny
rscasny over 6 years ago

I was sent some info on a new dev board called the MaaXBoard. image

 

The MaaXBoard is based on the NXP i.MX 8M applications processor, and it's good for embedded computing and applications for AI at the edge, industrial automation, multimedia, and IoT applications -- all topics of interest on element14.

 

The MaaXBoard uses NXP’s i.MX 8M family of applications processors, which are based on the ArmRegistered CortexRegistered-A53 and Cortex-M4 cores, providing audio, voice and video processing. The MaaXBoard has a range of capabilities making it ideal to investigate AI, IoT and multimedia applications, offering designers everything they need to support and create a Linux, Android, Windows 10 IoT Core or other OS-based system. The platform’s on-board peripherals include 2GB of DDR4 memory, a Gigabit Ethernet port, dual USB 3.0 host ports, HDMI output, MIPI-DSI, MPI-CSI, WiFi, Bluetooth Low Energy, MicroSD card slot and eMMC storage.

Here's some tech specs:

  • Processor
    • NXP i.MX 8M Processor with Quad Arm Cortex-A53 and single Cortex-M4F
  • Memory
    • 2GB DDR4 SDRAM
    • 8GB eMMC
    • MicroSD Slot
  • Communications and User Interface
    • Gigabit Ethernet
    • Dual USB 3.0
    • MIPI-DSI
    • MIIP-CSI
    • HDMI
    • Supports up to 4k resolution
    • Wi-Fi 802.11 b/g/n/ac
    • Bluetooth 4.2 (Bluetooth Low Energy)
    • Onboard Ceramic Antenna (Default)
    • External Antenna supported
    • Audio Expansion
  • User I/O
    • 40 Pin Low Speed Expansion Interface
    • Raspberry Pi Hat Compatible
    • Digital I/O voltage: 3.3V
  • Other
    • Voltage Regulators
    • USB Type C 5V/3A Power input
    • Operating Temperature: 0~70°C
  • Mechanical
    • 85mm x 56mm x 12mm form factor

 

Question: How would you roadtest this dev board?

  • Sign in to reply
  • Cancel
  • Jan Cumps
    0 Jan Cumps over 6 years ago in reply to phoenixcomm

    phoenixcomm  wrote:

     

    rscasny  For me there are two drawbacks.

     

    one. I still owe you a road test, so Im out!

    two. when I looked at the man page it did not show a RJ45 image and for my Smarthab WIFI is OUT!

    Isn’t that gigabit Ethernet connector RJ-45?

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • dougw
    0 dougw over 6 years ago in reply to gordonmx

    NXP MaaXBoard

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • phoenixcomm
    0 phoenixcomm over 6 years ago

    rscasny For me there are two drawbacks.

     

    one. I still owe you a road test, so Im out!

    two. when I looked at the man page it did not show a RJ45 image and for my Smarthab WIFI is OUT!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • phoenixcomm
    0 phoenixcomm over 6 years ago in reply to gordonmx

    God just use GOOGLE! https://www.variscite.com/product/system-on-module-som/cortex-a53-krait/dart-mx8m-nxp-imx-8m/

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • gordonmx
    0 gordonmx over 6 years ago

    Do you have a link to the documentation?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 6 years ago

    This system has a really nice suite of all the latest hardware features. I especially like the camera interfaces. It would make a very nice time-lapse video camera system for 3D print jobs and electronics project assembly videos. It would run off a power supply so no danger of batteries dying over long print jobs and the high speed Ethernet provides ready access to the video data by video editing computers.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • crisdeodates
    0 crisdeodates over 6 years ago

    rscasny , I would definitely love to roadtest this board. This is, in simple terms, Raspberry Pi with 8 GB onboard storage which is a great advantage. Hoping to know more about this board and understand its capabilities. I could use this to upgrade my autonomous ground vehicle which currently uses a raspberry pi. A worthy candidate for IoT applications. With the given specs, not sure about the AI capability though. Glat to know that it is scalable, thanks to Rpi compatible headers. So a long list of HATs waiting and ready for plug and play applications. Also wondering how the audio expansions ports would be useful. It got a cleaner aesthetic appeal than the other boards of this genre. Waiting to scavenge on more information.. overall, this is a serious Rpi killer board.. 

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
<