RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum RoadTest POLL: Would You Be Interested in Roadtesting an SDR Active Learning Module
  • Blogs
  • RoadTest Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 28 replies
  • Subscribers 2659 subscribers
  • Views 7039 views
  • Users 0 members are here
  • ADALM-PLUTO
  • adi
  • roadtest survey
  • analog devices
  • software defined radio
  • sdr
Related

RoadTest POLL: Would You Be Interested in Roadtesting an SDR Active Learning Module

rscasny
rscasny over 3 years ago

ADALM-PLUTOI am getting to launch a roadtest on an active learning module used to learn the fundamentals of software-defined radio (SDR), radio frequency (RF), and wireless communications.

I wanted to gauge your interest in this roadtest.

Here's a some info on the product:

ADALM-PLUTO is a software-defined radio active learning module. The easy to use ADALM-PLUTO active learning module (PlutoSDR) helps introduce the fundamentals of software-defined radio (SDR), radio frequency (RF) and wireless communications.

Here are some features:

  • Portable self-contained RF learning module
  • Cost-effective experimentation platform
  • Based on Analog Devices AD9363--Highly Integrated RF Agile Transceiver and Xilinx® Zynq Z-7010 FPGA
  • RF coverage from 325MHz to 3.8GHz, up to 20MHz of instantaneous bandwidth
  • Flexible rate, 12bit ADC and DAC, GNU Radio sink and source blocks
  • MATLAB®, Simulink® support, libiio, a C, C++, C# and Python API
  • One transmitter and one receiver, half or full duplex
  • USB 2.0 powered Interface with Micro-USB 2.0 connector
  • High quality plastic enclosure

Here are some docs:

datasheet 
product overview
user guides 

For more information

Here's the poll questions:

  • Sign in to reply
  • Cancel

Top Replies

  • kmikemoo
    kmikemoo over 3 years ago +3
    As to the time, my first thought was "How much can I get?" I went with 20-40 because I don't count the time between selection and when the product arrives. You know... the time where you read everything…
  • shabaz
    shabaz over 3 years ago in reply to robogary +2
    Hi Gary, All the above is free/open source stuff, except the MATLAB item (and its associated Simulink). MATLAB has a free evaluation for 1 month. It is also available for for home use at about $120…
  • JWx
    JWx over 3 years ago +2
    This is much better than RLT-SDR I have - not only broader bandwidth, but with TX option as well. In my opinion software support (or better - good bundled software) is critical for beginners - when a beginner…
  • misaz
    misaz over 3 years ago

    Yes I am interested as I mentioned PLUTO in preivous poll. I chosen over 80 hours based on my experience with previous roadtest which always took me huge amount of free time and also I would have to learn a lot new things related to analog and RF. In this area I am not very skilled yet, so PLUTO looks like good entry point.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • rsc
    rsc over 3 years ago

    This kit would be fun to play with.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago

    Currently overloaded hehe, but this has got to be one of the best SDRs to work with because it comes with software!

    In contrast, I have Lime SDR which is technically on paper great, but in practice suffers loads from lack of software examples and documentation 

    The guy who did their technical articles tended to 'information-hide' I feel, and never shared enough detail. Lime SDR an extremely frustrating product, so I regret choosing it in some ways.

    An SDR is a fantastic tool for all sorts of RF work, often achieving things not possible with other test equipment.

    Even a low-cost RTL-SDR is interesting to experiment with, but a more complete SDR like PLUTO offers signal generation too.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • kmikemoo
    kmikemoo over 3 years ago

    As to the time, my first thought was "How much can I get?"  I went with 20-40 because I don't count the time between selection and when the product arrives.  You know... the time where you read everything that you can find about the device while you wait - patiently - for what feels like forever. LaughingThumbsup I'm like a small child waiting for Christmas or their birthday.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • kmschmi
    kmschmi over 3 years ago

    This looks like an interesting piece of hardware, with different applications that can be investigated. With that being said, to really do justice to the roadtest over 80 hours would be necessary to absorb new knowledge and apply it.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 3 years ago

    SDR is on my list to explore at some point. This looks like a good place to start. For me the learning curve would be steep so I expect it would require over 80 hours. The knowledge gained is a primary objective and it is bound to take time to learn.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • robogary
    robogary over 3 years ago

    Does evaluation include licenses for MATLAB®, Simulink® support, libiio, a C, C++, C# and Python API ? 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to robogary

    Hi Gary,

    All the above is free/open source stuff, except the MATLAB item (and its associated Simulink).

    MATLAB has a free evaluation for 1 month. It is also available for for home use at about $120, perpetual license, which is a lot lower than its usual cost! however if you're planning to go down the purchase route (it's not essential to use the SDR, but it is highly desirable for all sorts of work), then I'd strongly recommend discussing it in say a forum post, because there are some important things to keep in mind (to save costs). Also, sometimes MATLAB type work can be done for free in Python, but it's not the same, MATLAB has been heavily used for decades and so there are lots of examples that would work directly with MATLAB, but would need porting if Python was used. 

    Finally, there's another option called GNU Octave, that is free too, but it would probably need some work (in programming language of choice) to "connect" to the data to/from the ADALM PLUTO. For instance, Python could do it.

    The ADALM PLUTO documentation gives examples using different methods, so you could try the MATLAB examples if desired prior to purchasing MATLAB (in case you end up preferring using say GNU RADIO (which is building-block style) or Python or C etc.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • mp2100
    mp2100 over 3 years ago

    I would be very interested. It's a topic I'd like to learn. And it would take me a while to learn. So many options. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • saadtiwana_int
    saadtiwana_int over 3 years ago

    I took an SDR course on Udemy some time ago. Since I didn't have the hardware, I had to mostly do things on GNU radio without the hardware. This would be a good opportunity to do some actual SDR-ing! Slight smile

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
>