RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum ROADTEST POLL: Would You Be Interesting in Roadtesting a Multi-Hub Antenna?
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 14 replies
  • Subscribers 2751 subscribers
  • Views 4310 views
  • Users 0 members are here
  • multi-hub antenna
  • molex
  • 217853-1000
  • 216589-1000
  • roadtest survey
  • antenna
Related

ROADTEST POLL: Would You Be Interesting in Roadtesting a Multi-Hub Antenna?

rscasny
rscasny over 3 years ago

I have been in conversation with the roadtest sponsor about roadtesting a multi-hub antenna.

We both would like to to more activities around antennas, but we don't know much interest there would be in this particular product. Thus, I'm running this poll to gauge your interest in roadtesting it.

Here's some information about the product:

imageMulti-hub 5 in 1 external antenna

A multi-hub 5 in 1 external antenna including 2x 5G/LTE, 2 x WiFi and 1x GNSS. It provides 5G MIMO and Wi-Fi MIMO antenna system within compact antenna box and use in automotive telematics, transportation and remote monitoring applications.

Features

  • Working frequency 698-960MHz/1500-1700MHz /1710-2690MHz/3300-5000MHz for 5G/LTE
    MIMO, Frequency 2400-2500MHz/5000-6000MHz for WIFI MIMO, 1561-1602MHz for GNSS
  • Antenna Size:155x65x20mm with 1000mm Cable Length
  • Connector Type: SMA (M) ST
  • IP67

Here are some docs:

Datasheet

Product Specs

Application Specs

For other information

 imageMulti-hub antenna 7-in-1

A Multi-hub 7-in-1 Antenna including 2 x LTE/5G full band, 2 x LTE/5G high band, 2 x WI-FI, and 1x GNSS. It provides LTE/5G 4 x 4 MIMO, WI-FI 2 x 2 MIMO and GNSS antenna system within compact antenna box and use in automotive telematics, transportation and remote monitoring applications.

Features

  • Working frequency 600-960MHz/1400-1550MHz/1710-2690MHz/3300-5000MHz for 5G MIMO, Frequency 2400-2500MHz/5150-5850MHz/5925-7125MHz for WIFI MIMO, 1561-1602MHz for GNSS
  • Antenna Size:160x115x22.5mm with 1000mm Cable Length
  • Connector Type: SMA (M)
  • IPX7

Here are some docs:

Datasheet

Product Specs

Application Specs

For other information

  • Sign in to reply
  • Cancel
  • kmikemoo
    kmikemoo over 3 years ago

    Alas... no.  It sounds really cool, but I don't have anything to really plug into most of it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Gough Lui
    Gough Lui over 3 years ago

    I think this one will be a tough one to draw a crowd. It's difficult to test antennas for performance objectively in ordinary environments, although perhaps use in an application is easier to demonstrate. The design seems to be most suited for vehicles or constrained space applications where the vehicle's own systems need an antenna to connect to various networks and for GNSS.

    While it may be tested or applied outside of a vehicle, I think it would be fairly tricky to get a single system that would have all the necessary radios and the adapters necessary to connect them all just to make sure they work together. Instead, testing each input separately may be easier, but then we don't see the "self-interference" potential. Many cellular phones, for example, don't even have external antenna connectors nowadays and even when they do, it's usually cellular only - nothing for Wi-Fi or GNSS. Perhaps a laptop with a cellular card may be a better candidate - but they will probably use tiny MHF or smaller connectors, not SMA. I do have a gateway device that has SMA GNSS, LTE-M/NB-IoT, LoRaWAN but not Wi-Fi.

    It's a tricky one for sure ... ideally one would have a VNA to sweep each antenna for some real data, something I don't have. A proper anechoic chamber and calibrated automated measurement for radiation pattern would be a proper test but you probably won't find more than a handful of labs in the world equipped to do it. The manufacturer (Molex) likely has good data here already, so replicating this is probably not a major point.

    - Gough

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • misaz
    misaz over 3 years ago

    I voted no because I have not equipment and skills to properly test this kind of devices.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • charlieo21
    charlieo21 over 3 years ago

    This is an interesting hub antenna for a roadtest, I vote no because I don't have the skills or equipment to test this antenna o any other antenna. I hope there's someone who has the expertise for this kind of roadtest, because this technology is really amazing, and I would learn a lot watching those roadtests.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
<