RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Seeking Your Interest in Roadtesting a Digital Isolator Board
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 36 replies
  • Subscribers 2747 subscribers
  • Views 5467 views
  • Users 0 members are here
  • digital isolators
  • adi
  • roadtest survey
Related

Seeking Your Interest in Roadtesting a Digital Isolator Board

rscasny
rscasny over 2 years ago

Hi All.

imageI had a call with one of suppliers who is interested in roadtesting one of its digital isolator boards. We have not done much with digital isolators in the roadtest program. But given the need for circuit isolation and the safety they provide, I wanted the community to roadtest this product. In addition, another reason was the learning experience the roadtesters can provide community members on this product.

Here is some basic information on this board:

The evaluation kits are designed to evaluate the MAX22563−MAX22566, a family of reinforced, six-channel, galvanic digital isolators in a 20-pin SSOP package.

Two types of evaluation boards are available:

  • The MAX22565CAEVKIT# is fully assembled and tested, and comes populated with the MAX22565CAAP+ (Not used in this roadtest)
  • The MAX2256XAEVKIT# is a generic board that has U1 unpopulated, allowing to select a device from the MAX22563−MAX22566 family. This is the kit that will be used for this roadtest. The MAX2256XAEVKIT# comes with U1 unpopulated and supports the following digital isolators: MAX22563BAAP+, MAX22563CAAP+, MAX22564BAAP+, MAX22564CAAP+, MAX22565BAAP+, MAX22565CAAP+, MAX22566BAAP+, and MAX22566CAAP+.

imageEquipment needed for roadtesting:

You need some test equipment to roadtest the MAX2256XA EV kit:
• MAX22563−MAX22566 device if U1 is unpopulated on EV kit. (The roadtester and I will get together to order the desired device needed.)
• Two DC power supplies with output range of 1.71V to 5.5V
• Signal/function generator
• Oscilloscope
Note: The EV kit should be powered from two independent isolated power supplies with nominal output voltage in the range from 1.71V to 5.5V. To evaluate the electrical parameters of the device without any isolation between the two sides, a single power supply can also be used.

Element14 would not provide the test equipment.

Roadtesters would need to have the bench equipment for this roadtest. If you are an electronic design engineer, you likely have access to most of these equipment. This seems like a lot to ask, and it is. But I think this is a valuable roadtest to offer the community. The reviews the roadtesters write would not only be good learning experiences, but would also provide customers more than a datasheet to select a digital isolator when the need arises. 

Here's some documentation on the board:

Datasheet
Manufacturer's page

For Additional Information

Here's a couple of polls for which to vote:



  • Sign in to reply
  • Cancel
  • rscasny
    rscasny over 2 years ago in reply to ciorga

    This is how the sponsor answered your questions:

    Agree with the comments in terms of signal integrity, power integrity, noise coupling and high voltage testing.

    These devices use ADI’s edge based differential architecture and capacitive isolation technology which enables lower power consumption per channel and the highest data rates supporting up to 200Mbps.

    The main features that should be called out are as follows:

    • High Channel Density ( 6 isolated channels available in multiple forward/reverse configurations.)
    • Edge based differential architecture ( Capacitive Isolation Technology) enabling:
      • Low Propagation Delay  (7ns )
      • Low Jitter  (11.1ps)
      • Low power consumption per channel (34mW per Channel at 1Mbps with VDD = 3.3V)
    • Highest Data Rate (200Mbps)
    • VISO = 3.75kVrms, VIOWM = 784 Vrms
    • CMTI = 50kV/us
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Andrew J
    Andrew J over 2 years ago in reply to jc2048

    I hadn’t spotted those.  Probably because they’re right in front of me and being male!  Makes it more flexible and that’s what I would have used with a board to knock the voltage level down.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jc2048
    jc2048 over 2 years ago in reply to colporteur

    J1 and J2 are SIL headers. You could wire up a simple board to plug onto them or, at a pinch, just push solid wires into them.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • netaddict
    netaddict over 2 years ago

    I'd love to try this one out. I've used digital isolators from another vendor successfully in the past, but when looking at this datasheet, the max propagation delay could be the double (even triple) from the minimum propagation delay. I would like to see that measured in practice; in particular at highest data rate and lowest Vdd.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • tarna
    tarna over 2 years ago in reply to rscasny

    My oscilloscope is so janky I wouldn’t really be able to do this well, the old tft is basically impossible to see. However if I were; I would not be afraid of soldering a 20 pin ssop, it wouldn’t necessarily be factory quality work but I have no doubt I could do it. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Andrew J
    Andrew J over 2 years ago in reply to michaelkellett

    If this roadtest had come up just over a year ago I would have applied because I could use the board for the same scenario that I created one for.  It would have required modding to drop input signals to 5V (from circa 220V)  and I would have had to buy (or be provided) some SMA to BNC and SMA to croc clips (eventually modding the board to remove them) and eventually modding to add the DC-DC converter.  I don't know whether that would be useful for the supplier because it's only slow, pulse-based, one-way signals, but it would have been a real-life scenario.  I'd have needed the parts to create the mods of course but that would be a good exercise in utilising the isolator rather than purely testing with a pre-built dev board and nice clean signals from a function generator.

    If I didn't get selected, I might even have bought one of them to do it - I think it would have worked out cheaper but it would be a close call on that basis.  

    I agree a real-life scenario would provide more useful results if a range of sufficiently different scenarios could be chosen from.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 2 years ago

    Why SMA connectors on input? I don't have them readily available on the test bench for doing digital testing.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 2 years ago

    I wouldn't apply for this Road Test. I use digital isolators in my designs but not like this. The board is set up to replicate the kind of tests done in a data sheet. If i didn't trust the supplier to have done the tests in their data sheet I wouldn't be buying their parts at all - so I have no interest in replicating those tests which are usually designed to test key parameters with as little interaction with other things as possible.

    But when you actually use a part you don't care about that - you care about how it works in real life. And if you can solder the chips to the test board you could solder them into your own board.

    I think a much more useful demo board for these parts would have 0.1" pin headers for IO and an isolated DC-DC converter to power the remote side - it could be about 1" square and easily patched into an existing design or hooked up with wires.

    MK

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • SensoredHacker0
    SensoredHacker0 over 2 years ago

    I know a guy who would do great road testing The MAX22565CAEVKIT
    he is on here too, not sure about his username though.
    johnmiller139  might be the guy, might not.
    this product isnt in my wheelhouse, but I know some guys.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • scottiebabe
    scottiebabe over 2 years ago in reply to jc2048

    That was my guess, I presume the through channel are length matched to all the DUT test channels.

    image

    Pretty fancy board for what might end up being a 20 MHz SPI bus...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
>