RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Seeking Your Interest in Roadtesting a Digital Isolator Board
  • Blogs
  • RoadTest Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 36 replies
  • Subscribers 2649 subscribers
  • Views 4650 views
  • Users 0 members are here
  • digital isolators
  • adi
  • roadtest survey
Related

Seeking Your Interest in Roadtesting a Digital Isolator Board

rscasny
rscasny over 2 years ago

Hi All.

imageI had a call with one of suppliers who is interested in roadtesting one of its digital isolator boards. We have not done much with digital isolators in the roadtest program. But given the need for circuit isolation and the safety they provide, I wanted the community to roadtest this product. In addition, another reason was the learning experience the roadtesters can provide community members on this product.

Here is some basic information on this board:

The evaluation kits are designed to evaluate the MAX22563−MAX22566, a family of reinforced, six-channel, galvanic digital isolators in a 20-pin SSOP package.

Two types of evaluation boards are available:

  • The MAX22565CAEVKIT# is fully assembled and tested, and comes populated with the MAX22565CAAP+ (Not used in this roadtest)
  • The MAX2256XAEVKIT# is a generic board that has U1 unpopulated, allowing to select a device from the MAX22563−MAX22566 family. This is the kit that will be used for this roadtest. The MAX2256XAEVKIT# comes with U1 unpopulated and supports the following digital isolators: MAX22563BAAP+, MAX22563CAAP+, MAX22564BAAP+, MAX22564CAAP+, MAX22565BAAP+, MAX22565CAAP+, MAX22566BAAP+, and MAX22566CAAP+.

imageEquipment needed for roadtesting:

You need some test equipment to roadtest the MAX2256XA EV kit:
• MAX22563−MAX22566 device if U1 is unpopulated on EV kit. (The roadtester and I will get together to order the desired device needed.)
• Two DC power supplies with output range of 1.71V to 5.5V
• Signal/function generator
• Oscilloscope
Note: The EV kit should be powered from two independent isolated power supplies with nominal output voltage in the range from 1.71V to 5.5V. To evaluate the electrical parameters of the device without any isolation between the two sides, a single power supply can also be used.

Element14 would not provide the test equipment.

Roadtesters would need to have the bench equipment for this roadtest. If you are an electronic design engineer, you likely have access to most of these equipment. This seems like a lot to ask, and it is. But I think this is a valuable roadtest to offer the community. The reviews the roadtesters write would not only be good learning experiences, but would also provide customers more than a datasheet to select a digital isolator when the need arises. 

Here's some documentation on the board:

Datasheet
Manufacturer's page

For Additional Information

Here's a couple of polls for which to vote:



  • Sign in to reply
  • Cancel

Top Replies

  • ciorga
    ciorga over 2 years ago +4
    It looks to me that this product needs roadtesters specialized in signal integrity, power integrity, noise coupling, and high voltage isolation testing. This work is very specialized and requires quite…
  • michaelkellett
    michaelkellett over 2 years ago +3
    I wouldn't apply for this Road Test. I use digital isolators in my designs but not like this. The board is set up to replicate the kind of tests done in a data sheet. If i didn't trust the supplier to…
  • jc2048
    jc2048 over 2 years ago +2
    "Two DC power supplies..." Wouldn't a tester need a third to establish the voltage difference betwen the two sides? If you just let bench supplies float, small amounts of leakage will slowly pull the…
  • dougw
    dougw over 2 years ago in reply to jc2048

    You might even want a signal generator to make the voltage between the 2 supplies vary in a known way... 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • baldengineer
    baldengineer over 2 years ago in reply to Jan Cumps

    Yeah... I didn't think about battery-powered options. However, the bandwidth limit (on gen or scope) makes me question if it is suitable for this family of chips.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rscasny
    rscasny over 2 years ago in reply to ciorga

    Well, the goal isn't just an unboxing. You ask very good questions. I'll ask the sponsor on Monday. The parts are suggested to me through our sponsor's contact and I presume were recommended from the applicable business unit. Since the type of testing is influenced by their goal, it's something I should get clarified for the roadtesters. Thanks for posting this comment.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rscasny
    rscasny over 2 years ago in reply to dougw

    Yes, all those are true, especially since their choices are passed to me through the sponsor's marketing department. I usually make the decision to roadtest it or not. I would like this roadtested; I just think this component needs some "air time" on the community. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • JWx
    JWx over 2 years ago in reply to rscasny

    In my opinion the main problem would be higher bandwidth parts - they offer parts rated at 25Mb/s (eg. MAX22563BAAP+) and 200Mb/s (MAX22563CAAP+) - it would be good to know if they have any preference which (sub)family is going to be tested.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rscasny
    rscasny over 2 years ago in reply to JWx

    No. It's your choice and that's another reason they chose this version of the board. They anticipate different roadtesters will choose different parts based upon what they want to do and how they plan on testing it.

    Randall

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • scottiebabe
    scottiebabe over 2 years ago in reply to jc2048

    That was my guess, I presume the through channel are length matched to all the DUT test channels.

    image

    Pretty fancy board for what might end up being a 20 MHz SPI bus...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • SensoredHacker0
    SensoredHacker0 over 2 years ago

    I know a guy who would do great road testing The MAX22565CAEVKIT
    he is on here too, not sure about his username though.
    johnmiller139  might be the guy, might not.
    this product isnt in my wheelhouse, but I know some guys.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 2 years ago

    I wouldn't apply for this Road Test. I use digital isolators in my designs but not like this. The board is set up to replicate the kind of tests done in a data sheet. If i didn't trust the supplier to have done the tests in their data sheet I wouldn't be buying their parts at all - so I have no interest in replicating those tests which are usually designed to test key parameters with as little interaction with other things as possible.

    But when you actually use a part you don't care about that - you care about how it works in real life. And if you can solder the chips to the test board you could solder them into your own board.

    I think a much more useful demo board for these parts would have 0.1" pin headers for IO and an isolated DC-DC converter to power the remote side - it could be about 1" square and easily patched into an existing design or hooked up with wires.

    MK

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 2 years ago

    Why SMA connectors on input? I don't have them readily available on the test bench for doing digital testing.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>