RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Seeking Your Feedback on RoadTesting an e-Fuse IC Eval Kit
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 14 replies
  • Subscribers 2748 subscribers
  • Views 3132 views
  • Users 0 members are here
  • roadtest survey
Related

Seeking Your Feedback on RoadTesting an e-Fuse IC Eval Kit

rscasny
rscasny over 1 year ago

imageWhen I was first approached about roadtesting an e-Fuse Eval kit, I had the following thought bubble up from deep in my mind: Why would we roadtest a fuse?

Then, I went to dear Google and asked it about the growth of e-Fuses. I'm not going to quote any particular study, but the use of e-Fuses is growing considerably.

So, I agreed to the roadtest because e-Fuses have a lot of tech in them for their size and I feel the community should explore them. Perhaps even compare them to ye old fashioned trip-wire fuse. It's perhaps something a new member, first time roadtester, or the curious-at-heart would be interested in spending some "quality" time with.

In any event, I wanted to get your thoughts on roadtesting e-Fuses.

Here's some facts about the product:

EVB-TCKE805NA is a TCKE805NAe-Fuse IC evaluation board (EVB). It is an evaluation board for supporting TCKE8xx series-design. The passive components required to operate IC are mounted, enabling easy operation check and characterization. The evaluation board features:
• Input voltage range from 4.4V to 18V
• Output limit current range from 0.5A to 5.0A adjustable
• Adjustable slew rate
• Active high enable control
• Auto retry function
• Auto discharge
• Available in 3x3mm WSON10B package

Here's the schematic

image

Here's the documentation:

Instruction Manual

Here's my poll:

  • Sign in to reply
  • Cancel
  • dougw
    dougw over 1 year ago

    A great way to get familiar with this cool technology.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • aswinvenu
    aswinvenu over 1 year ago
    rscasny said:
    hy would we roadtest a fuse?

    Very interesting! But just wondering if these devices can be used as a replacement for regular fuses in all use-cases. I was working on an Intrinsically safe device for an Atex Zone 0 device. Can these fuses used in such designs?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • battlecoder
    battlecoder over 1 year ago

    What a fascinating device. I have to admit I wasn't quite thrilled with a "fuse" but your short description of how sophisticated these devices actually are, definitely caught my attention. The fact that even the slew rate can be configured is kinda mind blowing.


    Now, I was already thinking of applying to a different Road test, and I don't think applying to two different RTs would be a good idea (although admittedly testing this one shouldn't take a lot of time, and sounds like lots of fun)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 1 year ago

    The board is supplied without reverse protection FET. The datasheet suggests Toshiba SSM6K513NU . Less than a $. Maybe the vendor could provide one of those? 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
<