RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Do you have the ability to RoadTest Power Integrations TinySwitch-5 RDK-1016?
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 18 replies
  • Subscribers 2748 subscribers
  • Views 1546 views
  • Users 0 members are here
  • e14-pi
  • tinyswitch-5
  • power integrations
Related

Do you have the ability to RoadTest Power Integrations TinySwitch-5 RDK-1016?

cstanton
cstanton 9 months ago

We're looking for a few members to RoadTest a product from power integrations.

Now, this is more of a 'reference design' than a 'demonstration kit', but we often receive requests from suppliers that are like this.

The product is:

image

26.5 W dual output isolated flyback power supply for appliances using TinySwitch-5 (TNY5073K)

Information and datasheets are available at: https://www.power.com/design-support/design-kits/rdk-1016-reference-design-kit 

With details about TinySwitch-5 at: https://www.power.com/products/tinyswitch/tinyswitch-5

We would likely be looking for a RoadTester that can put it through its paces and characteristics rather than plugging it in and saying "it works". This means we may deviate from our usual RoadTest of 'sign up and you may be selected' and instead go down the path of 'ok, two or three of you are selected and we'll see if we can also provide you with some parts that you need'. (We tend to call these RoadTest Plus or Special RoadTests).

  • Sign in to reply
  • Cancel
  • rsc
    rsc 9 months ago

    I was interested until I read the specs : 12V @ 2A, 5V @ only 0.5A 

    Not enough 5V power for the project I was thinking of. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • hlipka
    hlipka 9 months ago in reply to manojroy123

    From the data sheet / RDK description:

    Fuse F1 isolates the circuit and provides protection from component failure. Bulk Capacitors C19 and C2 together with differential mode choke L4 forms an EMI filter that attenuates both common mode and differential mode conducted EMI. BR2 converts the AC line voltage into the DC voltage seen across bulk capacitors C19 and C2.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • foxbat
    foxbat 9 months ago

    I'd definitely be in the 'turn it on and use it' camp, but the comments regarding environmental testing made me wonder about the viability of creating a shock / vibration test rig.  Motor and a selection of ALM cams to change the vibration or shock profiles, with a G Sensor and microcontroller to measure / characterise the vibration.  The ultimate aim would be to try and achieve something that could support some of the test profiles in a recognised standard (e.g.  MIL-STD-810)... but I might bite off more than I can chew with that last bit!!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps 9 months ago in reply to robogary

    Raised hand

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • robogary
    robogary 9 months ago in reply to Gough Lui

    Rofl - or inside listening to Pink Floyd on audiophile speakers.  :-) 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Gough Lui
    Gough Lui 9 months ago in reply to michaelkellett

    *stares enviously from half-way around the world*

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett 9 months ago in reply to Gough Lui
    Gough Lui said:
    (anyone with one of those, raise your hand?

    Raised hand

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Gough Lui
    Gough Lui 9 months ago in reply to manojroy123
    manojroy123 said:
    I usually use board with proper common mode choke filter at the primary side.

    It's their "feature" to reduce component count. I'd say that suggests they're controlling the switching waveform with respect to frequency to spread the noise out so as to (potentially) remain below limits.

    manojroy123 said:
    never seen common mode choke designed as inductor.

    Seems to be a pi-filter to limit the amount of noise injected back to the mains and smooth out the DC. That being said, as far as I can tell from their test reports, the board isn't officially agency approved, but I'd have to say that PI very likely know their stuff and the EMC pre-qualification they've done in their report shows it has a decent chance of passing conducted emissions depending which limit line is used ...

    - Gough

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Gough Lui
    Gough Lui 9 months ago in reply to robogary
    robogary said:
    How about shock-vibration (in transport or operation like in a dishwasher or refrigerator) on a shaker table, or ambient temperature/humidity corner points

    That's an interesting point - alluding to the numerous other possible tests I haven't thought of. Indeed, it may be of interest, but alas, temperature/humidity control often means an environmental test chamber (anyone with one of those, raise your hand? *leaves hand firmly lowered*). As for the shake table ... I don't have one either, but perhaps those tests are much more valuable when it's been integrated and constructed as per final-production-design rather than on a reference design that hasn't yet been qualified for EMC.

    robogary said:
    ambient noise measurements in an anechoic chamber for audible noise  :-)

    I suspect that would very much depend on the quality of the flyback transformer's winding and construction, and any sub-fundamental components of the switching waveform that lie in the audible range. But alas, if I had one of those chambers, perhaps you'd find me sleeping soundly inside ...

    - Gough

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gam3t3ch
    gam3t3ch 9 months ago

    I mean I would be game to play with it and put it through its paces. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
>