RoadTests & Reviews
  • Products & Partners
  • More
RoadTests & Reviews
RoadTest Forum POST 3 What is in the box... Red Pitaya STEMlab 125-14 PRO Gen 2 Starter Kit
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 14 replies
  • Subscribers 2746 subscribers
  • Views 492 views
  • Users 0 members are here
  • RoadTest
  • test equipment
  • red pitaya
Related

POST 3 What is in the box... Red Pitaya STEMlab 125-14 PRO Gen 2 Starter Kit

colporteur
colporteur 21 days ago

I've discovered that the documentation is significantly behind the product supplied for this RoadTest. I would have liked to provide the resource I discovered that my fellow RoadTester could use and not have to visit the dead end rabbit warrens that I have traveled.

image

It appears this is the unit used for the documentation. Notice next to the RJ45 connector the narrow silver case of a USB-A socket.

image

We are provided this unit. Note the USB is not present.

image

In addition, the kit comes with a QSPI eMCC module. It mates with the E3 connector on the board. This module promises to eliminate the need for the SD card, if it only worked!

I've discovered the firmware for this module has changed (as promised in documentation). I have been unsuccessful in trying to load the OS to this module in the current firmware version because of the watchdog timer. It reboots the OS when it fails to get a proper response. It has to be disabled to load the OS (through a USB port that doesn't exist) into the module. A github dev version I found appears to fix the issue.

The documentation is for the board I don't have so even if I solve the watchdog timer issue my board doesn't have the USB-A port to move the OS.

After backing out of the last warren run that ended in a dead end, I've sent an email to Red Pitaya support for assistance.

My intent was to get a stable Pitaya platform to pursue SDR objectives. A self contained bootable Pitaya I felt was a reasonable starting point. That would give me a chance to explore the setup and then investigate SDR. That setup part is proving to be a bit of a challenge.

Getting the OS working was a struggle. I'm going to park the module boot option until I get a response from support.

  • Sign in to reply
  • Cancel
  • beacon_dave
    beacon_dave 21 days ago in reply to obones
    obones said:
    as its first requirement is to have access to a ST-Link/V2 programmer which is not something that I have here anyway.

    Looks like lots of stuff not yet supported but you appear to have a second option for programming the module:

    Method 2: USB to micro USB cable (DFU)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • obones
    obones 21 days ago in reply to beacon_dave

    Yes, the documentation talks about using the CON port which is one of the three USB-C connectors on the underside.

    It also warns about that watchdog and has the following suggestion:

    Two options are available to disable the watchdog:

    Option 1 — Edit the E3 module firmware (currently supported)

    Modify the E3 module firmware source code to disable the watchdog timer check, then re-flash the STM32 microcontroller on the QSPI eMMC module before proceeding with the eMMC flashing steps.

    Refer to the E3 QSPI eMMC module software guide for instructions on building and programming the E3 firmware.

    Option 2 — Send the watchdog disable command via I2C (available in a future OS version)

    A future Red Pitaya OS version will include support for sending a watchdog disable command to the E3 module via I2C before rebooting into U-boot. When this feature is available, the firmware modification in Option 1 will no longer be required.

    Refer to the E3 I2C controller utility for information about I2C commands supported by the E3 module.

    Option 2 is apparently out of the equation, so one must reflash the STM32 controller on the eMMC module, as described here: https://redpitaya.readthedocs.io/en/latest/developerGuide/software/system_development/e3_software/QSPI_eMMC_sw/QSPI_eMMC_software.html#e3-qspi-emmc-module-sw

    But honestly, this feels like quite a daunting task as its first requirement is to have access to a ST-Link/V2 programmer which is not something that I have here anyway.

    I believe I'll do one very long post for this review, but this one thing that is starting to come through in my early testing: It's not a simple device and the learning curve is quite steep.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave 21 days ago
    colporteur said:
    through a USB port that doesn't exist

    Aren't you supposed to use the USB C console port on the back on the Gen 2 versions ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • embeddedguy
    embeddedguy 21 days ago

    Nice looking board.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
<