RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum RoadTests: Project vs Unboxing vs Experiment vs Other
  • Blogs
  • RoadTest Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 24 replies
  • Subscribers 2564 subscribers
  • Views 1895 views
  • Users 0 members are here
  • scasny
Related

RoadTests: Project vs Unboxing vs Experiment vs Other

rscasny
rscasny over 8 years ago

Over the past few months, I have implemented some changes to the RoadTest program. Some of these changes had to do with things that needed to change in order to have the program work for all stakeholders. Of course, some of them have to do with things that would help me manage the program better (e.g., asking applicants to use their profile email address on applications or my asking supplemental questions.)

 

But one comment caught my attention last week. To paraphrase it, the commenter thought that RoadTests were more or less morphing into prototyping "big" projects. This has led some individuals not to apply because of a lack of time.

 

While creating a big project would be nice, it's definitely not required. After all, we give you 60 days to complete testing and write a review. Not a whole lot of time to create something totally new.

 

A RoadTest can be a combination of performing an unboxing (start up/installation), conducting some experiments or tests (e.g., verify a power supply's load regulation is in specs), building a prototype, or doing something else.

 

When I review the applications -- all of which get sent to the supplier -- I do provide some recommendations. Sometimes they go with my recommendations, sometimes they do not.

 

But I've observed the following things regarding applications:

 

  • We are looking for a concise plan of testing.
  • Is the project do-able? Some projects aren't in 60 days.
  • Does the RoadTester appear to be able to pull off the testing and write the review.
  • The plan isn't being re-hashed over multiple RoadTests.
  • The application sounds like the applicant took the time to study the product; we have had some RoadTesters that submitted applications that were irrelevant to the product being tested.
  • Long applications may get looked at, but the winners are a combination of long or short applications. The application should be only as long as need be to explain your testing plan. But 1 sentence applications are rarely taken seriously.

 

I encourage everyone who is interested to keep on applying for RoadTests. Since we are given a limited number of units, we can't get everyone to test all the time. But a good plan will rise to the top.

 

Randall Scasny

RoadTest Program Manager

  • Sign in to reply
  • Cancel

Top Replies

  • Workshopshed
    Workshopshed over 8 years ago +6
    I wonder how long people spend on a road test? Perhaps a metric to capture with the roadtest reports?
  • mcb1
    mcb1 over 8 years ago in reply to hlipka +6
    Merit != Ambition. A project proposal does not have merit, only the person has it Sorry but I'm not sure I agree with that. We've seen some Roadtests where the applicant used the device for something outside…
  • balearicdynamics
    balearicdynamics over 8 years ago in reply to Workshopshed +5
    It's a good idea Andy. If I have understood it is the case to make an official poll. Some suggestions: You spend more on: time money personal components and material all And then what kind of extra tools…
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to Fred27

    well.... unboxing as the core of a road test I don't like eather. but unboxing as part of a road test I love.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • DAB
    DAB over 8 years ago in reply to rscasny

    I do not find the unboxing to be particularly useful.  Caveat, one vendor sent me a board and it was poorly constructed so I contacted them and provided them pictures of the issues I had with the board and they used that information to look into their quality control.

     

    So unboxing an item where issues are involved can be of great value to the manufacturer and the community.

     

    I personally am more interested in seeing people look into the product, verify that it works as advertised and validate the device as something "worth" purchasing for specific applications.

     

    As an example, I tested a MEMs microphone for Element14 and compared it to a standard Electret microphone.  The testing showed the improvement in frequency response and the effective direction of sensitivity of the MEMs device.

     

    I provided some basic summary and identified my preference based on the data.

     

    So road testing can provide a wide range of information depending upon the test plan and data collected.

     

    As for time and effort data collection, I find it a double edged idea.  Yes it could show how much effort some testing can take, which might encourage some to participate, but it might also scare some away.

     

    Again, I enter a road test with a fair understanding, based on my many years of experience, as to how much time and effort I plan to put into the testing.  Making a job of it would probably convince me not to participate except for exceptional gear.

     

    I think road testing should be a fun and flexible activity.  I think it would lose value to vendors and members if it gets too formalized.  I agree it is a fine line to walk.

     

    DAB

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 8 years ago in reply to DAB

    So unboxing an item where issues are involved can be of great value to the manufacturer and the community.

    I'm with you on the issues bit (Highlighted), otherwise it is a video or pictures of how well the freight department did versus the journey through the freight route.

     

     

    I personally am more interested in seeing people look into the product, verify that it works as advertised and validate the device as something "worth" purchasing for specific applications.

    I agree that a RT is a test of the product, not your specific project.

    There is room to use it in a project and show why it is better than xyz, which demonstrates why it is worth purchasing.

     

    It's very hard to have set rules around RT because element14 and the vendors supply Instruments thru to connectors and SBC.

     

    I'm sure the vendors aren't supplying the goods simply to get an 'Excellent' tick.

    Hopefully they are interested in hearing if the user had difficulties so they can improve their product, support or evene the purpose it can be used for.

     

    Mark

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 8 years ago in reply to Jan Cumps

    I agree, I like seeing what is in the kit or what kit is in the box, especially when there is a lot of stuff I've never seen before.

    Some unboxing blogs are much better and more interesting than others and I like watching them to learn what works and what doesn't work in trying to make an interesting unboxing blog. Although I agree unboxing is not the primary goal of a road test, it is definitely possible to make unboxing blogs both entertaining and informative - enhancing the road test.

    (I do not claim to have mastered thisimage)

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
<