E36313A Triple Output DC P.S.

View table of contents ...  

image

 

 

 

{tabbedtable} Tab LabelTab Content
About

The 160-Watt E36313A is a clean reliable bench power supply for general purpose applications. It combines next generation benchtop capabilities with flexible system features in a compact intuitive package. The E36313A is the best-in-class power supply of the E36300 Series product family. (The E36312A (80 W) offers the same feature set with reduced power and the E36311A (also 80 W) is the most economic model with reduced feature set for university classroom applications.)

image

Features

 

Clean, reliable power supply

  • Low, normal mode noise specifications assure quality power for precision circuitry applications enabling you to power your design with confidence.
  • Accurate voltage/current programming and read back capability provides excellent control to precisely power your device under test.
  • Characterizing small power devices with low current range to 1µA resolution.
  • Protection for your device under test (DUT) includes over voltage, over current, and over temperature protection.

 

Convenient benchtop capabilities

  • Three independent outputs in one instrument saves maintenance cost and bench space.
  • One of the quietest power supplies in its class provides a quiet and undisturbed work environment.

 

Compact, intuitive package

  • 4.3-inch LCD color display to show the voltage and current of all three channels at the same time.
  • Color-coded channels to simplify manual set-up.

 

Increased capability for increased productivity

  • Simultaneously log time-stamped data to the large color display and external USB thumb drive for data analysis. USB/LAN with Option GPIB available.
  • Generate complex sequences of output changes with rapid, precise timing and synchronized with internal or external signals to simulate on/off modes of your device.
  • Automatically set channels 2 and 3 to series or parallel to double the output voltage or current when a little more is needed.
  • Account for voltage drop in the power leads to achieve tight regulation and high voltage measurement accuracy with 4-wire remote sensing.
Specifications

Output Rating- 160 W

  • Output 1: 0 to 6 V, 0 to 10 A
  • Output 2: 0 to 25 V, 0 to 2 A
  • Output 3: 0 to 25 V, 0 to 2 A

 

Programming Accuracy ±(% of output + offset)

  • Voltage: 0.03% + 3 mV, 0.03% + 5 mV, 0.03% + 5 mV
  • Current: 0.05% + 4 mA, 0.04% + 3 mA, 0.04% + 3 mA

 

Ripple & Noise (20 Hz to 20 MHz)

  • Normal Mode Voltage: <350 µVrms/ 2 mV p-p, < 1 mVrms/ 5 mVpp, < 1 mVrms/ 5 mVpp
  • Normal-mode current: <4 mA rms, <2 mA rms, <1 mA rms

 

Readback Accuracy ±(% of output + offset)

  • Voltage: 0.04% + 3 mV, 0.03% + 5 mV, 0.03% + 5 mV,
  • Current: + 0.05% + 5 mA, 0.04% + 3 mA, 0.04% + 3 mA,
  • Low Range Current, 20 mA: 0.25% + 80 uA, 0.25% + 80 uA, 0.25% + 80 uA
Important Dates

Enrollment Begins: Oct 10 2017

Enrollment Ends: Nov 14 2017

RoadTesters Selected: Dec 1 2017

Product Shipped: Dec 5 2017

RoadTesting Begins: Dec 12 2017

Reminder/Update Email: Jan 12 2018*

Submit Reviews By: Feb 12 2018**

 

*The element14 RoadTest Staff will send this reminder/update email.

**If a RoadTester is unable to meet the deadline, please notify the RoadTest Program Lead, , as soon as possible before the deadline.

RoadTesters

These applicants were selected as official roadtesters:

 

Terms and Conditions

Keysight Triple Output DC Power Supply – RoadTest

Terms and Conditions

These are the terms and conditions which govern the Keysight Triple Output DC Power Supplyt RoadTest contest. This Contest requires participants to submit an application indicating their previous experience with this type of equipment/component, information on what they would do to test the equipment/component, and the applicant’s desire to post a thorough review of their experience with images, photos, or other supplemental materials. Participants will be required to meet the Conditions for Participation.  The winners of this RoadTest will receive the item(s) listed below. RoadTest Reviews are due no later than 60 days after the receipt of the item(s). No other prizes are offered.

The Principal terms of the Competition:

The following words and phrases are used in these terms and conditions and have the meanings given to them below.

RoadTest: Keysight Triple Output DC Power Supply

(RoadTest or Contest)

Key dates:

Applications Close: midnight (GMT) on 14 Nov 2017

Announcement of Winner (estimated):21 Nov 2017

 

Prize: Keysight Triple Output DC Power Supply

Additional Prizes: none

Competition Site: https://www.element14.com/community/groups/roadtest?ICID=menubar_resources_roadtest

Site or element14 Community: www.element14.com/community

Judges: members of the element14 community team chosen at the Organiser’s discretion.

Judging Criteria, All of the following which will have equal weighting:

· Demonstrated competence with the technologies including links or descriptions of past projects

· Qualifications as indicated by current job role and/or schooling/vocational training;

· A thorough description of how the prize would be tested;

· Likelihood that the Applicant will blog about the prize and provide a review on element14.com;

· Originality;

· Innovation.

Organiser: Premier Farnell plc (registered in England and Wales under company number 876412) whose registered office is at Farnell House, Forge Lane, Leeds, UK

Conditions for Qualification: in addition to meeting the requirements of these terms, all persons applying to take part in the Contest (each one an Applicant) must:

· Provide a RoadTest application describing what he/she would do if awarded the Prize including similar previous projects, product experience and qualifications

Terms: these terms and conditions which govern the Competition and to which the Organiser reserves the right to make changes from time to time and the latest version of these Terms from time to time will be posted to the Site.

  1. Eligibility
  2. Applications:
  3. Selecting Winners:  
  4. Liability:
  5. General:

1.1 Save as set out in these Terms, the Contest is open to any natural or legal person, firm or company or group of natural persons or unincorporated body.

1.2 All Applicants must be aged at least 18 at the time of their application.

1.3 Applicants must not enter the RoadTest if doing so or taking part may:

1.3.1 cause the Organiser and/or themselves to be in breach of any agreement (including but not limited to any contract of employment) to which they are a party or in breach of any law, regulation or rule having the force of law to which the Organiser or the Applicant may be subject or any policy of the Organiser or the Sponsor;

1.3.2 Require the Organiser to obtain any licence, authorisation or permission to deal with the Applicant; or

1.3.3 Be in breach of any policy or practice of their employer. Some employers prohibit or restrict their employees from taking part in competitions such as these or receiving prizes under them and the Organiser respects those policies and practices.

The Organiser reserves the right to disqualify any Application made in breach of these Terms and to reject any Application which it reasonably believes may be or become in breach. The Organiser reserves the right to require evidence in such form as the Organiser may reasonably require of any Applicant’s compliance with any of these Terms and to disqualify any Applicant or Participant who cannot provide such evidence reasonably promptly.

1.4 Multiple applications are not permitted.

1.5 Applications may not be submitted by an agent whether acting on behalf of an undisclosed principal or otherwise.

1.6 The Contest is NOT open to:

1.6.1 Any person or entity who is a resident or national of any country which is subject to sanctions, embargoes or national trade restrictions of the United States of America, the European Union or the United Kingdom;

1.6.2 Any employee, director, member, shareholder (as appropriate) or any of their direct families (parents, siblings, spouse, partner, children) (“Direct Families”) of the Organiser and Sponsors; or

2.1 Each Applicant must fully complete and submit a RoadTest Application by the Application Close.

2.2 By submitting a Registration Form, each Applicant:

2.2.1 Authorises the Organiser to use his or her personal data (as defined in the Data Protection Act 1998) for the purposes of running and promoting the RoadTest;

2.2.2 Authorises the Organizer to copy, reproduce and publish their application should they be accepted as a Participant;

2.2.3 Will be deemed to have read, accepted and agree to be bound by these Terms. Applicants are advised to print and keep safe these Terms;

2.2.4 Authorises the Organiser to copy, reproduce and use the Application and/or Review for the purposes of the RoadTest and as otherwise contemplated by these Terms. The Organiser will not be responsible for any inaccuracy, error or omission contained in any reproduction or use of the Project Blogs.

2.2.5 Licenses the Organiser to use the intellectual property in the Project (IP) for the purposes of this Contest. As between the Applicant and the Organiser the IP remains owned by the Applicant.

2.2.6 Grants the Organiser the right to use his or her likeness, photographs, logos, trademarks, audio or video recordings without restriction for the purposes of Contest or the promotion of it or the Site;

2.2.7 Agrees to participate positively in all publicity surrounding the Contest;

2.2.8 Agrees to be responsible for all expenses and costs incurred by him or her in preparing for, entering and participating in the Contest (save for any expenses expressly agreed by the Organiser to be borne by it in these Terms);

2.2.9 Confirms that he or she owns all IP used in his or her application or Project or Blogs and indemnifies the Organiser from any claim by a third party that use of any material provided by an Applicant to the Organiser infringes the intellectual property rights of any third party;

2.2.10 Agrees not to act in any way or fail to act in any way or be associated with any cause or group which would have a negative impact on the reputation of the Organiser and/or the RoadTest.

2.3 All applications submitted to this RoadTest must meet the following criteria:

2.3.1 Applicants must be the author, creator and owner of the proposed review idea. Applicants must not submit someone else’s idea;

2.3.2 The proposed application must be reasonably achievable by the within the time constraints of the Contest;

2.3.3 Applications must not include or propose any of the following, the inclusion of which shall render any proposed application ineligible:

(a) Applications which relate to socially taboo topics, such as illicit drug use or sexual gratification;

(b) Applications that are or could reasonably be considered to be illegal, immoral, discriminatory or offensive as determined by the Organiser;

(c) Applications in relation to them which if accepted would infringe or breach any of the policies or terms of access or use of the Site.

2.4 No Application may contain any of the hazardous substances identified by Article 4 of Directive 2002/95/EC of the European Parliament on the Restrictions on the Use of Substances in Electronic and Electrical Equipment ("the Directive") or the use of such hazardous substances in the in any such Project must not exceed the maximum concentration values set out in the Directive.

3.1 Winners will be selected by the Organiser on the basis of the quality of his or her application and its adherence to these Terms.

3.2 The total number of Winners selected will be at least the minimum number set out above but the actual number is at the sole discretion of the Organizer and/or the Sponsor, if applicable.

3.3 The Organiser will use all reasonable efforts to announce the Winners via an update to the RoadTest page by the date listed above.

3.4 Winners agree to take part in all publicity which the Organiser or the Sponsor wishes to use to promote the RoadTest, the Products featured or other Contests with which the Organiser may be connected from time to time.

3.5 Details of the Winners may also be published in the media.

3.6 Winners are responsible for all applicable taxes, duties or other charges payable in relation to any prize.

3.7

4.1 The Organiser hereby excludes all and any Liability arising out of the Contest or the acceptance, use, quality, condition, suitability or performance of any Prize, even where that Liability may arise from the Organiser’s negligence.

4.2 Nothing in these Terms will affect any Liability of the Organiser for death or personal injury arising from its negligence, for breach of Part II of the Consumer Protection Act 1987 (in the event that any entrant is entitled to claim rights under the Consumer Protection Act 1987) or for any matter in relation to which it would be illegal for the Organiser to exclude or to attempt to exclude its Liability.

4.3 Subject to 4.2, neither the Organiser, any parent company nor any subsidiary of the Organiser or such parent company or any of their directors, officers and employees (together referred to in these terms and the ‘Associates’) makes any guarantee, warranty or representation of any kind, express or implied, with respect to this Competition or the Prizes potentially available under it. Neither the Organiser nor any of its Associates shall be responsible for any Liability that may arise out of or in connection with person’s participation in this Competition, the claiming, redemption or value of any prizes under it, the use or enjoyment of such prizes or any events or circumstances arising out of or in connection with any of them. Any implied warranties of condition, merchantability or suitability or fitness for purpose of any of them are hereby expressly excluded. Wherever used in these Terms, ‘Liability’ shall mean any and all costs, expenses, claims, damages, actions, proceedings, demands, losses and other liabilities (including legal fees and costs on a full indemnity basis) arising directly or indirectly out of or in connection with the matter concerned.

5.1 The RoadTest is organised and sponsored by the Organiser. The Organiser reserves the right to delegate all or any of its powers, rights and obligations arising in relation to the RoadTest to any Associate and certain such rights and powers are assumed by the Organiser on behalf of itself and each Associate. Reference to “Organiser” shall be deemed to include reference to each Associate.

5.2 The RoadTest may be terminated at any time if there are, in the sole opinion of the Organiser, an insufficient number of entries, or if the Applications are not of an appropriate standard for a competition of this nature. The Organiser has the right to cancel or suspend the RoadTest at any time due to circumstances outside its reasonable control.

5.3 The Organiser shall have the sole discretion to disqualify (without correspondence or right of appeal) any Applicant it considers to be adversely affecting the process or the operation of the RoadTest or to be in breach of these Terms or to be acting in a disruptive manner or with intent to annoy, abuse, threaten or harass any other Applicant or Participant.

5.4 The Organiser has the right to amend or add to these Terms from time to time. Revised Terms and Conditions will be posted on the Contest Site and it is a condition of entry to the RoadTest that Applicants agree to comply with these Terms and, if appropriate, such Terms as amended from time to time.

5.5 Headings are for convenience only and do not affect the interpretation or construction of these Terms and Conditions.

5.6 These Terms and the operation of the Contest shall be governed by and construed in accordance with English Law and any claim or matter arising under these Terms shall be subject to the exclusive jurisdiction of the English courts.

Video

.

Additional Information

Keysight Technologies Practical Tips to Help You Get the Most Out of the E36300 Series Bench Power Supplies

RoadTest Reviews
Comments
Anonymous
  • Any update on who was selected as the road testers?

  • I guess that is the new thing compared to previous generations that output 2 and 3 are isolated from each other, but can be joined together electronically.

  • No, the data sheet explicitly says that the channels (at channels 2 and 3) are electrically isolated.

  • I don't think there isolated from each other. Possibly from the rest of the

    power supply  but there is a common 0v point .

     

    The signal drive is very week so you probably need and interface circuit

    anyway so if you need complete independence that would be easy to build

    with opt isolators

     

     

    On November 16, 2017 3:10:23 PM "DiligentMinds.com"

  • On one of the Keysight videos on this power supply series, they go into the feature set-- one of the most intriguing is that you can set up the 3 outputs to turn on and off in a certain sequence!  This is sometimes necessary with certain mixed-signal parts-- and this would really help when working with mixed-signal projects.  I also like that the 3 outputs are isolated from each other-- if you want them to have a common reference, you can tie them together through the user interface-- WOW!  I was going to buy a Rigol 832 (as I can afford that)-- but am waiting for the outcome of this road-test.  This supply on first-glance appears to be vastly superior to the Rigol 832 (at 3X the price-- you would expect that though).  It seems the Keysight engineers thought of everything on this supply (especially the separate voltage and current knobs).  I can't wait to see everyone's reviews on this product!

  • For me, the worst was a government project I worked on, this required what we called "Point In Time Architecture" for the Database, not only did it need to handle TimeZones but also an additional dimension of when the question is being asked

     

    So if you asked a question like how old someone was based on a date/time, the question also had to consider when the question is being asked (This was also provided as a parameter), so if today you are 20 but a week ago the database was updated, and I asked how old if I asked a week ago but im asking now, it had to consider any database updates, changes in the clock and all the fun stuff like did we change due to timezone too. this is no easy task, especially to just get your head arround. this also had to factor in single point values like a date of birth but items that can change like say salary... it was a nightmare

  • Hi Randall!

     

    Thank you very much!

    If i were elected, i will bring the review as soon as possible.

    This E36313A is a fine device for many of my application development.

     

    Best Regards

    Gerald

    ---

  • For us its the same - the application internally works with UTC and stores anything time-related that way. The fun starts with its users, since it will be used world-wide, in multiple time zones. So one user might enter a time in one time-zone, and then another one uses this in a different time zone. This can get confusing. Especially when you then need to store 'dates' (as in 'birthday') which internally are just a time stamp with 00:00 as a time. Yet they need to work in the users time zone correctly. (I think we still have test in that area which will fail on the next 29th of February...)

    Fun fact: did you know that all time zones called 'Etc/*' are handled backwards? E.g. 'Etc/-11' is actually 'UTC+11' which is just strange.

  • At work we have everything in UTC.

    All the alarm logs, operating systems, NOTAMs, Flights in fact everything related to the Operational side (which is why we are there) is UTC.

     

    I think all of us understand what "UTC" is...

    All except the managers ...

    We now have the manitenance recording system in local time, because they didn't think to have a user preference about your time setting (despite us suggesting and asking for it).

     

    So we are constantly battling with converting UTC to Local time and just for fun, NZ has Daylight saving. So sometimes it's 13 hrs, and the rest of the time it's 12 hrs.

    Mistakes do happen because of this, and it causes confusion in multiple places.

     

     

    Now that the little bug has been spotted, it's a matter of squashing it.

     

    Cheers

    Mark

  • That video reminded me that UTC <> GMT, they are out by a fraction of a second.

  • I've given the Exterminator badge to &

     

    Thanks for your help in identifying this issue image

  •  

    In this particular instance for the countdown clock - the code shouldn't be nearly as hard as this video makes it seem - because it doesn't really matter what timezone the browser is in. What matters is what the time is on the server and when the roadtest ends on the server.

     

    We have libraries to handle this thankfully - as said, it's just a handling of the GMT on the time string.

  • Time zones can be real problem.  For example, Venezuela sets their local time 30 minutes off from everyone else in the world.  Why?  Maybe to just be different?  If I had my way, everyone in the world would set their clocks to UTC, and there would not be any "time zones" or "daylight savings" adjustments anywhere, ever.  People would quickly get used to the idea of going to work at a UTC time that makes sense for their local area, and their hours of operation would reflect this.  That way, everyone everywhere would be on the same page.

  • Uhhh... I'll get my own line of code in Element14 ;-)

  • My last place, we had a horrible time with timezones - the original developer who had coded it had coded the timezone offset field to be an integer.

     

    My, how we had fun when we had our first customer with an office in India...

  • if (username==='berniwa') {

         print "ONLY APPLICANTS WITH THEIR LOCAL CLOCK SET TO GMT/UTC WILL BE ALLOWED" ;

    }

  • To All RoadTest Applicants,

     

    I just discovered after reading the comments that something was funny about the closing time. My apologies.

     

    I re-opened it until 23:59 tonight (CST).

     

    Feel free to apply.

     

    I'll hold off sending the applications to the supplier until tomorrow.

     

    Randall Scasny

    RoadTest Program Manager

  • See that's how I deal with it image Pass it to someone else. Much easier!