3 Series MDO Mixed Domain Oscilloscope

View table of contents ...  

image

 

{tabbedtable} Tab LabelTab Content
About

The 3 Series MDO minimizes rack or bench space by integrating multiple instrument, which combines analog, digital, and RF measurements with a signal source in a single, small (5.9 in., 149 mm deep) instrument. The combination of a small instrument and high level of integration aids in the teaching of various electronics principles as well as in its usage for more sophisticated lab experiments. Fully upgradable bandwidths and options enable adding functionality over time.

image

Installed Options

  • 1GHz bandwidth for analog channels
  • Arbitrary Function Generator
  • 16-digital channels
  • Spectrum analyzer, input frequency range 9khz to 3 Ghz and capture bandwidth 3 Ghz
  • Embedded serial triggering and analysis (I2C and SPI)

 

Main Features

  • 4 analog channel model
  • Large 11.6" (1920 x 1080 HD resolution) capacitive touch display, highly intuitive user interface
  • 1 GHz bandwidth version installed
  • Up to 5 GS/s sample rate
  • 10 M record length on all channels
  • >280,000 wfm/s maximum waveform capture rate
  • Standard passive voltage probes with 3.9 pF capacitive loading and 250 MHz or 500 MHz analog bandwidth
  • A DVM/frequency counter added at no cost following product registration
  • Option to add spectrum analyzer hardware at 1GHz or 3GHz
  • Debug complicated embedded designs with a wide range of serial decodes
  • 6-in-1 instrument integration

 

Applications

  • Aerospace, Defence, Military, Electronics Design, Embedded Design & Development, Lighting, Motor Drive & Control, Power Management, Power Supplies, Research & Development, Sensing & Instrumentation, Wireless

 

Contents

  • MDO34, One TPP0500 500 MHz passive probe per analog channel, Power cord, Calibration certificate documenting traceability to National Metrology Institute(s) and ISO9001/ISO17025 quality system registration, 3-year warranty covering all parts and labor on the instrument. 1-year warranty, parts and labor, on included probes.

 

Additional Information

Important Dates

Enrollment Begin: Sept 24 2019

Enrollment Ends: Oct 30 2019

RoadTesters Selected: Nov 21 2019

Product Shipped: Nov 21 2019

RoadTesting Begins: Nov 29 2019

Reminder/Update Email: Dec 29 2019

Submit Reviews By: Jan 29 2020

*The element14 RoadTest Staff will send this reminder/update email.

**If a RoadTester is unable to meet the deadline, please notify the RoadTest Program Lead, , as soon as possible before the deadline.

RoadTesters

Terms and Conditions

 

Roadtest

Terms and Conditions

Tektronix 3 Series MDO Mixed Domain Oscilloscope

 

These are the terms and conditions which govern the Tektronix 3 Series MDO

Mixed Domain Oscilloscope contest. This Contest requires participants to submit an application indicating their previous experience with this type of equipment/component, information on what they would do to test the equipment/component, and the applicant’s desire to post a thorough review of their experience with images, photos, or other supplemental materials. Participants will be required to meet the Conditions for Participation.  The winners of this RoadTest will receive the item(s) listed below. RoadTest Reviews are due no later than 60 days after the receipt of the item(s). No other prizes are offered.

 

The Principal terms of the Competition:

The following words and phrases are used in these terms and conditions and have the meanings given to them below.

(RoadTest or Contest)

Key dates:

Applications Close: midnight (GMT) on Oct 30 2019

Announcement of Winner (estimated): Nov 10 2019

Prize:

3 Series MDO Mixed Domain Oscilloscope

 

Additional Prizes: none

Competition Site: https://www.element14.com/community/groups/roadtest?ICID=menubar_resources_roadtest

Site or element14 Community: www.element14.com/community

Judges: members of the element14 community team chosen at the Organiser’s discretion.

Judging Criteria, All of the following which will have equal weighting:

· Demonstrated competence with the technologies including links or descriptions of past projects

· Qualifications as indicated by current job role and/or schooling/vocational training;

· A thorough description of how the prize would be tested;

· Likelihood that the Applicant will blog about the prize and provide a review on element14.com;

· Originality;

· Innovation.

Organiser: Premier Farnell plc (registered in England and Wales under company number 876412) whose registered office is at Farnell House, Forge Lane, Leeds, UK

Conditions for Qualification: in addition to meeting the requirements of these terms, all persons applying to take part in the Contest (each one an Applicant) must:

· Provide a RoadTest application describing what he/she would do if awarded the Prize including similar previous projects, product experience and qualifications

Terms: these terms and conditions which govern the Competition and to which the Organiser reserves the right to make changes from time to time and the latest version of these Terms from time to time will be posted to the Site.

  1. Eligibility
  2. Applications:
  3. Selecting Winners:
  4. Liability:
  5. General:

1.1 Save as set out in these Terms, the Contest is open to any natural or legal person, firm or company or group of natural persons or unincorporated body.

1.2 All Applicants must be aged at least 18 at the time of their application.

1.3 Applicants must not enter the RoadTest if doing so or taking part may:

1.3.1 cause the Organiser and/or themselves to be in breach of any agreement (including but not limited to any contract of employment) to which they are a party or in breach of any law, regulation or rule having the force of law to which the Organiser or the Applicant may be subject or any policy of the Organiser or the Sponsor;

1.3.2 Require the Organiser to obtain any licence, authorisation or permission to deal with the Applicant; or

1.3.3 Be in breach of any policy or practice of their employer. Some employers prohibit or restrict their employees from taking part in competitions such as these or receiving prizes under them and the Organiser respects those policies and practices.

The Organiser reserves the right to disqualify any Application made in breach of these Terms and to reject any Application which it reasonably believes may be or become in breach. The Organiser reserves the right to require evidence in such form as the Organiser may reasonably require of any Applicant’s compliance with any of these Terms and to disqualify any Applicant or Participant who cannot provide such evidence reasonably promptly.

1.4 Multiple applications are not permitted.

1.5 Applications may not be submitted by an agent whether acting on behalf of an undisclosed principal or otherwise.

1.6 The Contest is NOT open to:

1.6.1 Any person or entity who is a resident or national of any country which is subject to sanctions, embargoes or national trade restrictions of the United States of America, the European Union or the United Kingdom;

1.6.2 Any employee, director, member, shareholder (as appropriate) or any of their direct families (parents, siblings, spouse, partner, children) (“Direct Families”) of the Organiser and Sponsors; or

2.1 Each Applicant must fully complete and submit a RoadTest Application by the Application Close.

2.2 By submitting a Registration Form, each Applicant:

2.2.1 Authorises the Organiser to use his or her personal data (as defined in the Data Protection Act 1998) for the purposes of running and promoting the RoadTest;

2.2.2 Authorises the Organizer to copy, reproduce and publish their application should they be accepted as a Participant;

2.2.3 Will be deemed to have read, accepted and agree to be bound by these Terms. Applicants are advised to print and keep safe these Terms;

2.2.4 Authorises the Organiser to copy, reproduce and use the Application and/or Review for the purposes of the RoadTest and as otherwise contemplated by these Terms. The Organiser will not be responsible for any inaccuracy, error or omission contained in any reproduction or use of the Project Blogs.

2.2.5 Licenses the Organiser to use the intellectual property in the Project (IP) for the purposes of this Contest. As between the Applicant and the Organiser the IP remains owned by the Applicant.

2.2.6 Grants the Organiser the right to use his or her likeness, photographs, logos, trademarks, audio or video recordings without restriction for the purposes of Contest or the promotion of it or the Site;

2.2.7 Agrees to participate positively in all publicity surrounding the Contest;

2.2.8 Agrees to be responsible for all expenses and costs incurred by him or her in preparing for, entering and participating in the Contest (save for any expenses expressly agreed by the Organiser to be borne by it in these Terms);

2.2.9 Confirms that he or she owns all IP used in his or her application or Project or Blogs and indemnifies the Organiser from any claim by a third party that use of any material provided by an Applicant to the Organiser infringes the intellectual property rights of any third party;

2.2.10 Agrees not to act in any way or fail to act in any way or be associated with any cause or group which would have a negative impact on the reputation of the Organiser and/or the RoadTest.

2.3 All applications submitted to this RoadTest must meet the following criteria:

2.3.1 Applicants must be the author, creator and owner of the proposed review idea. Applicants must not submit someone else’s idea;

2.3.2 The proposed application must be reasonably achievable by the within the time constraints of the Contest;

2.3.3 Applications must not include or propose any of the following, the inclusion of which shall render any proposed application ineligible:

(a) Applications which relate to socially taboo topics, such as illicit drug use or sexual gratification;

(b) Applications that are or could reasonably be considered to be illegal, immoral, discriminatory or offensive as determined by the Organiser;

(c) Applications in relation to them which if accepted would infringe or breach any of the policies or terms of access or use of the Site.

2.4 No Application may contain any of the hazardous substances identified by Article 4 of Directive 2002/95/EC of the European Parliament on the Restrictions on the Use of Substances in Electronic and Electrical Equipment ("the Directive") or the use of such hazardous substances in the in any such Project must not exceed the maximum concentration values set out in the Directive.

3.1 Winners will be selected by the Organiser on the basis of the quality of his or her application and its adherence to these Terms.

3.2 The total number of Winners selected will be at least the minimum number set out above but the actual number is at the sole discretion of the Organizer and/or the Sponsor, if applicable.

3.3 The Organiser will use all reasonable efforts to announce the Winners via an update to the RoadTest page by the date listed above.

3.4 Winners agree to take part in all publicity which the Organiser or the Sponsor wishes to use to promote the RoadTest, the Products featured or other Contests with which the Organiser may be connected from time to time.

3.5 Details of the Winners may also be published in the media.

3.6 Winners are responsible for all applicable taxes, duties or other charges payable in relation to any prize.

3.7

4.1 The Organiser hereby excludes all and any Liability arising out of the Contest or the acceptance, use, quality, condition, suitability or performance of any Prize, even where that Liability may arise from the Organiser’s negligence.

4.2 Nothing in these Terms will affect any Liability of the Organiser for death or personal injury arising from its negligence, for breach of Part II of the Consumer Protection Act 1987 (in the event that any entrant is entitled to claim rights under the Consumer Protection Act 1987) or for any matter in relation to which it would be illegal for the Organiser to exclude or to attempt to exclude its Liability.

4.3 Subject to 4.2, neither the Organiser, any parent company nor any subsidiary of the Organiser or such parent company or any of their directors, officers and employees (together referred to in these terms and the ‘Associates’) makes any guarantee, warranty or representation of any kind, express or implied, with respect to this Competition or the Prizes potentially available under it. Neither the Organiser nor any of its Associates shall be responsible for any Liability that may arise out of or in connection with person’s participation in this Competition, the claiming, redemption or value of any prizes under it, the use or enjoyment of such prizes or any events or circumstances arising out of or in connection with any of them. Any implied warranties of condition, merchantability or suitability or fitness for purpose of any of them are hereby expressly excluded. Wherever used in these Terms, ‘Liability’ shall mean any and all costs, expenses, claims, damages, actions, proceedings, demands, losses and other liabilities (including legal fees and costs on a full indemnity basis) arising directly or indirectly out of or in connection with the matter concerned.

5.1 The RoadTest is organised and sponsored by the Organiser. The Organiser reserves the right to delegate all or any of its powers, rights and obligations arising in relation to the RoadTest to any Associate and certain such rights and powers are assumed by the Organiser on behalf of itself and each Associate. Reference to “Organiser” shall be deemed to include reference to each Associate.

5.2 The RoadTest may be terminated at any time if there are, in the sole opinion of the Organiser, an insufficient number of entries, or if the Applications are not of an appropriate standard for a competition of this nature. The Organiser has the right to cancel or suspend the RoadTest at any time due to circumstances outside its reasonable control.

5.3 The Organiser shall have the sole discretion to disqualify (without correspondence or right of appeal) any Applicant it considers to be adversely affecting the process or the operation of the RoadTest or to be in breach of these Terms or to be acting in a disruptive manner or with intent to annoy, abuse, threaten or harass any other Applicant or Participant.

5.4 The Organiser has the right to amend or add to these Terms from time to time. Revised Terms and Conditions will be posted on the Contest Site and it is a condition of entry to the RoadTest that Applicants agree to comply with these Terms and, if appropriate, such Terms as amended from time to time.

5.5 Headings are for convenience only and do not affect the interpretation or construction of these Terms and Conditions.

5.6 These Terms and the operation of the Contest shall be governed by and construed in accordance with English Law and any claim or matter arising under these Terms shall be subject to the exclusive jurisdiction of the English courts.

Tax IssuesIf you are a U.S. taxpayer, you will be required to complete a W-9 form and we will issue you a 1099 form. If you are not a U.S. tax payer, you need to follow the tax laws in your country as per the terms & conditions of this contest.
RoadTest Reviews
Comments
Anonymous
  • I'm waiting on the sponsor to decide.

  • - I don't think they will be that quick to decide on the recipients and alternate back-up reviewer. Sometimes it can take a week or two. Sometimes the chosen people do not respond within 24 hours and the alternate needs to be selected. Don't give up hope just yet - not until the official RoadTesters have been announced by on this page.

     

    That being said ... on probability ... with an even-odds chance of 1/56 of winning, there's a fair chance you might have to go and buy a new oscilloscope ...

     

    - Gough

  • Hi,

    I have not yet received news so that I think I have to go to buy a new oscilloscope. image

    Bye

  •   hang tight, you will get an email if selected which you should reply to as quick as possible. Good luck!

  • Hi Randall,

    I'm sweating, the wait is terrible!!

     

    When will the sponsor make it public?

    Will he contact only the winner or all applicants?

     

    Regards,

    Fulvio

  • To all applicants.....

     

    I sent the applications off to the sponsor.

     

    Randall

  • Bus pirate v3.6 is using FT232RL and its data transfer capability and features are very small as compared to FT232H (FT2232HL is same as FT232H but with dual interfaces). In term of speed, its closest alternate is cypress CY7C68013A.

    Bus pirate is using pic mcu to implement various protocols but FT232H has various built in functionalities.

  • A DC block is also a handy inline addition !

  • If you're going to get near field probes, you might want to go a bit higher in price, otherwise you will get better results with home made ones.

  • These probes work well on my Rigol

    image

  • If you want to generate these protocols without programming, a Bus Pirate is also a good utility. You can script uart, spi, i2c.

  • FT2232HL IC can be an ideal test subject for logic analyzer testing. It can be used as dual channel uart, i2c, spi, jtag, fifo, bitbang or combination of any two of these interfaces.

     

    I have ordered this IC board few days ago and I am planning to it as usb2.0 (480Mbps) interface between FPGA board (Digilent Cmod S6) and PC.

    https://www.ftdichip.com/Products/ICs/FT2232H.htm

  • To all roadtesters......

     

    I went through all the first-cut applications again. All 27 of them. For the 2nd cut, I brought it down to 11.

     

    These were compelling applications that promised to explore the full capabilities this scope.

     

    Now, I normally would do a third-cut in this case in order to send my selections to the sponsor. But the 11 applications are all very good and I would be happy with any of them. So, I made extensive notes and observations on each of them. I will send all 11 to the sponsor. We will decide on the 2 winners and an alternate together.

     

    Randall Scasny

    RoadTest  Program Manager

  • Thanks for this warning. It would be a pity if a reviewer destroys such a beautyfil piece of equipment!

  • Ever since the earlier MDO 3000 came out (which I've been fortunate enough to use) and now hearing about this successor 3 series, I've long thought these should win some product award (if they haven't already). There's so many capabilities packed in it, and of course it's quite a leap having the ability to look at signals in the frequency domain as well as the time domain, and along with the the 4000 and 4 series, they're the only instruments that do this well. There's some that may think that FFT on other 'scopes may be similar, but it really isn't, it is a world apart. I feel there's plenty of users who would benefit from spectrum analyser capabilities, but possibly either don't initially realise it, or try to work around it.. now they don't need to.

     

    There's enough capability in it to provide many years of functionality, as their needs evolve, to suit all sorts of engineers. The capabilities of the older 3000 series were immense, and the probes are really nice too.. definitely some innovation there for 1GHz capable passive probes, and there's memory in them, they self-calibrate and remember their adjustments. Although some of that is available on other 'scopes too, in any case the probe interface (it is called TekVPI) is nice, it is push-to-fit, no twisting BNCs to attach the probes.

     

    Whoever reviews these, I hope they take care to protect the spectrum analyser input.. leaving an attenuator on there initially perhaps, and thinking twice before proceeding with attaching anything to it, is highly recommended as a bit of protection.

  • woooooo, pricey, but so pretty!

  • Yes, this is a spectacular test instrument. More bandwidth and more options than the majority of engineers will ever need.

    It 'll also make it difficult to test correctly - in particular the high frequency will require the right skills.

  • To all applicants.....

     

    I am relaxed now. No one meetings, no calls. no editing. no research. So I figured I would take advantage of it to go through the first-cut list and do the next round.

     

    To do so, I went back to the literature on this product to refresh in my mind what it can do. First off, it's a multifunctional device: o'scope, arbitrary function generator, spectrum analyzer. It's a great tool for debugging.

     

    This line impressed me: "Verifying that your prototype's performance matches simulations and meets the project's design goals requires careful analysis."

     

    power analysis testing, rf measurement, serial protocol analysis

     

    So, this is a great tool.

     

    Randall

  • Sounds like there is a strong field of contenders for this Road Test.

     

    Will there be a third cut, or do the 27 go to Tektronix now with your recommendations?