We're Giving Away 10 Intel®Edison Kits for Arduino

View table of contents ...  

image

 

{tabbedtable} Tab LabelTab Content

About This RoadTest

RoadTest Review the Intel® Edison Kit for Arduino!

 

To apply, click on the "Enroll" button found in the top right box of the page. Fill out the application, and let us know what you would do with the kit and why you should be chosen to review it. If selected, we will notify you via the community  and send you over the kit. From the time you receive the kit, you will have 60 days to post an honest and detailed review of the kit. After posting, the kit is yours to keep.

 

About the Kit [1]


The Intel® Edison Kit for Arduino features the Intel® Edison module which is a SoC (System on Chip) that includes an Intel® Atom™ 500MHz dual-core, dual-threaded CPU and an Intel® Quark™ 100MHz microcontroller. This module has integrated Wi-Fi and Bluetooth 4.0LE and supports Yocto Linux, Node.js and Wolfram.

 

The kit  provides the Arduino 1.0 pin-out and standard connectors such as a micro USB connected to a UART, a USB OTG port that can be switched between a second micro USB device connector, a standard size USB host Type-A connector, a uSD card holder, and a DC power jack.This provides the potential for 20 digital input/output pins, of which 6 can be used as analog inputs. The Intel® Edison has 4 PWM outputs which can be configured via jumpers to any of the 6 pins supporting PWM on the Arduino Uno (pins 3, 5, 6, 9, 10, or 11). It is designed to be hardware and software pin-compatible with Arduino shields designed for the Arduino Uno R3. Digital pins 0 to 13 (and the adjacent AREF and GND pins), Analog inputs 0 to 5, the power header, ICSP header, and the UART port pins (0 and 1), are all in the same locations as on the Arduino Uno R3. The digital IOs and analog pins can be configured to operate at either 5V or 3.3V. The outputs can source or sink 24 mA at 3.3V and 32 mA at 5V.

 

[1][ Arduino - IntelEdison. (n.d.). Retrieved March 17, 2016, from https://www.arduino.cc/en/Guide/IntelEdison#toc1

{gallery} intel

image

image

image

image

image

image

The RoadTesters

Congrats to the below selected RoadTesters:

mschambe

The kit will be sent out shortly. You will have 60 days to submit a RoadTest review. You can create your reviews by selected "Create" from the top menu and "RoadTest Review". You will be able to see this RoadTest as an option to write the review. Have fun!

Terms and Conditions

Intel Edison Kit for Arduino

Terms and Conditions

 

These are the terms and conditions which govern the Intel Edison Kit for Arduino RoadTest. This Contest requires participants to submit an application indicating their previous experience with this type of equipment/component, information on what they would do to test the equipment/component, and the applicant’s desire to post a thorough review of their experience with images, photos, or other supplemental materials.. Participants will be required to meet the Conditions for Participation.  The winners of this RoadTest will receive the item(s) listed below. RoadTest Reviews are due no later than 60 days after the receipt of the item(s). No other prizes are offered.

1. 1 The Principal terms of the Contest:

The following words and phrases are used in these terms and conditions and have the meanings given to them below.

RoadTest:Intel Edison Kit for Arduino (or the Contest)

Key dates:

Applications Close: 11:59 (GMT) on 29 April 2016

Judging Close: 29 April  2016

Announcement of Winner(s) (estimated):  29 April 2016

RoadTest Item(s): Intel Edison Kit for Arduino

 

RoadTest Site: www.element14.com/community/roadTests/XXXX

Site or element14 Community: www.element14.com

Judges: members of the element14 community team chosen at the Organiser’s discretion.

Judging Criteria: All of the following which will have equal weighting:

1.1 • Demonstrated competence with the technologies including links or descriptions of past projects

1.2 • Qualifications as indicated by current job role and/or schooling/vocational training;

1.3 • A thorough description of how the prize would be tested

1.4 • Likelihood that the Applicant will blog about the prize and provide a review on element14.com

1.5 • Originality;

1.6 • Innovation.

Organiser: Premier Farnell plc (registered in England and Wales under company number 876412) whose registered office is at Farnell House, Forge Lane, Leeds, UK

Conditions for Qualification: in addition to meeting the requirements of these terms, all persons applying to take part in the Contest (each one an Applicant) must:

1.7 • Provide a RoadTest application describing what he/she would do if awarded the Prize including similar previous projects, product experience and qualifications

Minimum number of Prizes: 10

Terms: these terms and conditions which govern the Contest and to which the Organiser reserves the right to make changes from time to time and the latest version of these Terms from time to time will be posted to the Site.

1. 2 Eligibility

2. 3 Applications:

3. 4 Selecting Winners:

4. 5 Liability:

5. 6 General:

1.8 2.1 Save as set out in these Terms, the RoadTest is open to any natural or legal person, firm or company or group of natural persons or unincorporated body.

1.9 2.2 All Applicants must be aged at least 18 at the time of their application.

1.10 2.3 Applicants must not enter the Contest if doing so or taking part may:

1.10.1 2.3.1 cause the Organiser and/or themselves to be in breach of any agreement (including but not limited to any contract of employment) to which they are a party or in breach of any law, regulation or rule having the force of law to which the Organiser or the Applicant may be subject or any policy of the Organiser or the Sponsor;

1.10.2 2.3.2 Require the Organiser to obtain any licence, authorisation or permission to deal with the Applicant; or

1.10.3 2.3.3 Be in breach of any policy or practice of their employer. Some employers prohibit or restrict their employees from taking part in contests such as these or receiving prizes under them and the Organiser respects those policies and practices.

1.10.4 The Organiser reserves the right to disqualify any Application made in breach of these Terms and to reject any Application which it reasonably believes may be or become in breach. The Organiser reserves the right to require evidence in such form as the Organiser may reasonably require of any Applicant’s compliance with any of these Terms and to disqualify any Applicant or Participant who cannot provide such evidence reasonably promptly.

1.11 2.4 Multiple applications are not permitted.

1.12 2.5 Applications may not be submitted by an agent whether acting on behalf of an undisclosed principal or otherwise.

1.13 2.6 The Contest is NOT open to:

1.13.1 2.6.1 Any person or entity who is a resident or national of any country which is subject to sanctions, embargoes or national trade restrictions of the United States of America, the European Union or the United Kingdom;

1.13.2 2.6.2 Any employee, director, member, shareholder (as appropriate) or any of their direct families (parents, siblings, spouse, partner, children) (“Direct Families”) of the Organiser.

1.14 3.1 Each Applicant must fully complete and submit a response by the Application Close.

1.15 3.2 By submitting a response, each Applicant:

1.15.1 3.2.1 Authorises the Organiser to use his or her personal data (as defined in the Data Protection Act 1998) for the purposes of running and promoting the RoadTest;

1.15.2 3.2.2 Authorises the Organizer to copy, reproduce and publish their application should they be accepted as a Participant;

1.15.3 3.2.3 Will be deemed to have read, accepted and agree to be bound by these Terms. Applicants are advised to print and keep safe these Terms;

1.15.4 3.2.4 Authorises the Organiser to copy, reproduce and use the application or subsequent Blogs submitted for the purposes of the Contest and as otherwise contemplated by these Terms. The Organiser will not be responsible for any inaccuracy, error or omission contained in any reproduction or use of the Project Blogs.

1.15.5 3.2.5 Licenses the Organiser to use the intellectual property in the Project (IP) for the purposes of this Contest. As between the Applicant and the Organiser the IP remains owned by the Applicant.

1.15.6 3.2.6 Grants the Organiser the right to use his or her likeness, photographs, logos, trademarks, audio or video recordings without restriction for the purposes of Contest or the promotion of it or the Site;

1.15.7 3.2.7 Agrees to participate positively in all publicity surrounding the Contest;

1.15.8 3.2.8 Agrees to be responsible for all expenses and costs incurred by him or her in preparing for, entering and participating in the Contest (save for any expenses expressly agreed by the Organiser to be borne by it in these Terms);

1.15.9 3.2.9 Confirms that he or she owns all IP used in his or her application or Project or Blogs and indemnifies the Organiser from any claim by a third party that use of any material provided by an Applicant to the Organiser infringes the intellectual property rights of any third party;

1.15.10 3.2.10 Agrees not to act in any way or fail to act in any way or be associated with any cause or group which would have a negative impact on the reputation of the Organiser and/or the Contest.

1.16 3.3 All applications submitted to this Contest must meet the following criteria:

1.16.1 3.3.1 Applications must not include or propose any of the following, the inclusion of which shall render any application null and void:

(a) (a) Applications or designs which relate to socially taboo topics, such as illicit drug use or sexual gratification;

(b) (b) Applications or designs that are or could reasonably be considered to be illegal, immoral, discriminatory or offensive as determined by the Organiser and/or the Judges;

(c) (c) Applications or applications in relation to them which if accepted would infringe or breach any of the policies or terms of access or use of the Site.

1.17 3.4 No proposed Application may contain any of the hazardous substances identified by Article 4 of Directive 2002/95/EC of the European Parliament on the Restrictions on the Use of Substances in Electronic and Electrical Equipment ("the Directive") or the use of such hazardous substances in the in any such Project must not exceed the maximum concentration values set out in the Directive.

1.18 3.5 A proposed Application must not have been entered into any other Contest, unless that Contest has closed and the Application did not win a prize.

1.19 4.1 Winners will be selected by the Organiser on the basis of the quality of his or her Application and its adherence to these Terms.

1.20 4.2 The total number of Winners selected will be at least the minimum number set out in condition 1 above but the actual number is at the sole discretion of the Organizer.

1.21 4.3 The Organiser will use all reasonable efforts to announce the Participants within 10 business days the Applications Close.

1.22 4.4 The winner(s) will be selected by the Organiser in their absolute discretion based on the Judging Criteria. Winners must meet all eligibility requirements of these Terms. There shall be such number of winners as the Organiser shall determine.

1.23 4.5 The Organiser’s decision is final and without right of appeal. No correspondence will be entered into. The Organiser reserves the right not to select a winner if, in their sole discretion, they do not consider any of the applications to merit the Prize.

1.24 4.6 The Organiser will use all reasonable efforts to complete judging by Judging and Voting Close and to notify the winner(s) via a blog posted on the Contest Site by the Announcement of Winner Date.

1.25 4.7 Winners agree to take part in all publicity which the Organiser or the Sponsor wishes to use to promote the RoadTest, the Products featured or other Contests with which the Organiser may be connected from time to time.

1.26 4.8 Details of the Winners will also be published in the media.

1.27 5.1 The Organiser hereby excludes all and any Liability arising out of the Contest or the acceptance, use, quality, condition, suitability or performance of any Prize, even where that Liability may arise from the Organiser’s negligence.

1.28 5.2 Nothing in these Terms will affect any Liability of the Organiser for death or personal injury arising from its negligence, for breach of Part II of the Consumer Protection Act 1987 (in the event that any entrant is entitled to claim rights under the Consumer Protection Act 1987) or for any matter in relation to which it would be illegal for the Organiser to exclude or to attempt to exclude its Liability.

1.29 5.3 Subject to 10.2, neither the Organiser, any parent company nor any subsidiary of the Organiser or such parent company or any of their directors, officers and employees (together referred to in these terms and the ‘Associates’) makes any guarantee, warranty or representation of any kind, express or implied, with respect to this Contest or the Prizes potentially available under it. Neither the Organiser nor any of its Associates shall be responsible for any Liability that may arise out of or in connection with person’s participation in this Contest, the claiming, redemption or value of any prizes under it, the use or enjoyment of such prizes or any events or circumstances arising out of or in connection with any of them. Any implied warranties of condition, merchantability or suitability or fitness for purpose of any of them are hereby expressly excluded. Wherever used in these Terms, ‘Liability’ shall mean any and all costs, expenses, claims, damages, actions, proceedings, demands, losses and other liabilities (including legal fees and costs on a full indemnity basis) arising directly or indirectly out of or in connection with the matter concerned.

1.30 6.1 The RoadTest is organised and sponsored by the Organiser. The Organiser reserves the right to delegate all or any of its powers, rights and obligations arising in relation to the RoadTest to any Associate and certain such rights and powers are assumed by the Organiser on behalf of itself and each Associate. Reference to “Organiser” shall be deemed to include reference to each Associate.

1.31 6.2 The RoadTest may be terminated at any time if there are, in the sole opinion of the Organiser, an insufficient number of entries, or if the Applications are not of an appropriate standard for a Contest of this nature. The Organiser has the right to cancel or suspend the RoadTest at any time due to circumstances outside its reasonable control.

1.32 6.3 The Organiser shall have the sole discretion to disqualify (without correspondence or right of appeal) any Applicant it considers to be adversely affecting the process or the operation of the RoadTest or to be in breach of these Terms or to be acting in a disruptive manner or with intent to annoy, abuse, threaten or harass any other Applicant or Participant.

1.33 6.4 The Organiser has the right to amend or add to these Terms from time to time. Revised Terms and Conditions will be posted on the RoadTest Site and it is a condition of entry to the RoadTest that Applicants and Winners agree to comply with these Terms and, if appropriate, such Terms as amended from time to time.

1.34 6.5 Headings are for convenience only and do not affect the interpretation or construction of these Terms and Conditions.

1.35 6.6 These Terms and the operation of the RoadTest shall be governed by and construed in accordance with English Law and any claim or matter arising under these Terms shall be subject to the exclusive jurisdiction of the English courts.

1.36 the exclusive jurisdiction of the English courts.

RoadTest Reviews
Comments
Anonymous
  • Makes me thing the board was a development one released.

  • Agree, it is a shame that there are not many smaller adapter boards at a good price - I'm guessing Intel hoped third parties would produce them where needed.

    As you say it is large-ish on the supplied Arduino-shield-compatible adapter board, and similar sized to a few older boards as you noticed - not much bigger than the 'pi, and (in practice) smaller than the original Pi with the sticking-out WiFi adapter. For prototyping it is a nice board as a result. I still don't like Arduino connector spacing, but at least it is a semi-standard that people can understand and work with quickly.

    image

    The good thing is that it should be still feasible to get a PCB made and build up a smaller adapter board by hand despite Edison's tiny size. For those who have not seen it in the flesh, it is about half the size of a Pi zero!

  • It would have to be a pretty special and specific application to get me to spend that kind of money.

    Yes but you'd also need to add level conversion to interface to most external intelligence.

    Sure pushbuttons and transistors will work, many opto-couplers might also work, but other that many others will need some form of conversion.

     

    Sadly this is a very capable and powerful device let down by it's interface.

     

     

    Mark

  • trouble was I didn't like the $156 price tag.!!

     

    I know, right !!??

    It would have to be a pretty special and specific application to get me to spend that kind of money.

  • I liked your link to the small board .... trouble was I didn't like the $156 price tag.!! image

    It's even expensive back at Adafruit at USD$74

     

    It only provides access to the GPIO and doesn't have level conversion, so while small makes the whole thing uneconomic.

     

     

    MANUFACTURERS

    If you want people to use your excellent products, consider making access to using them affordable and easy.

     

    Mark

  • This looks like a smallish breakout board for it, but the price leaves me wondering if it was made by Apple image

    EDI2BB.AL.K INTEL, X86 EDISON BREAKOUT BOARD KIT, Newark element14 Canada

     

    I see AdaFruit has a connector:

    https://www.adafruit.com/products/2227

  • If someone could make a connecting board that had

    I agree. Looking through the pictures above I noticed that odd little connector. I was hoping it could be easily programmed and tinkered with using the mother board, and then separated off to work its magic in a tiny little space where it's needed.

     

    I like that it's supported within the Arduino IDE, for easy programming: https://www.arduino.cc/en/Guide/IntelEdison

    but that seems to be a sad waste of a powerful SoC!

     

    Cheers,

    -Nico

  • Clem Martins wrote:

     

    I will byte. Why?

    When I first read of the Intel Edison, I noticed that the rhythm of the words exactly matched Maxwell Edison, the title character of the Beatles' "Maxwell's Silver Hammer" (1969) which I first heard at an impressionable age.  "PC31" (Police Constable #31) begins the third stanza.

  • Not to shoot the messenger of this RoadTest ...

     

    I purchased one of these.

    They are a very small (that is a AA battery next to it)

    The second image shows it on the "mother board"  with a VoCore superimposed at the same scale.

     

    image  image

     

     

    I have some concerns that the connection system lets it down.

    In order to power it, you need to attach it to a "mother board" of some description.

     

    At the time of purchase most of the boards were almost as large, and many didn't include the necessary level converters to be able to connect with even the 3v3 devices.

    I didn't get to chase down any connectors.

     

    Sadly the makers did not think to make it a little more self contained.

    I returned it to it's very nice box.

     

    If someone could make a connectng board that had :-

    1.     Power connections and a step down regulator.

    2.     Level interfacing to allow 3v3 or 5v device to interface to it.

    3.     A number of I/O pins so that you could join wires on.

    4.     A size profile that was no larger than the original device with fixing holes.

     

    You would be onto a winner.

     

     

    Mark

  • If I had an Intel Edison, majoring in medicine, I'd make a PC 31 image