Enrollment closes in
Days 0 Hours 0 Mins 0 Secs 0
| {tabbedtable} Tab Label | Tab Content | |||
|---|---|---|---|---|
| About This RoadTest | The Educational BoosterPack MKII is an add-on board designed to expand your evaluation of and development with the MSP-EXP432P401R LaunchPad. The Educational BoosterPack MKII offers a high level of integration for developers to quickly prototype complete solutions. Various analog and digital inputs/outputs are at your disposal including an analog joystick, temperature sensor, RGB LED, microphone, buzzer, color LCD display, and more.
The MSP432P401R LaunchPad, enables you to develop high performance applications that benefit from low power operation. It features the MSP432P401R – which includes a 48MHz ARM Cortx M4F, 95uA/MHz active power and 850nA RTC operation, 14-bit 1MSPS differential SAR ADC and AES256 accelerator. This Launchpad includes an on-board emulator with EnergyTrace+ Technology, which means you can program and debug your projects without the need for additional tools, while also measuring total system energy consumption.
RoadTesters Selected:
| |||
| Product Features | Educational BoosterPack MKII Features:
MSP432P401R LaunchPad Features:
| |||
| Terms and Conditions | Texas Instruments Educational Boosterpack II Terms and Conditions
These are the terms and conditions which govern the Texas Instruments Educational Boosterpack II RoadTest. This Contest requires participants to submit an application indicating their previous experience with this type of equipment/component, information on what they would do to test the equipment/component, and the applicant’s desire to post a thorough review of their experience with images, photos, or other supplemental materials.. Participants will be required to meet the Conditions for Participation. The winners of this RoadTest will receive the item(s) listed below. RoadTest Reviews are due no later than 60 days after the receipt of the item(s). No other prizes are offered.
The following words and phrases are used in these terms and conditions and have the meanings given to them below. RoadTest: Texas Instruments Educational Boosterpack II (or the Contest) Key dates: Applications Close: 11:59PM (GMT) on 28 September 2015 Judging Close: midnight (GMT) on 9 October 2015 Announcement of Winner(s) (estimated): 13 October 2015 RoadTest Item(s): MSP-EXP432P401R, Educational BoosterPack MKII RoadTest Site: http://www.element14.com/community/roadTests/1479 Site or element14 Community: www.element14.com Judges: members of the element14 community team chosen at the Organiser’s discretion. Judging Criteria: All of the following which will have equal weighting:
Organiser: Premier Farnell plc (registered in England and Wales under company number 876412) whose registered office is at Farnell House, Forge Lane, Leeds, UK Conditions for Qualification: in addition to meeting the requirements of these terms, all persons applying to take part in the Contest (each one an Applicant) must:
Minimum number of Prizes: 10 Terms: these terms and conditions which govern the Contest and to which the Organiser reserves the right to make changes from time to time and the latest version of these Terms from time to time will be posted to the Site.
(a) (a) Applications or designs which relate to socially taboo topics, such as illicit drug use or sexual gratification; (b) (b) Applications or designs that are or could reasonably be considered to be illegal, immoral, discriminatory or offensive as determined by the Organiser and/or the Judges; (c) (c) Applications or applications in relation to them which if accepted would infringe or breach any of the policies or terms of access or use of the Site.
|
Top Comments
I just read the TI release on this new board.
It looks really useful, bundled with the MSP432 it would be a welcome addition for use, especially as a UI device.
DAB
RoadTesters Selected:
kas.lewis
dwinhold
stefacc
ashishshelke989
balearicdynamics
satyavrat
DoctorC
bfvillaluna
maperales
billabott
As it seems almost useful the first blog I posted in this section that is one of the article I am preparing to Road Test the TI Edutcational Boosterpack MKII, here is the article link: TI Educational Boosterpack…