CEL Robox 3D Printer

View table of contents ...  

Roadtest Closed: Scroll down to see the reviews!

Introduction
Robox 3D PrinterRobox is a micro manufacturing platform that features a removable head and material feed. Using a FFF dual nozzle head and a suitable filament material feed you can create 3d printed models of any 3d model in .stl format.
Features
  • Works Out of the Box - Plug in the power and USB cord and start printing.. automated bed levelling, intuitive software and advanced hardware all come together to make Robox reliable and easy to use.
  • High Resolution - Robox has one of the highest print resolutions of any FFF printer in the market - 20µm (0.02mm) layers.
  • Dual Nozzle System for Speed - Robox includes a dual-nozzle system which closes the flow of material and lifts the unused nozzle. Up to 300% faster than our competitors.
  • Automatic Material Recognition, No Vendor Lock-in - Robox requires no programming for different materials - just load the SmartReel and go! Each reel contains a chip which is programed with all the necessary parameters. You can load and programme these reels yourself or buy them loaded with filament ready to go.
  • Quick-Change Head - The removable head system allows you to change the function of Robox quickly and easily. Upgrade your Robox to become a dual material printer, stylus cutter, milling head or 3D scanner, the possibilities are endless!
  • Replaceable, 'Tape-less' and Removable PEI Bed - Sticky when hot, free when cool - no hassle. The print surface is easily removable - allowing for easy replacement for other functions.
  • Future Proof - Robox is ready for a second extruder, and we've kept in mind all possible later upgrades.
  • Compact Frame and Case Design - The frame and motion systems are extremely rigid and accurately positioned. BIG parts can be cut into multiple sections keeping the printer desktop but your projects endless.
Product Video
Terms & Conditions
  • Testers will be selected on the basis of quality of applications: we expect a full and complete description of why you want to test this particular product.
  • Testers are required to produce a full, comprehensive and well thought out review within 2 months of receipt of the product.
  • Failure to provide this review within the above timescale will result in the enrolee being excluded from future RoadTests.
RoadTest Reviews
Comments
Anonymous
  • You are correct fredrick, we all start at level 0, but some of us start helping, asking questions or other things first or at the very least start with smaller simpler road tests. I have done a few now and they have all been small ones. As for "discrimination" by saying level 0 take the kit and run, its not so far of if you look around sO would NOT say its discrimination. The other thing I have seen a bit of is a very lame review "I tried to get kit working nothing happend so I'm done...". Especially in a case like this were a company is trying to PROMOTE their product we would expect the reviewers to put in a GREAT deal of effort. If you look at some of the other big reviews how the testers have put in weeks of work if not more to get a good full review even working with the manufacturer to solve issues. I do believe that big reviews like this should be earned by proving that someone can deliver through smaller reviews and that they can actually write a proper review.

     

    The other issue is duplicate accounts, people opening 5, 10 or who knows how any new accounts to try increase their odds. If you don't allow level 0 this becomes a non issue as someone would need to maintain ALL their duplicate accounts to get them to a respectable level in order for it to be worth anything.

     

    I know you probably wont like what I had to say Fredrick and Danieal but its how I feel and what I have seen looking around the road test review section of this site. If Element14 wants the site to grow and be more useful than the content needs to be that way too, its not just about the number of "members" but about the number of users.

     

    Kas

  • We all started als Level 0 at some point. Getting selected on a Roadtest as a level 0 is what got me started here.

    It's sad to see people run off with their kit, but we shouldn't generalise ...

     

    Frederick

  • not all new members will do that I wont its border line discrimination saying that

  • I completely agree with you, we spend hours and hours on the community looking for answers and solutions to our problems and solving other's problems. there must be some kind of eligibility criteria for the participants. Most of the new members selected in road tests just keep the goodies and never write any reviews, this happens almost in all big road tests...

  • Dawn,

    I believe Michael has a pretty good guess.

     

    -Steve

  • Over 200 applications so far, so I'm gonna guess about 9 days after it closes. That's just a guess.

  • I was wondering when the testers will be announced. Will it be at the end date on the 27th?

  • it looks like it could be done don't really know to I see it up close

  • We all will Gabriel,

     

    I'm sure we we'll have some good reviews.

    There's a lot to review.

     

    -Steve

  • I'll be very unhappy if any of the chosen do not make a comment about it.

  • daniel lyall wrote:

     

    yea that's what this machine is meant to be for.

    A all in one I would say the makers of this machine I hope that they would give a plan for the mounting bracket to someone that would be keen to make a add on for it. I know I would like to add a laser to it for engraving.

    don't need a router add on I all ready have one.

    connecting a drag knife would be very easy to do same as a scanner/probe as you only need the machine to move to do what's needed it will just require a couple of different G code profiles.

     

    and by the look of the extruder head it just connects to the carriage so all you need to know is its paten and what its connections do.

    I agree Daniel,

    As long as the alignment can be calibrated and maintained, the bracket can be modified as necessary to accommodate custom heads.

     

    We discussed the development of a platform with this capability earlier in the year. I'm eager to see if this is a versatile enough platform to ware the all-in-one badge.

     

    -Steve

  • Andy Clark wrote:

     

    I find time and money are typically more limiting than my imagination, althought most problems can be resolved by applying more imagination...

    ClockFaceFinished.jpg

    True,  that's why  our designs must be more intuitive, be multitask capable. and above all, they must be efficient.

     

    By the way, that's a nice looking clock.  Did you build it?

     

    -Steve

  • yea that's what this machine is meant to be for.

    A all in one I would say the makers of this machine I hope that they would give a plan for the mounting bracket to someone that would be keen to make a add on for it. I know I would like to add a laser to it for engraving.

    don't need a router add on I all ready have one.

     

    connecting a drag knife would be very easy to do same as a scanner/probe as you only need the machine to move to do what's needed it will just require a couple of different G code profiles.

     

    and by the look of the extruder head it just connects to the carage so all you need to know is its paten and what its connections do.

  • "Quick-Change Head - The removable head system allows you to change the function of Robox quickly and easily. Upgrade your Robox to become a dual material printer, stylus cutter, milling head or 3D scanner, the possibilities are endless!"

     

    A probe could be added to check dimensions of a part. Perhaps the first thing to be printed would be mounting platform to attach other things to the head?

  • any way this is meant to be about this 3D printer not what I am doing

  • the controller takes all of that into account, I am not the person who came up with this in the first place I just get to help getting it running on a different laser set up.

    it is working really well it just need different set ups to make it a use by any one system or for it to be used for rebuilds of crap lasers.

    it will be able to be used as a add on to different cnc set-ups soon, it just need lots more testing and refinement of the codes it will be at lest a year before its all go

  • There was a discussion on a LinkedIn metalworking group about overheating issues with sharp corners and points. In those cases it would be good to dial down the laser power or use pulsing as is done in welding to avoid overheating

  • I find time and money are typically more limiting than my imagination, althought most problems can be resolved by applying more imagination...

    ClockFaceFinished.jpg

  • Technology, isn't it marvelous?

    You are only limited by your imagination.

     

    -Steve