Apply to review the ams OSRAM AS1170 Evaluation Kit

View table of contents ...  

We're looking for engineers to take ams OSRAM's AS1170 Evaluation Kit for a spin, stretch its legs and evaluate what it can do. We'll send you the hardware, for free. You test it out and once you've posted your review, it's yours to keep forever.

What is the AS1170 Evaluation Kit?

The AS1170 Evaluation Kit (AS1170 EVK) integrates the ams AS1170 with 4 on-board 850nm Infrared (IR) LEDs. Intended to drive High Current LEDs and VCSELs, the AS1170 is a DCDC step up converter designed to easily integrate into noise-sensitive RF systems. Controlled by I2C, the AS1170 EVK is outfitted with an IR LED break-out board connector also included within the kit, connection points for an external lab power supply and the included ESP32 for programming and control. The break-out board includes solder points for different LED footprints from ams OSRAM and other LED and VCSEL types. 
image

Key Features of the ams AS1170

  • High efficiency 4 MHz fixed frequency DCDC boost converter
  • Independently controlled channels
  • Channels can be combined for single output - 2 channels independently with up to 1000 mA each or 2000 mA combined
  • PWM operation for lower output current 31.25 kHz to avoid audible noise
  • Automatic current adjustment for low battery voltage for automatic battery lifetime extension
  • Integrated circuit protection functions

What's Included

RoadTesters will receive or have access to:

  • ams OSRAM AS1170 WL EVM EB Evaluation Kit, including:
    • ams OSRAM AS1170 EVK
    • 2 x ams OSRAM IR LED Break-out board
    • ESP32 S2 DevKit M1
    • 1m USB 2.0A to USB2.0 Micro-B Cable
  • 2 x OSRAM OSLONTm Black SFH 4726 BS A01 LEDs
  • 2 x OSRAM SYNIOSTm P2720 SFH 4795BS LEDs
  • ams AS1170 PC GUI Software V1.1

image

Documentation & Useful Links

Equipment You'll Need to Try It

To try out the AS1170 Evaluation Kit, you'll need the following:

  • A computer capable of connecting to the ESP32 S2 DevKit M1 via USB Type-A.
  • The Arduino IDE for writing MCU Sketches.
  • A digital camera such as that on a phone, laptop or tablet where you can take video to verify the IR LEDs are working.

You may also find it helpful to have the following equipment on-hand:

  • A Soldering Iron and associated solder, suiitable to perform surface mount soldering.
  • A laboratory power supply and cables, capable of supplying 4.4 V.

RoadTester Tasks and Instructions

  1. Unbox and explore the Evaluation Kit following the available Quick Start Guide.
  2. Try the kit as-it-comes, using the available software to try out the kit's capabilities.
  3. Run the example code available to trigger integrated LEDs.
  4. Develop your own program, using the Evaluation kit to complete a task.
  5. Document your experience in a review, including where the kit was strong and where it could improve.

If you have a project to use the kit for, that would be ideal as a test case for the review. Otherwise use the kit as it comes and test out what you can do with the included documentation, hardware and available software. Show to the reader what will likely be their experience using the kit for the first time. Text, pictures, video and/or any other media, so the reader understands what is involved in using the product.

Important Dates

Begin enrollment December 17 2025
End enrollment January 18 2026
Select RoadTesters Week of January 26 2026
Ship unit

Ideally within 14 days upon confirmation of selected RoadTesters and subject to compliance checks.

Begin RoadTesting On Receipt of Kit
element14 follow-up 6 weeks after selection
Post reviews 2 to 3 months after Kit Receipt

Terms and Conditions

About the Sponsor

ams OSRAM pioneer differentiating light and sensor solutions. Looking back on more than 100 years of industry experience, they combine engineering excellence and global manufacturing capabilities with passion for cutting-edge innovation. Their commitment to pushing the boundaries of illumination, visualization, and sensing has earned them the trust of customers worldwide. Together, they create break-through applications that make our world safer, smarter, and more sustainable. 

“Sense the power of light” – their success is based on their deep understanding of the potential of light. They harness its full spectrum – visible and invisible – to illuminate their surroundings as well as gather information from them. By adding intelligence to light, they enable their customers to drive transformative applications. 

Their distinct portfolio of advanced light and sensor technologies sets them apart in our industry. It includes high-quality semiconductor-based light emitters, sensors, CMOS ICs and software as well as a range of traditional lighting technologies for automotive and special applications. To learn more, click here.

RoadTest Reviews
Comments
Anonymous